<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCF52277 Doubt in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-Doubt/m-p/168453#M6044</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All. I am using MCF52277 for my design. I need CAN and I2C. But in this device both are multiplexed in the same pin. How can I use bith CAN and I2C. My primary communication is CAN and it can happen any time from the peripherals. But I2C is time triggered on and will happen once in 5 minutes or so.&lt;/P&gt;&lt;P&gt;Tapping this pin to CAN and I2C , a good design?. I am sure No. Help me how to use CAN and I2C\&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gilbert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Dec 2010 14:59:28 GMT</pubDate>
    <dc:creator>Gilbert</dc:creator>
    <dc:date>2010-12-09T14:59:28Z</dc:date>
    <item>
      <title>MCF52277 Doubt</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-Doubt/m-p/168453#M6044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All. I am using MCF52277 for my design. I need CAN and I2C. But in this device both are multiplexed in the same pin. How can I use bith CAN and I2C. My primary communication is CAN and it can happen any time from the peripherals. But I2C is time triggered on and will happen once in 5 minutes or so.&lt;/P&gt;&lt;P&gt;Tapping this pin to CAN and I2C , a good design?. I am sure No. Help me how to use CAN and I2C\&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gilbert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Dec 2010 14:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-Doubt/m-p/168453#M6044</guid>
      <dc:creator>Gilbert</dc:creator>
      <dc:date>2010-12-09T14:59:28Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52277 Doubt</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-Doubt/m-p/168454#M6045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it seems there are another pins have i2c function &amp;nbsp;in mcf52277, except for those multiplex with can&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;by the way, I also do 52277 board, but I find it has too many multiplex pins, which is a very bad design, currently, I am going to quit the project, and select new mpu to do it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Dec 2010 15:12:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-Doubt/m-p/168454#M6045</guid>
      <dc:creator>bluehacker</dc:creator>
      <dc:date>2010-12-10T15:12:00Z</dc:date>
    </item>
  </channel>
</rss>