<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックMCF52277 USB Protocol Stack</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-USB-Protocol-Stack/m-p/168309#M6011</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am using a M52277EVB board for evaluation of the MCF52277. I want to know if there is a USB protocol stack available for it. I am aware that the Linux already installed supports the USB OTG port, however I want to create a bare metal (No OS) application. On other Freescale MCU's there is available the CMX USB stack. It however is not available for this micro. I believe the reason is that the USB OTG module on this micro is different to the ones used on other MCU's such as the MCF52211. I have looked at the data sheets and the OTG modules are completely different - different registers etc. I do wonder why Freescale would do something like this especially since they&amp;nbsp;both&amp;nbsp; use Coldfire V2 cores and are both relatively new products.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 29 Mar 2009 17:48:37 GMT</pubDate>
    <dc:creator>paulsky</dc:creator>
    <dc:date>2009-03-29T17:48:37Z</dc:date>
    <item>
      <title>MCF52277 USB Protocol Stack</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-USB-Protocol-Stack/m-p/168309#M6011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am using a M52277EVB board for evaluation of the MCF52277. I want to know if there is a USB protocol stack available for it. I am aware that the Linux already installed supports the USB OTG port, however I want to create a bare metal (No OS) application. On other Freescale MCU's there is available the CMX USB stack. It however is not available for this micro. I believe the reason is that the USB OTG module on this micro is different to the ones used on other MCU's such as the MCF52211. I have looked at the data sheets and the OTG modules are completely different - different registers etc. I do wonder why Freescale would do something like this especially since they&amp;nbsp;both&amp;nbsp; use Coldfire V2 cores and are both relatively new products.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Mar 2009 17:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-USB-Protocol-Stack/m-p/168309#M6011</guid>
      <dc:creator>paulsky</dc:creator>
      <dc:date>2009-03-29T17:48:37Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52277 USB Protocol Stack</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-USB-Protocol-Stack/m-p/168310#M6012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please check this link:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?ProdMetaId=PID%2FDT%2FMCF5227X&amp;amp;isAdvanceSearch=false&amp;amp;showCustomCollateral=false&amp;amp;RELEVANCE=true&amp;amp;fromTrng=false&amp;amp;fromPSP=true&amp;amp;showAllCategories=false&amp;amp;fpsp=1&amp;amp;SelectedAsset=Design%20Tools&amp;amp;&amp;amp;assetLocked=false&amp;amp;leftNavCode=1&amp;amp;assetLockedForNavigation=true&amp;amp;code=MCF5227X&amp;amp;isResult=false&amp;amp;componentId=2&amp;amp;searchSessionId=8fd62f1238477239821.3&amp;amp;fromDAP=false&amp;amp;fromWebPages=false&amp;amp;tab=Design_Tools_Tab&amp;amp;isTree=false&amp;amp;isFromFlex=false&amp;amp;Design%20Tools=Design%20Tools/020JOVEXKHR6%60%60Run-time%20Software/070JOVFM2DJB%60%60Snippets%2C%20Boot%20Code%2C%20Headers%2C%20Monitors%2C%20Etc.&amp;amp;isComparison=false&amp;amp;" target="test_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?ProdMetaId=PID%2FDT%2FMCF5227X&amp;amp;isAdvanceSearch=false&amp;amp;showCustomCollateral=false&amp;amp;RELEVANCE=true&amp;amp;fromTrng=false&amp;amp;fromPSP=true&amp;amp;showAllCategories=false&amp;amp;fpsp=1&amp;amp;SelectedAsset=Design%20Tools&amp;amp;&amp;amp;assetLocked=false&amp;amp;leftNavCode=1&amp;amp;assetLockedForNavigation=true&amp;amp;code=MCF5227X&amp;amp;isResult=false&amp;amp;componentId=2&amp;amp;searchSessionId=8fd62f1238477239821.3&amp;amp;fromDAP=false&amp;amp;fromWebPages=false&amp;amp;tab=Design_Tools_Tab&amp;amp;isTree=false&amp;amp;isFromFlex=false&amp;amp;Design%20Tools=Design%20Tools/020JOVEXKHR6%60%60Run-time%20Software/070JOVFM2DJB%60%60Snippets%2C%20Boot%20Code%2C%20Headers%2C%20Monitors%2C%20Etc.&amp;amp;isComparison=false&amp;amp;&lt;/A&gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It has some sample code for using USB module found on MCF52277, I think you can build on that for your own stack.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The reason for using different USB modules on MCF52277 and MCF5221x is because MCF52277 is the MPU series and the USB module implements a simplied EHCI-compliant USB module(supports high speed), while MCF5221x is a MCU, its USB module is more simple and does not support high speed, only support full and low speed. Check AN3631 for more information on MCF52277 USB module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?ProdMetaId=PID%2FDC%2FMCF5227X&amp;amp;isAdvanceSearch=false&amp;amp;showCustomCollateral=false&amp;amp;RELEVANCE=true&amp;amp;fromTrng=false&amp;amp;showAllCategories=false&amp;amp;fpsp=1&amp;amp;fromPSP=true&amp;amp;SelectedAsset=Documentation&amp;amp;&amp;amp;assetLocked=false&amp;amp;leftNavCode=1&amp;amp;assetLockedForNavigation=true&amp;amp;code=MCF5227X&amp;amp;isResult=false&amp;amp;componentId=2&amp;amp;searchSessionId=34ce581238477601021.0&amp;amp;fromDAP=false&amp;amp;fromWebPages=false&amp;amp;tab=Documentation_Tab&amp;amp;isTree=false&amp;amp;isFromFlex=false&amp;amp;isComparison=false&amp;amp;Documentation=Documentation/11010KscRcb%60%60Application%20Notes&amp;amp;" target="test_blank"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?ProdMetaId=PID%2FDC%2FMCF5227X&amp;amp;isAdvanceSearch=false&amp;amp;showCustomCollateral=false&amp;amp;RELEVANCE=true&amp;amp;fromTrng=false&amp;amp;showAllCategories=false&amp;amp;fpsp=1&amp;amp;fromPSP=true&amp;amp;SelectedAsset=Documentation&amp;amp;&amp;amp;assetLocked=false&amp;amp;leftNavCode=1&amp;amp;assetLockedForNavigation=true&amp;amp;code=MCF5227X&amp;amp;isResult=false&amp;amp;componentId=2&amp;amp;searchSessionId=34ce581238477601021.0&amp;amp;fromDAP=false&amp;amp;fromWebPages=false&amp;amp;tab=Documentation_Tab&amp;amp;isTree=false&amp;amp;isFromFlex=false&amp;amp;isComparison=false&amp;amp;Documentation=Documentation/11010KscRcb%60%60Application%20Notes&amp;amp;&lt;/A&gt;;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Mar 2009 12:34:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52277-USB-Protocol-Stack/m-p/168310#M6012</guid>
      <dc:creator>cutworth</dc:creator>
      <dc:date>2009-03-31T12:34:35Z</dc:date>
    </item>
  </channel>
</rss>