<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: SDHC card MISO Remains Low</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDHC-card-MISO-Remains-Low/m-p/167440#M5938</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It was not quite as 2 dimensional as that, there were no changes in the electrical schematic only in the PCB layout so there should have been no hardware induced issues.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was hoping there was a common problem that caused a low MISO but I couldn't find anything on forums.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However I solved the issue, it came down to a poor contact that was hidden under the smd sd socket.&amp;nbsp; It wasn't immediately clear even with a microscope.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Sep 2011 19:33:24 GMT</pubDate>
    <dc:creator>Dave_W</dc:creator>
    <dc:date>2011-09-19T19:33:24Z</dc:date>
    <item>
      <title>SDHC card MISO Remains Low</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDHC-card-MISO-Remains-Low/m-p/167438#M5936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm having an issue communicating with my SDHC card.&amp;nbsp; I should mention that I have communicated with this card before with the same code on a slightly older version of the circuit.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The mcf51 is communicating with the card via SPI via potential dividers on CS, MOSI and SCK as the micro is running at 5V to fulfill several other requirements.&amp;nbsp; The MISO line is put through a hex inverter to buffer the signal up to 5V.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have not connected any pullup resistors anywhere, but I assumed that it wasn't necessary given that first prototype I made worked without them with this same card.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Essentially I get no response from the card.&amp;nbsp; The MISO line remains Low all the time.&amp;nbsp; Can anyone suggest a potential reason for this?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Dave Wright&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Sep 2011 20:25:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDHC-card-MISO-Remains-Low/m-p/167438#M5936</guid>
      <dc:creator>Dave_W</dc:creator>
      <dc:date>2011-09-16T20:25:13Z</dc:date>
    </item>
    <item>
      <title>Re: SDHC card MISO Remains Low</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDHC-card-MISO-Remains-Low/m-p/167439#M5937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So it was working, then you changed the circuit and it doesn't work anymore. I think there's a clue there &lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What does the electrical specification say for each of the devices you're using?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2011 19:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDHC-card-MISO-Remains-Low/m-p/167439#M5937</guid>
      <dc:creator>FridgeFreezer</dc:creator>
      <dc:date>2011-09-19T19:14:38Z</dc:date>
    </item>
    <item>
      <title>Re: SDHC card MISO Remains Low</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDHC-card-MISO-Remains-Low/m-p/167440#M5938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It was not quite as 2 dimensional as that, there were no changes in the electrical schematic only in the PCB layout so there should have been no hardware induced issues.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was hoping there was a common problem that caused a low MISO but I couldn't find anything on forums.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;However I solved the issue, it came down to a poor contact that was hidden under the smd sd socket.&amp;nbsp; It wasn't immediately clear even with a microscope.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the response.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Sep 2011 19:33:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/SDHC-card-MISO-Remains-Low/m-p/167440#M5938</guid>
      <dc:creator>Dave_W</dc:creator>
      <dc:date>2011-09-19T19:33:24Z</dc:date>
    </item>
  </channel>
</rss>