<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB controller on MCF5474 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167225#M5905</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You might consider one of the MCF5445x processors.&amp;nbsp; These are also based on the Coldfire V4e core with a MMU and run Linux.&amp;nbsp; There are variations of the processor with different functionality in them.&lt;BR /&gt;&lt;BR /&gt;The MCF54451 part does not have the PCI and ATA functionality but does have USB, I2C and DSPI - which you mentioned you need.&lt;BR /&gt;&lt;BR /&gt;--Kurt&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jun 2008 13:26:29 GMT</pubDate>
    <dc:creator>kmahan</dc:creator>
    <dc:date>2008-06-25T13:26:29Z</dc:date>
    <item>
      <title>USB controller on MCF5474</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167222#M5902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i have some questions about the MCF5474 USB controller:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Why is possible in the USBAISR register, that IN as well as OUT Tocken are seted in a definitely OUT Endpoint Interrupt, although the ACK Bit for In-transaction is not seted???&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2.Why are core-interrupt as well as endpoint(0-7)-interrupt at the same time there, if the host controller send a In-Tocken to the MCF5474 ???&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance for the help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2008 18:45:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167222#M5902</guid>
      <dc:creator>mcf5474</dc:creator>
      <dc:date>2008-06-24T18:45:40Z</dc:date>
    </item>
    <item>
      <title>Re: USB controller on MCF5474</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167223#M5903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;I'm sorry to be the bearer of bad news, but the USB Controller on the MCF547x/8x devices has an errata that makes them basically unusable: &lt;A href="http://www.freescale.com/files/32bit/doc/errata/MCF5475DE.pdf?fpsp=1&amp;amp;WT_TYPE=Errata&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation" rel="nofollow" target="_blank"&gt;MCF5475DE&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;-mnorman&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2008 03:33:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167223#M5903</guid>
      <dc:creator>mnorman</dc:creator>
      <dc:date>2008-06-25T03:33:49Z</dc:date>
    </item>
    <item>
      <title>Re: USB controller on MCF5474</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167224#M5904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hallo mnorman,&lt;BR /&gt;&lt;BR /&gt;thanks for the very quick reply. Do you can advise me some other, better MC, analog to the functionality from MCF5474? I use USB, I2C and DSPI...&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;best regards ivan&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2008 13:10:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167224#M5904</guid>
      <dc:creator>mcf5474</dc:creator>
      <dc:date>2008-06-25T13:10:32Z</dc:date>
    </item>
    <item>
      <title>Re: USB controller on MCF5474</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167225#M5905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You might consider one of the MCF5445x processors.&amp;nbsp; These are also based on the Coldfire V4e core with a MMU and run Linux.&amp;nbsp; There are variations of the processor with different functionality in them.&lt;BR /&gt;&lt;BR /&gt;The MCF54451 part does not have the PCI and ATA functionality but does have USB, I2C and DSPI - which you mentioned you need.&lt;BR /&gt;&lt;BR /&gt;--Kurt&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2008 13:26:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167225#M5905</guid>
      <dc:creator>kmahan</dc:creator>
      <dc:date>2008-06-25T13:26:29Z</dc:date>
    </item>
    <item>
      <title>Re: USB controller on MCF5474</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167226#M5906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;It is a nice mikroprocessor, i forgot to say, that i need some one with FPU too. Any other recommendations?&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2008 14:17:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-controller-on-MCF5474/m-p/167226#M5906</guid>
      <dc:creator>mcf5474</dc:creator>
      <dc:date>2008-06-27T14:17:01Z</dc:date>
    </item>
  </channel>
</rss>