<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: M52233DEMO board</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167149#M5891</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;This MCF52233DEMO is a very problematic board &lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have one that was faulty out of the box and it would not connect to USB at all. I eventually traced the problem to bad soldering. I removed and refitted the HCS12 micro in the BDM section and used&amp;nbsp;new solder&amp;nbsp;and that resolved problems with the BDM I was having. I was finally able to connect after discovering the BDM came to life if I pressed down on the chip.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The board draws an astronomical amount of current, it will, for example, trip the current limiting on my PC motherboard if plugged in with the power switch on. I suspect there's also problems with the CPU itself as it sometimes will run my code, sometimes not and Codewarrior will swear that the code is running perfectly.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Because I can't be sure of whether I have a good board or not or if my code is at fault, I've since scrapped the board and have ordered a new one, which this time I hope will work.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jul 2008 14:31:40 GMT</pubDate>
    <dc:creator>JTech</dc:creator>
    <dc:date>2008-07-24T14:31:40Z</dc:date>
    <item>
      <title>M52233DEMO board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167145#M5887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I got M52233DEMO board with P&amp;amp;E USB Multilink from my colleague. It don't have CD, so i downloaded codewarrior standard edition. I have tried the example program, but when ever tried to connect with host PC and turn the power supply switch to ON position, all the LEDs are start blinking. Power LED is not on at all. I have connected properly and verified the jumper connection. Everything is correct. Can someone help me. I could not able to find more artcle on this except some schematics, user guide from AXIOM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in Advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Baski&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2008 15:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167145#M5887</guid>
      <dc:creator>Boss</dc:creator>
      <dc:date>2008-06-24T15:55:14Z</dc:date>
    </item>
    <item>
      <title>Re: M52233DEMO board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167146#M5888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;If you don't get an answer, Axiom tech support will look at it.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jun 2008 19:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167146#M5888</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2008-06-24T19:40:57Z</dc:date>
    </item>
    <item>
      <title>Re: M52233DEMO board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167147#M5889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Thank you for your mail. I don't know by some how the board working now. In one PC its not working due to USB driver problem. Other PC with properly installed Codewarrior IDE works fine with board. If any queries, I am searching for MCF52233 C Compiler manual. I could not able to find in Freescale site. If any one has the manual please mail me.&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Boss.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jun 2008 12:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167147#M5889</guid>
      <dc:creator>Boss</dc:creator>
      <dc:date>2008-06-26T12:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: M52233DEMO board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167148#M5890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;There is not a processor-specific compiler manual. For CodeWarrior installations, you'll find the &lt;I&gt;MSL C Manual&lt;/I&gt; and the &lt;I&gt;Targeting ColdFire&lt;/I&gt; manual in the \Help directory where you installed the software.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jun 2008 04:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167148#M5890</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2008-06-27T04:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: M52233DEMO board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167149#M5891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;This MCF52233DEMO is a very problematic board &lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I have one that was faulty out of the box and it would not connect to USB at all. I eventually traced the problem to bad soldering. I removed and refitted the HCS12 micro in the BDM section and used&amp;nbsp;new solder&amp;nbsp;and that resolved problems with the BDM I was having. I was finally able to connect after discovering the BDM came to life if I pressed down on the chip.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The board draws an astronomical amount of current, it will, for example, trip the current limiting on my PC motherboard if plugged in with the power switch on. I suspect there's also problems with the CPU itself as it sometimes will run my code, sometimes not and Codewarrior will swear that the code is running perfectly.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Because I can't be sure of whether I have a good board or not or if my code is at fault, I've since scrapped the board and have ordered a new one, which this time I hope will work.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2008 14:31:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52233DEMO-board/m-p/167149#M5891</guid>
      <dc:creator>JTech</dc:creator>
      <dc:date>2008-07-24T14:31:40Z</dc:date>
    </item>
  </channel>
</rss>