<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: MCF537x - ( LTIB - uClinux - BSP ) Kernel Startup Questions ( seems simple isn't it ? )</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166475#M5826</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. I am not 100% sure how to get the early boot messages to show up in your UART2.&amp;nbsp; That is a good question to post to the uclinux mailing list.&amp;nbsp; Here is a link that may be useful as well.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.linux.it/~rubini/docs/sercons/sercons.html" rel="nofollow" target="_blank"&gt;http://www.linux.it/~rubini/docs/sercons/sercons.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. To add custom files you can use the merge directory.&amp;nbsp; there is typically a ltib_install/config/platform/platform_name/merge directory that you can place customized files in.&amp;nbsp; If there is not one you can create it and the put your new rc.conf in merge/etc/rc.d&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jun 2009 00:20:40 GMT</pubDate>
    <dc:creator>fsl_linux_spt</dc:creator>
    <dc:date>2009-06-10T00:20:40Z</dc:date>
    <item>
      <title>MCF537x - ( LTIB - uClinux - BSP ) Kernel Startup Questions ( seems simple isn't it ? )</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166473#M5824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello to everyone...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working in a custom board ( partialy ) based&amp;nbsp; on LOGICPD m537xEVB board.&lt;/P&gt;&lt;P&gt;After many troubles and difficults, we have our own board partially working with linux, but still there are some minor ( ! ) dificults that we can not overcome.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1 - First we need to change ( redirect, etc.. ) the default serial port ( console ) from UART0 to UART2.&lt;/P&gt;&lt;P&gt;At first sigth seems easy because you can set the console device by setting on the kcl command line from bootloader ( dBUG in this case... ), but this setting does not change the serial port from the kernel early boot, this is done late when almost the entire system is running. So we loose all the debug information from the kernekl start-up.&lt;/P&gt;&lt;P&gt;It's supoosedto be a temporal buffer where the 'printk' stores the text if there no console device but in our case this is not true, because if we set the console to UART2, these lines never are printed on ANY UART.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Any IDEA????? we need just to know where the 537x is first, first is set, or where the default port, not in linux side, is set.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2 - This seems more easy; I need to change the loading order for linux services, because i want to automatize a cifs mount via fstab, but as the 'network' is loaded after 'filesystems' the fist attempt fails. Of course after boot, a simple 'mount -a' does the job without problems!!!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried to change the order position of 'network' service at 'rc.conf' to put before 'filesystems' but when i compile via ./ltib the file is set to it's defaults so my modification is lost.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also i have tried to modify the position in sysconfig.lkc without success..... compiling the kernel leaves all unchanged....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What i can do???&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;3 - Finally i have problems compiling the 'libusb' package: ( as on many others...)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #0000ff; font-size: 1;"&gt;m68k-uclinux-gcc -shared&amp;nbsp; .libs/usb.o .libs/error.o .libs/descriptors.o .libs/linux.o&amp;nbsp;&amp;nbsp; -Wl,-soname -Wl,libusb-0.1.so.4 -o .libs/libusb-0.1.so.4.4.0&lt;BR /&gt;/opt/freescale/usr/local/gcc-4.2.47-uclibc-0.9.47/m68k-uclinux/m68k-uclinux/libc/usr/lib/crt1.o: &lt;STRONG&gt;In function `_start':&lt;/STRONG&gt;&lt;BR /&gt;(.text+0x1c): &lt;STRONG&gt;undefined reference to `main'&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;...note that other packages are properly compiled and updated from GPP automatically...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Ok, thats all.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank's a lot!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Oscar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2009 21:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166473#M5824</guid>
      <dc:creator>osanz</dc:creator>
      <dc:date>2009-03-24T21:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: MCF537x - ( LTIB - uClinux - BSP ) Kernel Startup Questions ( seems simple isn't it ? )</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166474#M5825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oscar,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm having a similar problem to your point 2) - i want to add some startup commands to /etc/rc.local but every time i run ltib --configure to generate images for my MPC8315E-RBD eval board, it resets this file back to defaults, and i'm not sure where those defaults are stored. Did you ever resolve this issue ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Rob&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2009 20:36:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166474#M5825</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-06-09T20:36:15Z</dc:date>
    </item>
    <item>
      <title>Re: MCF537x - ( LTIB - uClinux - BSP ) Kernel Startup Questions ( seems simple isn't it ? )</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166475#M5826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. I am not 100% sure how to get the early boot messages to show up in your UART2.&amp;nbsp; That is a good question to post to the uclinux mailing list.&amp;nbsp; Here is a link that may be useful as well.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.linux.it/~rubini/docs/sercons/sercons.html" rel="nofollow" target="_blank"&gt;http://www.linux.it/~rubini/docs/sercons/sercons.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. To add custom files you can use the merge directory.&amp;nbsp; there is typically a ltib_install/config/platform/platform_name/merge directory that you can place customized files in.&amp;nbsp; If there is not one you can create it and the put your new rc.conf in merge/etc/rc.d&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2009 00:20:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166475#M5826</guid>
      <dc:creator>fsl_linux_spt</dc:creator>
      <dc:date>2009-06-10T00:20:40Z</dc:date>
    </item>
    <item>
      <title>Re: MCF537x - ( LTIB - uClinux - BSP ) Kernel Startup Questions ( seems simple isn't it ? )</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166476#M5827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I realized that I did not respond to libusb question.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks like libusb is not supported for uclinux targtets in LTIB.&amp;nbsp; Many of the packages available in LTIB are not tested to build or run on each bsp.&amp;nbsp; Only the packages selected by default in a bsp are considered tested and known to work.&amp;nbsp; Most of the time the other packages&amp;nbsp;work, but sometimes they do not.&amp;nbsp; LTIB targets both mmu-full (linux) and mmu-less (uclinux)&amp;nbsp;bsps.&amp;nbsp; The uclinux bsps have fewer packages that will build and run from the general LTIB package list.&amp;nbsp; Libusb is not a package&amp;nbsp;that is enabled in the bsp by default and it is no&amp;nbsp;longer presented as an option in more recent&amp;nbsp;LTIB uclinux targeted bsps.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2009 03:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166476#M5827</guid>
      <dc:creator>fsl_linux_spt</dc:creator>
      <dc:date>2009-06-10T03:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: MCF537x - ( LTIB - uClinux - BSP ) Kernel Startup Questions ( seems simple isn't it ? )</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166477#M5828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have some solution, but i had no time for post... sorry:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding the #1, UART redirection i finally have done by modifying the file 'mcf.c'.&lt;/P&gt;&lt;P&gt;Basically is need to 'force' to use the UART2 when the system is starting up:&lt;/P&gt;&lt;P&gt;First is need to configure the GPIO pins for this UART, because on this uP UART2 is not the default&lt;/P&gt;&lt;P&gt;function; I have done like this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1"&gt;&lt;FONT color="#0000ff"&gt;static void &lt;STRONG&gt;mcf_config_port&lt;/STRONG&gt;(struct uart_port *port, int flags)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; port-&amp;gt;type = PORT_MCF;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printk("MK36-&amp;gt;mcf_config_port( line= %d )\n", port-&amp;gt;line );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/FONT&gt; &lt;FONT color="#0000ff"&gt;&lt;STRONG&gt;if( port-&amp;gt;line == 2 )&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_GPIO_PAR_TIMER = ( 0 | MCF_GPIO_PAR_TIMER_PAR_TIN2(1) | MCF_GPIO_PAR_TIMER_PAR_TIN3(1) );&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_GPIO_PDDR_UART = ( 0 | MCF_GPIO_PDDR_UART_PDDR_UART6 );&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/STRONG&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Clear mask, so no surprise interrupts. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; writeb(0, port-&amp;gt;membase + MCFUART_UIMR);&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (request_irq(port-&amp;gt;irq, mcf_interrupt, IRQF_DISABLED, "UART", port))&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; printk(KERN_ERR "MCF: unable to attach ColdFire UART %d "&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; "interrupt vector=%d\n", port-&amp;gt;line, port-&amp;gt;irq);&lt;BR /&gt;}&lt;/FONT&gt;&lt;BR /&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Then force the UART channel:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000ff" size="1"&gt;static int __init mcf_console_setup(struct console *co, char *options)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; struct uart_port *port;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int baud = CONFIG_SERIAL_MCF_BAUDRATE;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int bits = 8;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int parity = 'n';&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int flow = 'n';&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if ((co-&amp;gt;index &amp;gt;= 0) &amp;amp;&amp;amp; (co-&amp;gt;index &amp;lt;= MCF_MAXPORTS))&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; co-&amp;gt;index = 0;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;STRONG&gt;co-&amp;gt;index = 2;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; port = &amp;amp;mcf_ports[co-&amp;gt;index].port;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (port-&amp;gt;membase == 0)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; return -ENODEV;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printk("mcf_console_setup( port= %d )\n", co-&amp;gt;index ); //To see it on startup...&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (options)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; uart_parse_options(options, &amp;amp;baud, &amp;amp;parity, &amp;amp;bits, &amp;amp;flow);&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; return uart_set_options(port, co, baud, parity, bits, flow);&lt;BR /&gt;}&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="1"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Also check on 'linux/arch/m68knommu/platform/537x/config.c' the interrupts are properly set for UART2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think that's all, but note that this is working on&amp;nbsp; &lt;STRONG&gt;"ltib-cf_nommu-20081215"&lt;/STRONG&gt; not on "&lt;STRONG&gt;ltib-m537xevb-20071109&lt;/STRONG&gt;". The new release is set by default to use "mcf.c" driver, while the previous one is set by default to "mfcserial.c".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding the #2:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is no posible combination ( i have not found ) to do this by setting the startup order.&lt;/P&gt;&lt;P&gt;Because a strange problem i have on the current distribution ( &lt;FONT size="1"&gt;see&amp;nbsp; &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=6925#M6925" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=6925#M6925&lt;/A&gt;&lt;/FONT&gt; ) i have found a good way to setup the board without scripts; put it on inittab !!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is my inittab file:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000ff" size="1"&gt;console::sysinit:/bin/mount -n -t proc proc /proc&lt;BR /&gt;console::sysinit:/bin/mount -n -t sysfs sys /sys&lt;BR /&gt;console::sysinit:/sbin/ifconfig eth0 xxx.xxx.xxx.xxx&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000ff" size="1"&gt;console::sysinit:/bin/mount -a&lt;BR /&gt;::respawn:-/bin/sh&lt;BR /&gt;::ctrlaltdel:/sbin/reboot&lt;BR /&gt;::shutdown:/etc/rc.d/rcS stop&lt;BR /&gt;::restart:/sbin/init&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also note that&amp;nbsp; &lt;FONT color="#0000ff" size="1"&gt;mount -a&amp;nbsp;&lt;/FONT&gt; Is using 'fstab' config where i can mount a network unit via CIFS, very useful on a board without samba or ftp server support!!! ( hey yaffs2* on a 2k block NAND!!! )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;fstab lines:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000ff" size="1"&gt;//xxx.xxx.xxx.xxx/PROGRAMS&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; /debug&amp;nbsp;&amp;nbsp;&amp;nbsp; cifs&amp;nbsp;&amp;nbsp;&amp;nbsp; rw,username=xxxx,password=xxxx &amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;0&lt;BR /&gt;/dev/mtdblock1&amp;nbsp;&amp;nbsp;&amp;nbsp; /newdir/nand1&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; yaffs&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; defaults&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; 0&lt;BR /&gt;/dev/mtdblock2&amp;nbsp;&amp;nbsp;&amp;nbsp; /newdir/nand2&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; yaffs&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; defaults&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; 0&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000ff" size="1"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;yaffs2*: Is need to patch 'yaffs_ObjectHeader' struct on 'ysffs_guts.h' by adding a dummy WORD:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000ff" size="1"&gt;typedef struct {&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000ff" size="1"&gt;...&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000ff" size="1"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* isShrink applies to object headers written when we shrink the file (ie resize) */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __u32 isShrink;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; __u16 dummy;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;------ DUMMY WORD!!!&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;} yaffs_ObjectHeader;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have found it on a forum but don't remember where....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regarding the #3:&lt;/P&gt;&lt;P&gt;Really is no need to use libusb at all. But note that on &lt;STRONG&gt;'ltib-m537xevb-20071109'&amp;nbsp;&lt;/STRONG&gt; USB system simply does not work.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suggest to upgrade to "&lt;STRONG&gt;ltib-cf_nommu-20081215"&lt;/STRONG&gt; ,under this distribution USB is working fine&lt;/P&gt;&lt;P&gt;( well.. i only have tested with some USB mouse, and some flash pen ).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="5"&gt;BUT&lt;/FONT&gt;:&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;&lt;STRONG&gt;ltib-cf_nommu-20081215&lt;/STRONG&gt;&lt;/FONT&gt;, under some unknown conditions, CAN NOT EXECUTE SCRIPTS???????&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I already have posted this question at:&lt;/P&gt;&lt;P&gt;&lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=6925#M6925" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=6925#M6925&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this can help some one!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR;&lt;/P&gt;&lt;P&gt;Oscar Sanz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2009 15:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF537x-LTIB-uClinux-BSP-Kernel-Startup-Questions-seems-simple/m-p/166477#M5828</guid>
      <dc:creator>osanz</dc:creator>
      <dc:date>2009-06-11T15:04:42Z</dc:date>
    </item>
  </channel>
</rss>