<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックAC'97 driver for the SSI bus</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AC-97-driver-for-the-SSI-bus/m-p/165865#M5746</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am currently using the linux kernel 2.6.29 with the mcf54451. I want to interface the SSI bus with a cs4202 audio codec. This chip conforms to the ac-link protocol, but I am not sure if there is driver support. It looks like there is some built in driver support in ALSA, but I'm not sure if this is true. If not I will need to get a driver for it and I have found none. Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 10 Sep 2011 01:34:33 GMT</pubDate>
    <dc:creator>mendelbullex</dc:creator>
    <dc:date>2011-09-10T01:34:33Z</dc:date>
    <item>
      <title>AC'97 driver for the SSI bus</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AC-97-driver-for-the-SSI-bus/m-p/165865#M5746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am currently using the linux kernel 2.6.29 with the mcf54451. I want to interface the SSI bus with a cs4202 audio codec. This chip conforms to the ac-link protocol, but I am not sure if there is driver support. It looks like there is some built in driver support in ALSA, but I'm not sure if this is true. If not I will need to get a driver for it and I have found none. Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 10 Sep 2011 01:34:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AC-97-driver-for-the-SSI-bus/m-p/165865#M5746</guid>
      <dc:creator>mendelbullex</dc:creator>
      <dc:date>2011-09-10T01:34:33Z</dc:date>
    </item>
    <item>
      <title>Re: AC'97 driver for the SSI bus</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AC-97-driver-for-the-SSI-bus/m-p/165866#M5747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, so it appears that the linux kernel has a driver for AC97 using PCI. Does nayone know if there is an interface that allows the mcf5445x to use this driver or another similar one with the SSI bus?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2011 00:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/AC-97-driver-for-the-SSI-bus/m-p/165866#M5747</guid>
      <dc:creator>mendelbullex</dc:creator>
      <dc:date>2011-09-13T00:32:25Z</dc:date>
    </item>
  </channel>
</rss>