<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCF52259/MCF52256 FB_CLK pin in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164123#M5478</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The FB_CLK signal is just internal synchronization signal which determines how fast the external access could be. On MCF52259 it could be set to equal fsys or Fsys/2 and you can refer to bus cycle execution and timing examples in the reference manual to get a clear point of the usage of FB_CLK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Minibus can connect asynchrous devices like SRAM, so there is no specific need for an clock signal like that on a SDRAM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Mar 2009 12:44:51 GMT</pubDate>
    <dc:creator>cutworth</dc:creator>
    <dc:date>2009-03-26T12:44:51Z</dc:date>
    <item>
      <title>MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164120#M5475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone.&lt;/P&gt;&lt;P&gt;I am wiring up an external dual-port RAM to the mini-FlexBus on the MCF52256, but I'm havuing trouble figuring out where the FB_CLK woul be on the 144 pin LQFP package.&amp;nbsp; Although its described in the text of the Flexbus secton, its not shown anywhere on the pin assigment.&amp;nbsp; Can anyone shed some light on this?&amp;nbsp; Its mentioned in the text, but then not shown in the pin tables.&amp;nbsp; I don't even see the CLKOUT pin.&amp;nbsp; I had the same trouble sorting out some of the BDM/JTAG pins, so I figure this output clock pin is&amp;nbsp;a dual-labled pin not shown completetly?.....&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2009 00:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164120#M5475</guid>
      <dc:creator>JMAC</dc:creator>
      <dc:date>2009-03-19T00:31:22Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164121#M5476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi&lt;BR /&gt;&lt;BR /&gt;Pin M3/43:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCLK/PSTCLK&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Secondary function: CLKOUT&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Tertiary function: FB_CLK&lt;BR /&gt;&lt;BR /&gt;I don’t actually see how this is controlled, but I expect that it is automatically activated when the debugger is not enabled and when the flex bus is active.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;BR /&gt;- OS, TCP/IP stack, USB, device drivers and simulator for M5221X, M5222X, M5223X, M5225X. One package does them all - &lt;EM&gt;"Embedding it better..."&lt;/EM&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2009 03:27:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164121#M5476</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-03-19T03:27:40Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164122#M5477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Current MCF52259 Ref Manual signal description table is crap.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The MCF52259_GPIO.h and other header&amp;nbsp;files in the downloadable EVB source is the most clarifying documentation on it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2009 18:23:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164122#M5477</guid>
      <dc:creator>MrBean</dc:creator>
      <dc:date>2009-03-19T18:23:20Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164123#M5478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The FB_CLK signal is just internal synchronization signal which determines how fast the external access could be. On MCF52259 it could be set to equal fsys or Fsys/2 and you can refer to bus cycle execution and timing examples in the reference manual to get a clear point of the usage of FB_CLK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Minibus can connect asynchrous devices like SRAM, so there is no specific need for an clock signal like that on a SDRAM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2009 12:44:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164123#M5478</guid>
      <dc:creator>cutworth</dc:creator>
      <dc:date>2009-03-26T12:44:51Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164124#M5479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Something to add,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pin M3/43:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCLK/PSTCLK&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Secondary function: CLKOUT&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Tertiary function: FB_CLK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So when you are not using BDM, you can configure this pin to output FB_CLK, so you can watch the FB_CLK with oscilloscope.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2009 12:48:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164124#M5479</guid>
      <dc:creator>cutworth</dc:creator>
      <dc:date>2009-03-26T12:48:18Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164125#M5480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you inform how the pin can be configured to connect the FB_CLK?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2009 19:29:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164125#M5480</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-03-26T19:29:07Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164126#M5481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can configure M3 to use as FB_CLK and connect it to external synchronous device like the dual-port FIFO ram.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2009 10:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164126#M5481</guid>
      <dc:creator>cutworth</dc:creator>
      <dc:date>2009-03-27T10:04:10Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164127#M5482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any tips on how to actually do this?&lt;/P&gt;&lt;P&gt;That is, in which register can it be programmed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The FB_CLK is a tertiary function on the TCLK/PSTCLK line (pin M3 on the 144 pin MAPBGA package) but the pin doesn't seem to belong to any port which can be controlled via a (PORT)PAR register. Therefore I assume that this is controlled from another block (like the System Control Module, or the the MiniFlex module itself) but the method hasn't been discovered yet...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2009 20:06:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164127#M5482</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-03-27T20:06:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164128#M5483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is a register in Table 15-1(Reference manual) named CLKOUTPAR at address 0x100074, this is used to select the output value of FB_CLK since it could be Fsys or Fsys/2. Unfortunate, it is not stated in the reference manual how to use it. Here is the code sample for how to use this register:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;FONT color="#000080" face="Courier New" size="2"&gt;&lt;SPAN&gt;#define MCF_GPIO_CLKOUTPAR&amp;nbsp; (*(vuint8 *)(0x40100077))&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;FONT color="#000080" face="Courier New" size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;FONT color="#000080" face="Courier New" size="2"&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_GPIO_CLKOUTPAR = 0x0;&amp;nbsp;&amp;nbsp; // off&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;FONT color="#000080" face="Courier New" size="2"&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_GPIO_CLKOUTPAR = 0x1;&amp;nbsp;&amp;nbsp; // clkout (80Mhz)&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;FONT color="#000080" face="Courier New" size="2"&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_GPIO_CLKOUTPAR = 0x2;&amp;nbsp;&amp;nbsp; // off&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;FONT color="#000080" face="Courier New" size="2"&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCF_GPIO_CLKOUTPAR = 0x3;&amp;nbsp;&amp;nbsp; // fb_clk&amp;nbsp; (40Mhz if MiniFlexBus default 1:2 Mode)&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;FONT color="#000080" face="Courier New" size="2"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;FONT color="#000080" face="Courier New" size="2"&gt;&lt;SPAN&gt;Hope this can help.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2009 09:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164128#M5483</guid>
      <dc:creator>cutworth</dc:creator>
      <dc:date>2009-04-01T09:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164129#M5484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks, that was the missing info. that was required.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2009 17:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164129#M5484</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-04-01T17:26:14Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259/MCF52256 FB_CLK pin</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164130#M5485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;so when &lt;FONT face="courier new,courier"&gt;CLKOUTPAR = 0x3&lt;/FONT&gt; and &lt;FONT face="courier new,courier"&gt;CCE[MBMOD] = 0x1&lt;/FONT&gt; (1:1 Mode)&lt;/P&gt;&lt;P&gt;Pin M3(144 MAPBGA) should be FB_CLK @ SYSCLK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And when &lt;FONT face="courier new,courier"&gt;CLKOUTPAR = 0x3&lt;/FONT&gt; and &lt;FONT face="courier new,courier"&gt;CCE[MBMOD] = 0x0&lt;/FONT&gt; (1:2 Mode)&lt;/P&gt;&lt;P&gt;Pin M3(144 MAPBGA) should be FB_CLK @ SYSCLK/2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this assumption correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For me the first assuption (1:1 Mode ) it is not possible to realize as shown above.&lt;/P&gt;&lt;P&gt;It seems that Pin M3(144 MAPBGA) is SYSCLK if &lt;FONT face="courier new,courier"&gt;CLKOUTPAR = 0x1&lt;/FONT&gt; and SYSCLK/2 if &lt;FONT face="courier new,courier"&gt;CLKOUTPAR = 0x3&lt;/FONT&gt;, regardless &lt;FONT face="courier new,courier"&gt;CCE[MBMOD]&lt;/FONT&gt; setting.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;How can I assign FB_CLK to Pin M3(144 MAPBGA) if FB_CLK is in 1:1 Mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2010 17:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-MCF52256-FB-CLK-pin/m-p/164130#M5485</guid>
      <dc:creator>Miggi</dc:creator>
      <dc:date>2010-01-13T17:55:08Z</dc:date>
    </item>
  </channel>
</rss>