<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: Linker Command File for MCF52277 - M52277EVB</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163586#M5413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the .lcf file that came with the CodeWarrior project was in error, that needs to be reported. Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework" rel="nofollow" target="_blank"&gt;here&lt;/A&gt; to file a service request to do that. Include the corrected .lcf file that you posted here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2009 20:40:58 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2009-03-19T20:40:58Z</dc:date>
    <item>
      <title>Linker Command File for MCF52277 - M52277EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163582#M5409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the M52277EVB with CodeWarrior for ColdFire V7.0.&amp;nbsp; I have successfully created projects that run from the external SDRAM and external Flash, but not both together.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to create a .lcf that puts code into external Flash, and use SDRAM for Ram.&amp;nbsp; When creating a project through the CodeWarrior New Project Wizard, the only targets I get are EXTERNAL_FLASH, EXTERNAL_RAM and CONSOLE_EXTERNAL_RAM.&amp;nbsp; I need a target like "EXTERNAL_FLASH_AND_RAM".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried to use a .lcf from a third-party project but I cannot easily use this as the initialisation code is very different.&amp;nbsp; For reference (and if it helps anyone else) the sample project is available here: &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.segger.com%2Fdownloads_eval.html" rel="nofollow" target="_blank"&gt;http://www.segger.com/downloads_eval.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have eliminated any problems with the compiler environment, hardware&amp;nbsp;and CF Flasher, as I can successfully build and flash the Segger example project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attached the .lcf files that I would like to combine.&amp;nbsp; Has anyone done this already?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Chris.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2009 22:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163582#M5409</guid>
      <dc:creator>cchilds</dc:creator>
      <dc:date>2009-03-17T22:29:49Z</dc:date>
    </item>
    <item>
      <title>Re: Linker Command File for MCF52277 - M52277EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163583#M5410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am a little bit confuse here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What do you want to do exactly?&lt;/P&gt;&lt;P&gt;What do you want to get in Flash? What do you want to get in SDRAM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How should the final memory map look like?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2009 22:48:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163583#M5410</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2009-03-17T22:48:57Z</dc:date>
    </item>
    <item>
      <title>Re: Linker Command File for MCF52277 - M52277EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163584#M5411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Many thanks for replying.&amp;nbsp; I will try to clarify my problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My project works fine using the External Ram LCF, where everything (code and data) goes into the external SDRAM at 0x40000000.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now that I have finished debugging, I want to place the code into External Flash, and use External SDRAM for runtime variables.&amp;nbsp; My Ram requirement is greater than the 128Kb on-chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want the memory map to be as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier"&gt;MEMORY {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; vectorrom&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000000, LENGTH = 0x00000400&lt;BR /&gt;&amp;nbsp;&amp;nbsp; cfmprotrom&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000400, LENGTH = 0x00000020&lt;BR /&gt;&amp;nbsp;&amp;nbsp; code&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RX)&amp;nbsp; : ORIGIN = 0x00000500, LENGTH = 0x0001FB00&lt;BR /&gt;&amp;nbsp;&amp;nbsp; vectorram&amp;nbsp;&amp;nbsp; (RWX) : ORIGIN = 0x80000000, LENGTH = 0x00000400&lt;BR /&gt;&amp;nbsp;&amp;nbsp; userram&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (RWX) : ORIGIN = 0x40000000, LENGTH = 0x04000000&lt;BR /&gt;}&lt;/FONT&gt;&lt;FONT face="courier new,courier"&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is identical to the CodeWarrior example stationery, except I have moved the 'userram' segment into External SDRAM at 0x4000000 (previously it was at 0x80000400 length 0x00007C00).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My project links with no errors, but after flashing with CF Flasher it doesn't run.&amp;nbsp; CF Flasher works with another example, so I am confident I am using it properly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Chris.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2009 23:03:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163584#M5411</guid>
      <dc:creator>cchilds</dc:creator>
      <dc:date>2009-03-17T23:03:17Z</dc:date>
    </item>
    <item>
      <title>Re: Linker Command File for MCF52277 - M52277EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163585#M5412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have resolved my problem with the linker file.&amp;nbsp; In case it helps anyone else, I have attached the .lcf that works for me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The sample .lcf files supplied with the M52277EVB&amp;nbsp;seem to be copied from a previous evaluation board, so were not exactly correct for the Flash and Ram on this particular board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Chris.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2009 22:17:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163585#M5412</guid>
      <dc:creator>cchilds</dc:creator>
      <dc:date>2009-03-18T22:17:58Z</dc:date>
    </item>
    <item>
      <title>Re: Linker Command File for MCF52277 - M52277EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163586#M5413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the .lcf file that came with the CodeWarrior project was in error, that needs to be reported. Click &lt;A href="https://www.freescale.com/webapp/servicerequest.create_SR.framework" rel="nofollow" target="_blank"&gt;here&lt;/A&gt; to file a service request to do that. Include the corrected .lcf file that you posted here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2009 20:40:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163586#M5413</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2009-03-19T20:40:58Z</dc:date>
    </item>
    <item>
      <title>Re: Linker Command File for MCF52277 - M52277EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163587#M5414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Service request submitted.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Chris.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2009 19:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linker-Command-File-for-MCF52277-M52277EVB/m-p/163587#M5414</guid>
      <dc:creator>cchilds</dc:creator>
      <dc:date>2009-03-23T19:14:47Z</dc:date>
    </item>
  </channel>
</rss>