<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem in executing CDC Demo Program in M52223EVB and CW 5.9.0 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-in-executing-CDC-Demo-Program-in-M52223EVB-and-CW-5-9-0/m-p/163535#M5406</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to transmit data between PC and M52223EVB via USB (J1 plug-in). I try to use cdc-demo in CMXUSB example program package. When I make the project I receive the following error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Link Error: Undefined: "_start"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For some reason I couldn't install Windows DDK to my PC with XP SP3. Is that the reason of the error? Is there a possibility that I can use CDC Demo without DDK?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Teoman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Dec 2009 20:46:27 GMT</pubDate>
    <dc:creator>K8Lxqg</dc:creator>
    <dc:date>2009-12-23T20:46:27Z</dc:date>
    <item>
      <title>Problem in executing CDC Demo Program in M52223EVB and CW 5.9.0</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-in-executing-CDC-Demo-Program-in-M52223EVB-and-CW-5-9-0/m-p/163535#M5406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to transmit data between PC and M52223EVB via USB (J1 plug-in). I try to use cdc-demo in CMXUSB example program package. When I make the project I receive the following error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Link Error: Undefined: "_start"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For some reason I couldn't install Windows DDK to my PC with XP SP3. Is that the reason of the error? Is there a possibility that I can use CDC Demo without DDK?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Teoman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Dec 2009 20:46:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-in-executing-CDC-Demo-Program-in-M52223EVB-and-CW-5-9-0/m-p/163535#M5406</guid>
      <dc:creator>K8Lxqg</dc:creator>
      <dc:date>2009-12-23T20:46:27Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in executing CDC Demo Program in M52223EVB and CW 5.9.0</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-in-executing-CDC-Demo-Program-in-M52223EVB-and-CW-5-9-0/m-p/163536#M5407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Wrong CW Version info sorry, I'm using CW 7.1.2&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 27 Dec 2009 22:03:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-in-executing-CDC-Demo-Program-in-M52223EVB-and-CW-5-9-0/m-p/163536#M5407</guid>
      <dc:creator>K8Lxqg</dc:creator>
      <dc:date>2009-12-27T22:03:38Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in executing CDC Demo Program in M52223EVB and CW 5.9.0</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-in-executing-CDC-Demo-Program-in-M52223EVB-and-CW-5-9-0/m-p/163537#M5408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you try the flash programmer utility for the mcf52223 MCU?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DDK utility is not needed to run CDC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Windows will ask for INF file provided with the ZIP as soon as USB device is recognized&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Probably the DDK you're referring to is the Windows Studio project that needs DDK to recompile the HID source code, which at runtime is not needed at all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Dec 2009 03:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-in-executing-CDC-Demo-Program-in-M52223EVB-and-CW-5-9-0/m-p/163537#M5408</guid>
      <dc:creator>PaoloRenzo</dc:creator>
      <dc:date>2009-12-29T03:00:37Z</dc:date>
    </item>
  </channel>
</rss>