<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: printf through usart in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/printf-through-usart/m-p/124100#M54</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;If you've created a sample project from the CodeWarrior Stationery, you should find that it has three build targets. The names are something like:&lt;BR /&gt;&lt;BR /&gt;M52233 DEMO Console Debug&lt;BR /&gt;M52233 DEMO UART Debug&lt;BR /&gt;M52233 DEMO Internal ROM&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;The first two of these targets are for quickly getting your code up and running. The debugger initialises the board for you and then downloads your code into RAM on the board.&lt;BR /&gt;&lt;BR /&gt;The final target builds the version where the application boots from Flash, which is what you'll need to do in the end. After building it, you need to 'burn' the code into the Flash memory on the board.&lt;BR /&gt;&lt;BR /&gt;To answer your question specifically, if you select the first target 'Console Debug', all I/O will appear in a Console Window on your PC. You need to choose the second target 'UART Debug' if you want I/O to be done via the UART (The third target also does this).&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Hope this helps&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Simon&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Feb 2007 18:29:55 GMT</pubDate>
    <dc:creator>SimonMarsden_de</dc:creator>
    <dc:date>2007-02-22T18:29:55Z</dc:date>
    <item>
      <title>printf through usart</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/printf-through-usart/m-p/124099#M53</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi every one,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am using the M52233DEMO board with codewarrior 6.3.&lt;/DIV&gt;&lt;DIV&gt;I have to access the USART via the printf() statement, but I don't succeed in redirect stdout.&lt;/DIV&gt;&lt;DIV&gt;The 'Console I/O' window appears with the text I have to transmit, but the terminal I use doesn't display this message. Does anyone know how to resolve this problem ?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2007 18:11:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/printf-through-usart/m-p/124099#M53</guid>
      <dc:creator>GP</dc:creator>
      <dc:date>2007-02-22T18:11:45Z</dc:date>
    </item>
    <item>
      <title>Re: printf through usart</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/printf-through-usart/m-p/124100#M54</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;If you've created a sample project from the CodeWarrior Stationery, you should find that it has three build targets. The names are something like:&lt;BR /&gt;&lt;BR /&gt;M52233 DEMO Console Debug&lt;BR /&gt;M52233 DEMO UART Debug&lt;BR /&gt;M52233 DEMO Internal ROM&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;The first two of these targets are for quickly getting your code up and running. The debugger initialises the board for you and then downloads your code into RAM on the board.&lt;BR /&gt;&lt;BR /&gt;The final target builds the version where the application boots from Flash, which is what you'll need to do in the end. After building it, you need to 'burn' the code into the Flash memory on the board.&lt;BR /&gt;&lt;BR /&gt;To answer your question specifically, if you select the first target 'Console Debug', all I/O will appear in a Console Window on your PC. You need to choose the second target 'UART Debug' if you want I/O to be done via the UART (The third target also does this).&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Hope this helps&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Simon&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2007 18:29:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/printf-through-usart/m-p/124100#M54</guid>
      <dc:creator>SimonMarsden_de</dc:creator>
      <dc:date>2007-02-22T18:29:55Z</dc:date>
    </item>
    <item>
      <title>Re: printf through usart</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/printf-through-usart/m-p/124101#M55</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Allright Simon, I understand now&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Many thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2007 17:10:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/printf-through-usart/m-p/124101#M55</guid>
      <dc:creator>GP</dc:creator>
      <dc:date>2007-03-02T17:10:38Z</dc:date>
    </item>
  </channel>
</rss>