<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: TWR-MCF5441X U-Boot Destroyed</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TWR-MCF5441X-U-Boot-Destroyed/m-p/162859#M5338</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Oops, forget that about U-Boot TFTP, the problems was with the host setup.&amp;nbsp; The host had two IP addresses, asking for TFTP to one IP address resulted in being given a socket on the other IP address.&amp;nbsp; My mistake.&amp;nbsp; Other TFTP clients could handle this, but not U-Boot, hence initially why I thought the problem was with U-Boot.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Jan 2014 01:38:24 GMT</pubDate>
    <dc:creator>yibbidy</dc:creator>
    <dc:date>2014-01-04T01:38:24Z</dc:date>
    <item>
      <title>TWR-MCF5441X U-Boot Destroyed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TWR-MCF5441X-U-Boot-Destroyed/m-p/162856#M5335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a TWR-MCF5441X and&amp;nbsp;did U-Boot upgrade in MRAM with:&lt;/P&gt;&lt;P&gt;-&amp;gt; set u-boot u-boot.bin&lt;/P&gt;&lt;P&gt;-&amp;gt; run upd&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But now it won't start up anymore.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have been trying to program U-Boot through the USB multilink&amp;nbsp;with the CFFlasher tool in the&amp;nbsp;M54418Tower_Linux_BSP_20110422_ltib, without any luck.&lt;/P&gt;&lt;P&gt;when running the commands:&lt;/P&gt;&lt;P&gt;C:\CFFlasher-nand&amp;gt;cf nand erase m54418twr_nand 0 80000&amp;nbsp;&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;C:\CFFlasher-nand&amp;gt;cf nand write m54418twr_nand 0 80000 1 flash_M54418TWR_uboot.bin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I get the message: Could not initialize BDM device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The following I already tried:&lt;/P&gt;&lt;P&gt;Running commands on win7 with CW 10.1 installed.&lt;/P&gt;&lt;P&gt;Running commands on winXP SP3 with CW 10.1 installed. (also virtual)&lt;/P&gt;&lt;P&gt;Running commands on winXP SP2 with CW 10.1 / 2.5 &amp;nbsp;and P&amp;amp;E version 10 drivers. installed&amp;nbsp;&lt;/P&gt;&lt;P&gt;Replacing unit_cfz.dll with other versions(from MQX and CW) and alse placing it in system32&lt;/P&gt;&lt;P&gt;Putting/Removing jumper on J10.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;All jumpers are on the default places. (j5 is on 3-4) SW1.1 is on ON&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm out of idea's, any help is appreciated.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Aug 2011 21:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TWR-MCF5441X-U-Boot-Destroyed/m-p/162856#M5335</guid>
      <dc:creator>Deleted</dc:creator>
      <dc:date>2011-08-29T21:21:39Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-MCF5441X U-Boot Destroyed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TWR-MCF5441X-U-Boot-Destroyed/m-p/162857#M5336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;﻿Solution:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="column"&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.000000pt; font-family: 'TTE1C4EF48t00';"&gt;Using CW10.1 to update U-boot for TWR-MCF5441X&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.000000pt; font-family: 'TTE55462C0t00';"&gt;Create a project with the project wizard for TWR-MCF5441X board and change the build configuration to TWR-MCF5441X_External_Flash&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.000000pt; font-family: 'TTE55462C0t00';"&gt;Launch Flash Programmer&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.000000pt; font-family: 'TTE55462C0t00';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.000000pt; font-family: 'TTE55462C0t00';"&gt;Use Flash File to Target and configure the Flash Programmer﻿&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.000000pt; font-family: 'TTE55462C0t00';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.000000pt; font-family: 'TTE55462C0t00';"&gt;The Flash Configuration file can be found from within “CW MCU v10.1\MCU\bin\plugins\support\TargetTask\Flash_Programmer\ColdFire”﻿&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.000000pt; font-family: 'TTE55462C0t00';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.000000pt; font-family: 'TTE55462C0t00';"&gt;Click Erase and Program to flash the U-boot to NAND Flash.﻿&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Sep 2011 04:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TWR-MCF5441X-U-Boot-Destroyed/m-p/162857#M5336</guid>
      <dc:creator>Deleted</dc:creator>
      <dc:date>2011-09-03T04:46:12Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-MCF5441X U-Boot Destroyed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TWR-MCF5441X-U-Boot-Destroyed/m-p/162858#M5337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for this solution.&amp;nbsp; I had the same problem and just used CW 10.2 to update to a newer U-Boot version.&amp;nbsp; For some reason the version that came with the TWR-MCF5441x board was not able to TFTP a file across.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Shaun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Dec 2013 07:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TWR-MCF5441X-U-Boot-Destroyed/m-p/162858#M5337</guid>
      <dc:creator>yibbidy</dc:creator>
      <dc:date>2013-12-26T07:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-MCF5441X U-Boot Destroyed</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TWR-MCF5441X-U-Boot-Destroyed/m-p/162859#M5338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Oops, forget that about U-Boot TFTP, the problems was with the host setup.&amp;nbsp; The host had two IP addresses, asking for TFTP to one IP address resulted in being given a socket on the other IP address.&amp;nbsp; My mistake.&amp;nbsp; Other TFTP clients could handle this, but not U-Boot, hence initially why I thought the problem was with U-Boot.&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Jan 2014 01:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/TWR-MCF5441X-U-Boot-Destroyed/m-p/162859#M5338</guid>
      <dc:creator>yibbidy</dc:creator>
      <dc:date>2014-01-04T01:38:24Z</dc:date>
    </item>
  </channel>
</rss>