<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: JM128 Pins not operating correctly</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/JM128-Pins-not-operating-correctly/m-p/162099#M5228</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;OK I found it...you were right...had some old code still stuck in there from the USB stack that was using the UART for talking to the terminal window I suppose...thanks again Rich&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 14 Mar 2009 02:27:30 GMT</pubDate>
    <dc:creator>ariclowe</dc:creator>
    <dc:date>2009-03-14T02:27:30Z</dc:date>
    <item>
      <title>JM128 Pins not operating correctly</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/JM128-Pins-not-operating-correctly/m-p/162096#M5225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Id appreciate any advice I can on a little problem Im experiencing with the JM128 chip.&amp;nbsp; Im currently interfacing to an external SRAM chip with the JM128.&amp;nbsp; The problem that Im having is when I set the address on the pins ( Most sig. byte port D, Mid sig. Port E, and least sig. byte Port F).&amp;nbsp; I need to use 3 ports to address 500K spaces.&amp;nbsp; The problem however is within Port E pins 0 and 1.&amp;nbsp; The rest of the pins are set correctly however Port E pin 0 is ALWAYS high, and Port E pin 1 sits at about 1.5 V regardless of what I set them at.&amp;nbsp; Obvisouly this posses a significant problem in addressing a specific memory address when two of the middle bits are consistently erraneous.&amp;nbsp; Im not using any of these pins for any other function of that this and have not enabled any serial communication that these two pins could potentially be used for.&amp;nbsp; Any thoughts out there from the great Freescale Masters??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Aric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Mar 2009 01:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/JM128-Pins-not-operating-correctly/m-p/162096#M5225</guid>
      <dc:creator>ariclowe</dc:creator>
      <dc:date>2009-03-14T01:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: JM128 Pins not operating correctly</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/JM128-Pins-not-operating-correctly/m-p/162097#M5226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you have uart (SPI) 1 configured somehow?&amp;nbsp; uart 1 shares those pins for its transmit and receive data.&amp;nbsp; Check register SPI1C1 and make sure bit 6 (SPE)&amp;nbsp;is a 0 (meaning the uart is not stealing pins pte0 and pte1), and then check your board to make sure you are not expecting a uart to be there -- on the demo boards you can typically remove a couple of jumpers to leave those pins alone.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-- Rich&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Mar 2009 01:27:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/JM128-Pins-not-operating-correctly/m-p/162097#M5226</guid>
      <dc:creator>RichTestardi</dc:creator>
      <dc:date>2009-03-14T01:27:38Z</dc:date>
    </item>
    <item>
      <title>Re: JM128 Pins not operating correctly</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/JM128-Pins-not-operating-correctly/m-p/162098#M5227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yeah I tried that already.&amp;nbsp; Removed the jumpers, and set SCI1C1_SPE to zero.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Mar 2009 02:01:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/JM128-Pins-not-operating-correctly/m-p/162098#M5227</guid>
      <dc:creator>ariclowe</dc:creator>
      <dc:date>2009-03-14T02:01:45Z</dc:date>
    </item>
    <item>
      <title>Re: JM128 Pins not operating correctly</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/JM128-Pins-not-operating-correctly/m-p/162099#M5228</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;OK I found it...you were right...had some old code still stuck in there from the USB stack that was using the UART for talking to the terminal window I suppose...thanks again Rich&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Mar 2009 02:27:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/JM128-Pins-not-operating-correctly/m-p/162099#M5228</guid>
      <dc:creator>ariclowe</dc:creator>
      <dc:date>2009-03-14T02:27:30Z</dc:date>
    </item>
  </channel>
</rss>