<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ext. MRAM vs Ext. SDRAM targets in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ext-MRAM-vs-Ext-SDRAM-targets/m-p/159462#M4934</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FB,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes... There are differences.&amp;nbsp; In theory the code should run just fine... once you have the SDRAM configured correctly the SDRAM controller in the 5282 will make the SDRAM look like 'RAM'.&amp;nbsp; You always need to make sure your linker correctly points the new memory mapped region.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MRAM, SRAM, etc...&amp;nbsp; Are non-mux'd simple linear memories.&amp;nbsp; SDRAMs require init code for the SDRAM itself and the controller inside the ColdFire or other microcontroller.&amp;nbsp; Look at an example codewarrior stationary for the 5282 board that you are using.&amp;nbsp; In that stationary should be some example code for the SDRAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Other places to look for init code:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF528X&amp;amp;nodeId=0162468rH3YTLC00M95448&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#" rel="nofollow" target="_blank"&gt;Try ColdFire Init.&lt;/A&gt;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;And the MCF5282 example code&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Link is &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF528X&amp;amp;nodeId=0162468rH3YTLC00M95448&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#" rel="nofollow" target="_blank"&gt;HERE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-JWW&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Mar 2009 23:09:26 GMT</pubDate>
    <dc:creator>JWW</dc:creator>
    <dc:date>2009-03-10T23:09:26Z</dc:date>
    <item>
      <title>Ext. MRAM vs Ext. SDRAM targets</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ext-MRAM-vs-Ext-SDRAM-targets/m-p/159461#M4933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to execute a program from the ext. SDRAM on the m5282evb.&amp;nbsp; THe program itself comes from the m52259evb which have an external MRAM target.&amp;nbsp; This program compiles and runs in the SRAM and in FLASH, but wjen it comes to ent SDRAM, it fails to execute. &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I execute a program intended to target ext MRAM when my RAM is different?&amp;nbsp; Is it the linker file that should be checked?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;SPAN&gt;Thx&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Mar 2009 04:08:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ext-MRAM-vs-Ext-SDRAM-targets/m-p/159461#M4933</guid>
      <dc:creator>francois_boucha</dc:creator>
      <dc:date>2009-03-07T04:08:05Z</dc:date>
    </item>
    <item>
      <title>Re: Ext. MRAM vs Ext. SDRAM targets</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ext-MRAM-vs-Ext-SDRAM-targets/m-p/159462#M4934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FB,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes... There are differences.&amp;nbsp; In theory the code should run just fine... once you have the SDRAM configured correctly the SDRAM controller in the 5282 will make the SDRAM look like 'RAM'.&amp;nbsp; You always need to make sure your linker correctly points the new memory mapped region.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;MRAM, SRAM, etc...&amp;nbsp; Are non-mux'd simple linear memories.&amp;nbsp; SDRAMs require init code for the SDRAM itself and the controller inside the ColdFire or other microcontroller.&amp;nbsp; Look at an example codewarrior stationary for the 5282 board that you are using.&amp;nbsp; In that stationary should be some example code for the SDRAM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Other places to look for init code:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF528X&amp;amp;nodeId=0162468rH3YTLC00M95448&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#" rel="nofollow" target="_blank"&gt;Try ColdFire Init.&lt;/A&gt;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;And the MCF5282 example code&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Link is &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF528X&amp;amp;nodeId=0162468rH3YTLC00M95448&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#" rel="nofollow" target="_blank"&gt;HERE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-JWW&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2009 23:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ext-MRAM-vs-Ext-SDRAM-targets/m-p/159462#M4934</guid>
      <dc:creator>JWW</dc:creator>
      <dc:date>2009-03-10T23:09:26Z</dc:date>
    </item>
  </channel>
</rss>