<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: invalid pointer in Freescale MAC?</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/invalid-pointer-in-Freescale-MAC/m-p/158848#M4868</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've just solved this problem, luckily. As I checked and rechecked the build configuration options, I noticed that I set parameter passing to "standard". If I set that one to "compact" (the My Wireless Application project uses that one), the stuff works all right.&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Richard&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Oct 2007 23:54:11 GMT</pubDate>
    <dc:creator>KRichard</dc:creator>
    <dc:date>2007-10-29T23:54:11Z</dc:date>
    <item>
      <title>invalid pointer in Freescale MAC?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/invalid-pointer-in-Freescale-MAC/m-p/158847#M4867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a problem, I use mcf5373 with Freescale MAC and our custom board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What I see is, when the binary MAC library calls my function, it calls it with an invalid pointer parameter, a pointer that points to 0x3FB2362A. I don't have anything there, I have flash at 0x0, SRAM at 0x80000000, SDRAM at 0x40000000. My other code works all right, so the board is usable and in working condition.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What might cause this?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance, have a nice weekend.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Richard&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 28 Oct 2007 02:48:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/invalid-pointer-in-Freescale-MAC/m-p/158847#M4867</guid>
      <dc:creator>KRichard</dc:creator>
      <dc:date>2007-10-28T02:48:06Z</dc:date>
    </item>
    <item>
      <title>Re: invalid pointer in Freescale MAC?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/invalid-pointer-in-Freescale-MAC/m-p/158848#M4868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I've just solved this problem, luckily. As I checked and rechecked the build configuration options, I noticed that I set parameter passing to "standard". If I set that one to "compact" (the My Wireless Application project uses that one), the stuff works all right.&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Richard&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Oct 2007 23:54:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/invalid-pointer-in-Freescale-MAC/m-p/158848#M4868</guid>
      <dc:creator>KRichard</dc:creator>
      <dc:date>2007-10-29T23:54:11Z</dc:date>
    </item>
  </channel>
</rss>