<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックV1 USB CDC Rx 64 byte msg (without locking up)?</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/V1-USB-CDC-Rx-64-byte-msg-without-locking-up/m-p/158150#M4793</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the JE256 ColdFire V1 part and codewarrior 6.3 to make used of the USB phcp demo for CDC.&lt;/P&gt;&lt;P&gt;We can successfully recieve 1 message over USB that is 64 bytes in length and then send and ACK which is 1 byte in length, after that the micro code continues to run, but no matter what I send from the PC to the mico I can't get theVirtual_Com_App function to see that a new message has been transmitted.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, Kerrie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Apr 2012 03:35:31 GMT</pubDate>
    <dc:creator>Kerrie</dc:creator>
    <dc:date>2012-04-27T03:35:31Z</dc:date>
    <item>
      <title>V1 USB CDC Rx 64 byte msg (without locking up)?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/V1-USB-CDC-Rx-64-byte-msg-without-locking-up/m-p/158150#M4793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the JE256 ColdFire V1 part and codewarrior 6.3 to make used of the USB phcp demo for CDC.&lt;/P&gt;&lt;P&gt;We can successfully recieve 1 message over USB that is 64 bytes in length and then send and ACK which is 1 byte in length, after that the micro code continues to run, but no matter what I send from the PC to the mico I can't get theVirtual_Com_App function to see that a new message has been transmitted.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks, Kerrie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2012 03:35:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/V1-USB-CDC-Rx-64-byte-msg-without-locking-up/m-p/158150#M4793</guid>
      <dc:creator>Kerrie</dc:creator>
      <dc:date>2012-04-27T03:35:31Z</dc:date>
    </item>
    <item>
      <title>Re: V1 USB CDC Rx 64 byte msg (without locking up)?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/V1-USB-CDC-Rx-64-byte-msg-without-locking-up/m-p/158151#M4794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Bump,&amp;nbsp; anyone have any ideas.....&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2012 00:22:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/V1-USB-CDC-Rx-64-byte-msg-without-locking-up/m-p/158151#M4794</guid>
      <dc:creator>Kerrie</dc:creator>
      <dc:date>2012-05-03T00:22:09Z</dc:date>
    </item>
  </channel>
</rss>