<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: About MCF5482 SPI to USB solution in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MCF5482-SPI-to-USB-solution/m-p/158121#M4788</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The DSPI module on MCF54xx can attain up to 25MHz and also you can use the eDMA module to reduce CPU load, I think with 26MHz SPI on MAX3421, it can satisfy the requirements for USB 12Mbps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By the way, you are not supposed to attain 12Mbps any way, it's just&amp;nbsp;a theoratical value.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Mar 2009 11:14:46 GMT</pubDate>
    <dc:creator>cutworth</dc:creator>
    <dc:date>2009-03-06T11:14:46Z</dc:date>
    <item>
      <title>About MCF5482 SPI to USB solution</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MCF5482-SPI-to-USB-solution/m-p/158120#M4787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to connect a USB host to my MCF5482 platform via a MAX3421, the interface is SPI, the MAX3421 support spi clk up to 26M, and suport full speed USB host 12M bps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any one used MCF54xx like this? I want to know how fast it is up to, I think it is impossible to reach 12M bps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2009 16:51:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MCF5482-SPI-to-USB-solution/m-p/158120#M4787</guid>
      <dc:creator>Jason_Shi</dc:creator>
      <dc:date>2009-03-03T16:51:44Z</dc:date>
    </item>
    <item>
      <title>Re: About MCF5482 SPI to USB solution</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MCF5482-SPI-to-USB-solution/m-p/158121#M4788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The DSPI module on MCF54xx can attain up to 25MHz and also you can use the eDMA module to reduce CPU load, I think with 26MHz SPI on MAX3421, it can satisfy the requirements for USB 12Mbps.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By the way, you are not supposed to attain 12Mbps any way, it's just&amp;nbsp;a theoratical value.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2009 11:14:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MCF5482-SPI-to-USB-solution/m-p/158121#M4788</guid>
      <dc:creator>cutworth</dc:creator>
      <dc:date>2009-03-06T11:14:46Z</dc:date>
    </item>
  </channel>
</rss>