<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ColdFire MCF52233DEMO in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ColdFire-MCF52233DEMO/m-p/157659#M4735</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please help me. Am using MCF52233 Demo&amp;nbsp; board from freescale on that am using Ethernet Peripheral to send send transmitt the data to client. But am facing a problem that, am using the readymade code which given by freescale which the freescale demo board. The code was generated by interniche technologies in that if i made any changes in the code that is not been&amp;nbsp; reflecting in the .s19 file. Can you tell me please how to generate .s19 file from the changed code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 28 Feb 2009 17:57:50 GMT</pubDate>
    <dc:creator>smruti</dc:creator>
    <dc:date>2009-02-28T17:57:50Z</dc:date>
    <item>
      <title>ColdFire MCF52233DEMO</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ColdFire-MCF52233DEMO/m-p/157659#M4735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you please help me. Am using MCF52233 Demo&amp;nbsp; board from freescale on that am using Ethernet Peripheral to send send transmitt the data to client. But am facing a problem that, am using the readymade code which given by freescale which the freescale demo board. The code was generated by interniche technologies in that if i made any changes in the code that is not been&amp;nbsp; reflecting in the .s19 file. Can you tell me please how to generate .s19 file from the changed code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 28 Feb 2009 17:57:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ColdFire-MCF52233DEMO/m-p/157659#M4735</guid>
      <dc:creator>smruti</dc:creator>
      <dc:date>2009-02-28T17:57:50Z</dc:date>
    </item>
    <item>
      <title>Re: ColdFire MCF52233DEMO</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ColdFire-MCF52233DEMO/m-p/157660#M4736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; Although I am not familiar with 52233 demo board, I have been working with M52235EVB&lt;BR /&gt;&amp;nbsp; and I guess the projects are very similar.&lt;BR /&gt;&amp;nbsp; The example codes always include a complete S19 file so that you can load it&lt;BR /&gt;&amp;nbsp; with the Codewarrior Flasher if this file exceeds the limitations of a codewarrior&lt;BR /&gt;&amp;nbsp; test licence. I will call this S19 file, back up S19.&lt;BR /&gt;&amp;nbsp; What I am trying to say is that if you change the code and compile it, the back up&lt;BR /&gt;&amp;nbsp; file will never change, but there will be into the folders of the project another&lt;BR /&gt;&amp;nbsp; S19 file which is changing. Just make a search for S19 files into the project folders&lt;BR /&gt;&amp;nbsp; and I am almost sure you will find it.&lt;BR /&gt;&amp;nbsp; What are you using to load your code into the demo board?&lt;BR /&gt;&amp;nbsp; Is it codewarrior flash programmer?&lt;BR /&gt;&amp;nbsp; or is it Cold Fire Flasher(an application to load without Codewarrior)?&lt;BR /&gt;&amp;nbsp; If it is the Cold Fire flasher, now you just have to select the correct S19 file.&lt;BR /&gt;&amp;nbsp; Now if you are using codewarrior, then there are some mistakes when trying to load&lt;BR /&gt;&amp;nbsp; the file which result in never loading a file and running the application the board&lt;BR /&gt;&amp;nbsp; already has.&lt;BR /&gt;&amp;nbsp; In order to correctly flash a board you must click in TOOLS-&amp;gt;Flash Programmer, then&lt;BR /&gt;&amp;nbsp; you must select the right settings, you can load them clicking on load settings button.&lt;BR /&gt;&amp;nbsp; Then first erase the flash memory, then select the correct S19 file (not the back up)&lt;BR /&gt;&amp;nbsp; and finally click into the program button. If program command succeded, you will see a message.&lt;BR /&gt;&amp;nbsp; Reset the board to run the new program.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2009 22:38:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ColdFire-MCF52233DEMO/m-p/157660#M4736</guid>
      <dc:creator>JaimeR</dc:creator>
      <dc:date>2009-03-10T22:38:14Z</dc:date>
    </item>
  </channel>
</rss>