<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: MCF52259 PAD control registers&amp;bits.</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-PAD-control-registers-bits/m-p/156727#M4642</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mr bean&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, the M52259 (and its doc) is very new and there are a few places which are not correct.&lt;/P&gt;&lt;P&gt;I have found the best way to check is to connect with the debugger using CodeWarrior V7.1.1 and expand the registers using "View registers" - these are usually very accurate.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The pad control register section is the one to go by and not Table 2-1 - &lt;EM&gt;this requires some work before it can be used as definitive reference&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Feb 2009 06:54:22 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2009-02-27T06:54:22Z</dc:date>
    <item>
      <title>MCF52259 PAD control registers&amp;bits.</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-PAD-control-registers-bits/m-p/156726#M4641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MCF52259RM is a mess regarding PSRR and PDSR registers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Table 2-1 shows :&lt;/P&gt;&lt;P&gt;&amp;nbsp;28 bits of PDSR&lt;/P&gt;&lt;P&gt;&amp;nbsp;8 bits Pin wired-OR control.&lt;/P&gt;&lt;P&gt;&amp;nbsp;No Slew rate control.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Figure 15-1 page 15-5 shows :&lt;/P&gt;&lt;P&gt;&amp;nbsp;80 bits of PSRR (PSRR 0x10_0078, PSRRL 010_0080, PSRRH 0x10_0086)&lt;/P&gt;&lt;P&gt;&amp;nbsp;80 bits of PDSR (PDSR 0x10_007C, PDSRL 010_0088, PDSRH 0x10_008E)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paragraph 15.6.6 shows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;Reference to table 2-1. Alas most bits are not in there so one can only guess which bit controls which pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;PSRR is gone.&amp;nbsp;PSRRL has suddenly moved to 010_0078.&lt;/P&gt;&lt;P&gt;&amp;nbsp;PDSR also gone.&amp;nbsp;PDSRL *and* PDSRH have both suddenly moved to 0x10_007C.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;----------------&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;I'd like to know how they really work.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Can anyone tell me please ?&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Feb 2009 21:43:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-PAD-control-registers-bits/m-p/156726#M4641</guid>
      <dc:creator>MrBean</dc:creator>
      <dc:date>2009-02-26T21:43:52Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52259 PAD control registers&amp;bits.</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-PAD-control-registers-bits/m-p/156727#M4642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mr bean&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, the M52259 (and its doc) is very new and there are a few places which are not correct.&lt;/P&gt;&lt;P&gt;I have found the best way to check is to connect with the debugger using CodeWarrior V7.1.1 and expand the registers using "View registers" - these are usually very accurate.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The pad control register section is the one to go by and not Table 2-1 - &lt;EM&gt;this requires some work before it can be used as definitive reference&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2009 06:54:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52259-PAD-control-registers-bits/m-p/156727#M4642</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-02-27T06:54:22Z</dc:date>
    </item>
  </channel>
</rss>