<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: MCF5223x PWOR function ?</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5223x-PWOR-function/m-p/156701#M4633</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mr Bean&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I haven't used this function but I believe it is effectively setting open drain output so that several outputs can be connected together. Using a pull-up, any output driving '0' 'wins'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wired-OR is a little confusing because sometimes it is also called Wire-AND. See the following: &lt;A href="http://zone.ni.com/devzone/cda/tut/p/id/3544" rel="nofollow" target="_blank"&gt;Wired-OR&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Feb 2009 06:42:45 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2009-02-27T06:42:45Z</dc:date>
    <item>
      <title>MCF5223x PWOR function ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5223x-PWOR-function/m-p/156700#M4632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The PWOR bits set pins to "wired-OR".&lt;/P&gt;&lt;P&gt;There is no further explanation in the RM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know what it does ?&lt;/P&gt;&lt;P&gt;Does it disable the low side driver transistor of the pin ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Feb 2009 21:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5223x-PWOR-function/m-p/156700#M4632</guid>
      <dc:creator>MrBean</dc:creator>
      <dc:date>2009-02-26T21:28:17Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5223x PWOR function ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5223x-PWOR-function/m-p/156701#M4633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mr Bean&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I haven't used this function but I believe it is effectively setting open drain output so that several outputs can be connected together. Using a pull-up, any output driving '0' 'wins'.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wired-OR is a little confusing because sometimes it is also called Wire-AND. See the following: &lt;A href="http://zone.ni.com/devzone/cda/tut/p/id/3544" rel="nofollow" target="_blank"&gt;Wired-OR&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2009 06:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5223x-PWOR-function/m-p/156701#M4633</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-02-27T06:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5223x PWOR function ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5223x-PWOR-function/m-p/156702#M4634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yes, I think it is what is normally called open-drain output. I haven't tried it though.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2009 21:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5223x-PWOR-function/m-p/156702#M4634</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2009-02-27T21:02:34Z</dc:date>
    </item>
  </channel>
</rss>