<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic m52233DEMo and WDT in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/m52233DEMo-and-WDT/m-p/156314#M4561</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Can anyone explain how to enable and use the WDT on a the M52233DEMO?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 May 2008 02:22:09 GMT</pubDate>
    <dc:creator>WOLF</dc:creator>
    <dc:date>2008-05-16T02:22:09Z</dc:date>
    <item>
      <title>m52233DEMo and WDT</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/m52233DEMo-and-WDT/m-p/156314#M4561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Can anyone explain how to enable and use the WDT on a the M52233DEMO?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2008 02:22:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/m52233DEMo-and-WDT/m-p/156314#M4561</guid>
      <dc:creator>WOLF</dc:creator>
      <dc:date>2008-05-16T02:22:09Z</dc:date>
    </item>
    <item>
      <title>Re: m52233DEMo and WDT</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/m52233DEMo-and-WDT/m-p/156315#M4562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Wolf&lt;BR /&gt;&lt;BR /&gt;The M52233 has a core watchdog timer which can be disabled (writing 0 to CWCR) or programmed to generate an interrupt when it times out. Eg (with 2s timeout at 60MHz PLL):&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;#define WATCHDOG_2_SEC&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x30&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // about 2 seconds at 60MHz bus&lt;BR /&gt;CWCR = (CWE | WATCHDOG_2_SEC | CWTA | CWTAVA | CWTIF); // activate watchdog&lt;BR /&gt;fnSetIntHandler(SW_WD_VECTOR, (unsigned char *)_sw_wdog_timeout); // enter watchdog interruot&lt;BR /&gt;IC_ICR_0_8 = (INTERRUPT_LEVEL_7 | INTERRUPT_PRIORITY_7);&lt;BR /&gt;IC_IMRL_0 &amp;amp;= ~(SW_WDG_PIF_INT_L | MASK_ALL_INT);&amp;nbsp; // enable wacthdog interrupt&lt;BR /&gt;&lt;BR /&gt;Note that the watchdog can not generate a reset directly so the interrupt is set to highest level, non-maskable so that it has highest chance of being able to operate.&lt;BR /&gt;&lt;BR /&gt;To generate a reset when the watchdog fires, and its interrupt (_sw_wdog_timeout()) is called, the following can be performed:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; RESET_RCR = SOFT_RST;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // command a soft reset of the board&lt;BR /&gt;&lt;BR /&gt;To stop the watchdog from firing it must be regularly reset by using the following feed sequence:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CWSR = 0x55;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // retrigger the software watchdog&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CWSR = 0xaa;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // using this two byte sequence&lt;BR /&gt;&lt;BR /&gt;Note that the watchdog should not be enabled when debugging since it fires when single stepping and causes loss of debugger control.&lt;BR /&gt;&lt;BR /&gt;There are several other discussions about the pros and cons of the watchdog timer in the forum (eg. &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=2759&amp;amp;query.id=49225#M2759" target="_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&amp;amp;message.id=2759&amp;amp;query.id=49225#M2759)&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Note that other parts, like the M52213 include a second watchdog called the Background Watchdog Timer, which is capable of directly generating a warm reset on underflow - this allows more reliable protection against SW errors.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 May 2008 03:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/m52233DEMo-and-WDT/m-p/156315#M4562</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2008-05-17T03:18:58Z</dc:date>
    </item>
  </channel>
</rss>