<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: Linux BSP for the M54455 Eval Board</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155086#M4395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Hi Gkahn,&lt;/DIV&gt;&lt;DIV&gt;It would be in the same directory as the "ltib" perl script and it gets generated when you first run the ./ltib without any parameters and is named&amp;nbsp;"host_config.log".&lt;/DIV&gt;&lt;DIV&gt;So in summary, as root you mount the iso.&amp;nbsp; As a user you run the "./install" and follow the instructions and mostly use the default settings BUT be careful for where it ask you to install ltib.&amp;nbsp; It defaults to the mount point.&amp;nbsp; I usually point it to my user log in directory (ex: /home/david).&lt;/DIV&gt;&lt;DIV&gt;After the install process has happened, change directory to your install location (ex: /home/david/ltib-mcf547x_8x-20070107) and make sure that the first thing you do is run " ./ltib" without any parameters.&lt;/DIV&gt;&lt;DIV&gt;While ltib is running for the first time, it creates the "host_config.log".file.&amp;nbsp; So from another terminal window I change directory to the ltib root directory (ex: /home/david/ltib-mcf547x_8x-20070107)&amp;nbsp;and execute a "tail host_config.log" a few time to see that additional information is be added and that the "./ltib" is running.&amp;nbsp; This first run of ./ltib can take 10 minutes or so.&lt;/DIV&gt;&lt;DIV&gt;After the initial run you should have a complete "host_config.log". file.&amp;nbsp; I've attached mine as reference named "host_config..zip".&lt;/DIV&gt;&lt;DIV&gt;After the initial run of ltib has occured then you run "./ltib -c" to go thru the build process.&amp;nbsp; I usually selected to config the kernel and leave kernel source code but otherwise do not touch anything else just to see that all is running OK.&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;David&lt;/DIV&gt;&lt;DIV&gt;PS&lt;/DIV&gt;&lt;DIV&gt;In the root directory of the mounted iso, open the START_HERE.htm web page as it has great help within it.&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Nov 2007 04:38:59 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2007-11-04T04:38:59Z</dc:date>
    <item>
      <title>Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155079#M4388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm having a small problem getting the BSP for the M54455 Eval board to build.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have the default packages as provided by Freescale and even cracked open&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;a /opt/freescale directory to install into. The problem appears to be that the&lt;/SPAN&gt;&lt;BR /&gt;&lt;I&gt;rpmbuild&lt;/I&gt;&lt;SPAN&gt; routing (which is reading the spec file from the dist directory) cannot&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;find the source files in the pkgs directory. I have altered paths in the &lt;/SPAN&gt;&lt;I&gt;ltib&lt;/I&gt;&lt;SPAN&gt; script&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;but nothing seems to work. I have verified that the package(s) in question are&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;in the &lt;/SPAN&gt;&lt;I&gt;pkgs&lt;/I&gt;&lt;SPAN&gt; directory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am a native Linux user, but this is the first time I've worked with &lt;/SPAN&gt;&lt;I&gt;ltib&lt;/I&gt;&lt;SPAN&gt;. I will keep&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;working on this, but I would greatly appreciate any help or insight you could provide.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank You.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;------------- log file ---------------------------------&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Installing host support packages.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This only needs to be done once per host, but may take up to&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;an hour to complete ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If an error occurs, a log file with the full output may be found in:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/opt/freescale/ltib/host_config.log&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Exiting on error or interrupt&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please see &amp;gt;&amp;gt; /opt/freescale/ltib/host_config.log for details&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Processing platform: Native Linux support&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;===========================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;using&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Processing: rpm-fs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;====================&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/usr/bin/rpmbuild --dbpath /tmp/rpm-user/rpmdb --define '_unpackaged_files_terminate_build 0' --define '_target_cpu i686' --define '__strip strip' --define '_topdir /tmp/rpm-user' --define '_prefix /opt/freescale/ltib/usr' --define '_tmppath /tmp' --define '_mandir /opt/freescale/ltib/usr/share/man' --define '_sysconfdir /opt/freescale/ltib/etc' --define '_localstatedir /var' -bb&amp;nbsp; --clean --rmsource&amp;nbsp; /opt/freescale/ltib/dist/lfs-5.1/rpm/rpm-fs.spec&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;error: File ./rpm-4.0.4.tar.gz: No such file or directory&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Build time for rpm-fs: 0 seconds&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Failed building rpm-fs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Died at ltib line 1999.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Started: Fri Oct 12 15:39:51 2007&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ended:&amp;nbsp;&amp;nbsp; Fri Oct 12 15:39:52 2007&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Elapsed: 1 seconds&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;These packages failed to build:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;rpm-fs&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Build Failed&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;I&gt;&lt;/I&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Oct 2007 02:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155079#M4388</guid>
      <dc:creator>Gkahn</dc:creator>
      <dc:date>2007-10-13T02:42:51Z</dc:date>
    </item>
    <item>
      <title>Re: Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155080#M4389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Gkahn,&lt;/DIV&gt;&lt;DIV&gt;I've installed LTIB many times and have also removed and re-installed many times so have a success and failures.&amp;nbsp; Luckily more success than failures.&lt;/DIV&gt;&lt;DIV&gt;After I mount the iso as root and cd to the mnt directory, make sure you are non-root for the rest of the install process.&lt;/DIV&gt;&lt;DIV&gt;Next I use all of the defaults except for the install directory.&amp;nbsp; I change it to "/home/user" and do not install it to the "/opt" directory.&lt;/DIV&gt;&lt;DIV&gt;Once the install script completes, cd to your "/home/user/ltib-mcf5445x-20071001" directory.&lt;/DIV&gt;&lt;DIV&gt;Make sure as non-root to run "./ltib" all by itself.&lt;/DIV&gt;&lt;DIV&gt;After hopefully the success run of it just this first time, run "./ltib -c" to get the default setup to run/build.&lt;/DIV&gt;&lt;DIV&gt;If I mess up I just delete the LTIB and /opt/freescale directories and start over.&lt;/DIV&gt;&lt;DIV&gt;Hopefully this works/helps.&lt;/DIV&gt;&lt;DIV&gt;I've used FC5 and openSUSE10.1 recently.&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;David&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2007 03:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155080#M4389</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2007-10-17T03:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155081#M4390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for your reply David,&lt;BR /&gt;I'm a little worried now, I've tried all the steps you mentioned&lt;BR /&gt;without any success. I'm using Fedora 7, but tried FC5 with&lt;BR /&gt;the same results.&lt;BR /&gt;When your build failed, did you get a similar error??&lt;BR /&gt;I'll clean out everything and start fresh again.&lt;BR /&gt;&lt;BR /&gt;Thanks again.&lt;BR /&gt;&lt;BR /&gt;Gkahn&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2007 04:05:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155081#M4390</guid>
      <dc:creator>Gkahn</dc:creator>
      <dc:date>2007-10-17T04:05:42Z</dc:date>
    </item>
    <item>
      <title>Re: Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155082#M4391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Gkahn,&lt;/DIV&gt;&lt;DIV&gt;The team that build/integrate and test the LTIB try to do it on multiple distributions: RH7/9, FC4-6, and maybe another that doesn't come to mind.&amp;nbsp; As mentioned I've done it on openSUSE10.1.&lt;/DIV&gt;&lt;DIV&gt;FC7 is too new for them to have tested with yet.&lt;/DIV&gt;&lt;DIV&gt;I haven't seen the specific error you mention.&lt;/DIV&gt;&lt;DIV&gt;Sorry you have the issue but please let me know how the delete and re-install goes.&lt;/DIV&gt;&lt;DIV&gt;I'm using VMware Workstation so if I have too I can download FC7 and give it a try but I'll wait to see if you have success.&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;David&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Oct 2007 22:45:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155082#M4391</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2007-10-17T22:45:23Z</dc:date>
    </item>
    <item>
      <title>Re: Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155083#M4392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;David,&lt;BR /&gt;Well I scraped the install again and tried reinstalling and building under Fedora 7. No luck, same results.&lt;BR /&gt;I scraped again and reinstalled, this time I built under F5. Except for a problem with the temp directory,&lt;BR /&gt;it seems to be building. So there seems to be an issue with Fedora 7 or something in my environment.&lt;BR /&gt;I'm hoping that once I get through the first build, I can use my native Fedora 7 environment to do the&lt;BR /&gt;subsequent work, if not, I still have a path forward. Perhaps it's time to dig out that old FC5 Live-CD.&lt;BR /&gt;&lt;BR /&gt;Thanks again for your help.&lt;BR /&gt;Gkahn.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Oct 2007 00:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155083#M4392</guid>
      <dc:creator>Gkahn</dc:creator>
      <dc:date>2007-10-18T00:41:54Z</dc:date>
    </item>
    <item>
      <title>Re: Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155084#M4393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Can you post your host_config.log file from a fresh install from the ISO (as is, as a normal user)?&lt;BR /&gt;&lt;BR /&gt;-mnorman&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Nov 2007 00:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155084#M4393</guid>
      <dc:creator>mnorman</dc:creator>
      <dc:date>2007-11-02T00:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155085#M4394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I reinstalled into a clean directory but there doesn't appear to be any file with this name,&lt;BR /&gt;anywhere in the install branch. In fact, no file of this&amp;nbsp; name exists anywhere on my&lt;BR /&gt;machine. Do I need to set an option or environmental to get this file???&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;BR /&gt;&lt;BR /&gt;Gkahn&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Nov 2007 22:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155085#M4394</guid>
      <dc:creator>Gkahn</dc:creator>
      <dc:date>2007-11-02T22:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155086#M4395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;Hi Gkahn,&lt;/DIV&gt;&lt;DIV&gt;It would be in the same directory as the "ltib" perl script and it gets generated when you first run the ./ltib without any parameters and is named&amp;nbsp;"host_config.log".&lt;/DIV&gt;&lt;DIV&gt;So in summary, as root you mount the iso.&amp;nbsp; As a user you run the "./install" and follow the instructions and mostly use the default settings BUT be careful for where it ask you to install ltib.&amp;nbsp; It defaults to the mount point.&amp;nbsp; I usually point it to my user log in directory (ex: /home/david).&lt;/DIV&gt;&lt;DIV&gt;After the install process has happened, change directory to your install location (ex: /home/david/ltib-mcf547x_8x-20070107) and make sure that the first thing you do is run " ./ltib" without any parameters.&lt;/DIV&gt;&lt;DIV&gt;While ltib is running for the first time, it creates the "host_config.log".file.&amp;nbsp; So from another terminal window I change directory to the ltib root directory (ex: /home/david/ltib-mcf547x_8x-20070107)&amp;nbsp;and execute a "tail host_config.log" a few time to see that additional information is be added and that the "./ltib" is running.&amp;nbsp; This first run of ./ltib can take 10 minutes or so.&lt;/DIV&gt;&lt;DIV&gt;After the initial run you should have a complete "host_config.log". file.&amp;nbsp; I've attached mine as reference named "host_config..zip".&lt;/DIV&gt;&lt;DIV&gt;After the initial run of ltib has occured then you run "./ltib -c" to go thru the build process.&amp;nbsp; I usually selected to config the kernel and leave kernel source code but otherwise do not touch anything else just to see that all is running OK.&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;David&lt;/DIV&gt;&lt;DIV&gt;PS&lt;/DIV&gt;&lt;DIV&gt;In the root directory of the mounted iso, open the START_HERE.htm web page as it has great help within it.&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Nov 2007 04:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155086#M4395</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2007-11-04T04:38:59Z</dc:date>
    </item>
    <item>
      <title>Re: Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155087#M4396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Well, did a clean install and ran ltib.....&lt;BR /&gt;this time it seems to have completed. I don't know&lt;BR /&gt;what the exact difference is but I have installed a&lt;BR /&gt;couple updates since I first tried this. I'll include the&lt;BR /&gt;host_config.log file but I think it's working now.&lt;BR /&gt;I'll try it again in a real work directory.&lt;BR /&gt;&lt;BR /&gt;Gkahn&lt;BR /&gt;&lt;BR /&gt;P.S. sorry for the delay, I'm bouncing between a few&lt;BR /&gt;different projects.&lt;BR /&gt;&lt;BR /&gt;++++++++++++++++++++++++++++++++++++++++++++++++++++&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Updating lpp from local packages&lt;BR /&gt;Use of uninitialized value in scalar assignment at ./ltib line 1363.&lt;BR /&gt;&lt;BR /&gt;Processing platform: Host support packages&lt;BR /&gt;============================================&lt;BR /&gt;using test2/ltib-mcf5445x-20071001/config/platform/host/ltib.preconfig&lt;BR /&gt;&lt;BR /&gt;Processing: fake-provides&lt;BR /&gt;===========================&lt;BR /&gt;&lt;BR /&gt;Processing: mkspooflinks&lt;BR /&gt;==========================&lt;BR /&gt;&lt;BR /&gt;Processing: bison&lt;BR /&gt;===================&lt;BR /&gt;&lt;BR /&gt;Processing: flex&lt;BR /&gt;==================&lt;BR /&gt;&lt;BR /&gt;Processing: texinfo&lt;BR /&gt;=====================&lt;BR /&gt;&lt;BR /&gt;Processing: autoconf&lt;BR /&gt;======================&lt;BR /&gt;&lt;BR /&gt;Processing: libtool&lt;BR /&gt;=====================&lt;BR /&gt;&lt;BR /&gt;Processing: lkc&lt;BR /&gt;=================&lt;BR /&gt;&lt;BR /&gt;Processing: wget&lt;BR /&gt;==================&lt;BR /&gt;&lt;BR /&gt;Processing: uclinux-cksum&lt;BR /&gt;===========================&lt;BR /&gt;&lt;BR /&gt;Processing: genext2fs&lt;BR /&gt;=======================&lt;BR /&gt;&lt;BR /&gt;Processing: genromfs&lt;BR /&gt;======================&lt;BR /&gt;&lt;BR /&gt;Processing: u-boot-tools&lt;BR /&gt;==========================&lt;BR /&gt;&lt;BR /&gt;Processing: mtd-utils&lt;BR /&gt;=======================&lt;BR /&gt;&lt;BR /&gt;Processing: pkgconfig&lt;BR /&gt;=======================&lt;BR /&gt;&lt;BR /&gt;Processing: dtc&lt;BR /&gt;=================&lt;BR /&gt;&lt;BR /&gt;Processing: cramfs&lt;BR /&gt;====================&lt;BR /&gt;&lt;BR /&gt;Processing: distcc&lt;BR /&gt;====================&lt;BR /&gt;&lt;BR /&gt;Processing: unifdef&lt;BR /&gt;=====================&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Nov 2007 06:17:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155087#M4396</guid>
      <dc:creator>Gkahn</dc:creator>
      <dc:date>2007-11-08T06:17:29Z</dc:date>
    </item>
    <item>
      <title>Re: Linux BSP for the M54455 Eval Board</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155088#M4397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;rm -R /tmp/rpm-dan&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;allowed me to continue, thanks arnoox!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Apr 2011 04:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-BSP-for-the-M54455-Eval-Board/m-p/155088#M4397</guid>
      <dc:creator>dantebbs</dc:creator>
      <dc:date>2011-04-02T04:48:20Z</dc:date>
    </item>
  </channel>
</rss>