<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Ethernet With ColdFire V2</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154026#M4269</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;EM&gt;&amp;gt;&amp;gt;I was wondering how you and other users handle the GPL license&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;The FNET stack is LGPL.&lt;/P&gt;&lt;P&gt;&amp;gt;It means, that ONLY changes/fixes in the FNET stack source code should be shared with community, what is pretty fair.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes that is fair. RTEMS is the same but does not use or accept LGPL code. The demands on the user is too much.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;You should&amp;nbsp;NOT open your proprietary code and you may use LGPL with any other license code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As long as you provide access to the closed source object modules so an end users can use a new version of FNET, link it to the object modules and create a new version of the software. Being able to&amp;nbsp;practically do this is not important.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;(If you still need a special exception clause, it can be added).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have found in RTEMS this is the best solution. We use GCC's libgcc license. It does not make sense to rebuild software for an embedded system this way and shared libraries (or DLL) type technology is not used how-ever the users of the code still need to provide the ability to relink the application no matter how difficult.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;One additional bonus: LGPL is compatible with GPL, so you can use FNET in GPL projects too (LGPL automatically &amp;gt;converted to GPL). Many people do not know about this LGPL feature ,that is why FNET is dual licensed. So you can &amp;gt;choose what license to choose in your project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The libgcc license is the same. We all want users to contribute patches and new features back to the project.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Nov 2010 05:02:23 GMT</pubDate>
    <dc:creator>ChrisJohns</dc:creator>
    <dc:date>2010-11-05T05:02:23Z</dc:date>
    <item>
      <title>Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154016#M4259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i am just starting with ethernet on ColdFire. Is there any documentation about the C functions to deal with the ethernet port? Is it possible to use it with no OS? I got the example with NicheLite but if i understood correctly it is running with a OS. Do you know if i will need a OS to use NicheLite Stack? How about using the WebServer? After installing the CodeWarrior, where are praced the ethernet functions?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;OFFTOPIC (I CHOSE THIS ALIS BY MISTAKE... IS THERE ANY WAY TO CHANGE IT?????)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Oct 2010 20:33:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154016#M4259</guid>
      <dc:creator>EthernetHelp</dc:creator>
      <dc:date>2010-10-08T20:33:30Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154017#M4260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Maybe look into FNET, I believe it runs without OS.&lt;/P&gt;&lt;P&gt;&lt;A __default_attr="57196" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/57196" jivemacro="thread" title="https://community.freescale.com/thread/57196"&gt;https://community.freescale.com/thread/57196&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Oct 2010 15:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154017#M4260</guid>
      <dc:creator>vier_kuifjes</dc:creator>
      <dc:date>2010-10-10T15:13:46Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154018#M4261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey, thank you, that might help a lot. Any experience with that stack? Is it reliable? Any further comment? ç&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And back to NicheLite, is it possible to use it with no OS?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PS: Is there any way to change my nick at this forum?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Oct 2010 14:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154018#M4261</guid>
      <dc:creator>EthernetHelp</dc:creator>
      <dc:date>2010-10-11T14:26:16Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154019#M4262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think it can be done with NicheLite, although I'm not 100% positive.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Maybe send a message to "butok", the author of FNET. I think he is very responsive.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Oct 2010 17:41:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154019#M4262</guid>
      <dc:creator>vier_kuifjes</dc:creator>
      <dc:date>2010-10-11T17:41:47Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154020#M4263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To answer your other question: No, there is not an easy way to change your nickname in this forum. This is something I have been working on for a long time to change and have not got anywhere yet.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Oct 2010 20:05:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154020#M4263</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-10-11T20:05:08Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154021#M4264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Haha ok, so i will have to live with this nick ... Thank you anyway!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Oct 2010 15:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154021#M4264</guid>
      <dc:creator>EthernetHelp</dc:creator>
      <dc:date>2010-10-14T15:46:40Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154022#M4265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"Any experience with that stack? Is it reliable? Any further comment?"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding FNET, I'd like to add that I tried several stacks (MQX, uIP and lwIP) and this one actually turned out to be the most reliable of them. Havent had any problems with it so far (whereas the other stacks didnt survive a few quick reload clicks in the browser with the demo projects running).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;Sven&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Oct 2010 21:50:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154022#M4265</guid>
      <dc:creator>Kopone</dc:creator>
      <dc:date>2010-10-28T21:50:19Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154023#M4266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;Kopone wrote:&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regarding FNET, I'd like to add that I tried several stacks (MQX, uIP and lwIP) and this one actually turned out to be the most reliable of them. Havent had any problems with it so far (whereas the other stacks didnt survive a few quick reload clicks in the browser with the demo projects running).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Well, having used the lwIP stack extensively on various MCU's including ColdFire v2 I can say that it is reliable. Maybe you are referring to the quality of the particular ports that you tried out, as those may vary greatly. No-one is preventing you from writing your own high-quality port and fine-tuning all the parameters, but this does require some effort. If you are looking for a ready-to-go plug-and-play TCP/IP stack, you'll probably find that lwIP is not the way to go.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Oct 2010 22:04:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154023#M4266</guid>
      <dc:creator>scifi</dc:creator>
      <dc:date>2010-10-28T22:04:25Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154024#M4267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;Hi Sven,&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;I just looked at the FNET stack and I was wondering how you and other users handle the GPL license when embedding closed source code ?&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;For RTEMS GPL and LGPL code is not allowed unless it contains an exception clause similar to the one found in libgcc in GCC.&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;&lt;BR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Oct 2010 02:36:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154024#M4267</guid>
      <dc:creator>ChrisJohns</dc:creator>
      <dc:date>2010-10-29T02:36:11Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154025#M4268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;gt;&amp;gt;I was wondering how you and other users handle the GPL license&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The FNET stack is LGPL.&lt;/P&gt;&lt;P&gt;It means, that ONLY changes/fixes in the FNET stack source code should be shared with community, what is pretty fair.&lt;/P&gt;&lt;P&gt;You should&amp;nbsp;NOT open your proprietary code and you may use LGPL with any other license code.&lt;/P&gt;&lt;P&gt;(If you still need a special exception clause, it can be added).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One additional bonus: LGPL is compatible with GPL, so you can use FNET in GPL projects too (LGPL automatically converted to GPL). Many people do not know about this LGPL feature ,that is why FNET is dual licensed. So you can choose what license to choose in your project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Andrey Butok&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Oct 2010 13:48:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154025#M4268</guid>
      <dc:creator>butok</dc:creator>
      <dc:date>2010-10-29T13:48:54Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet With ColdFire V2</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154026#M4269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;EM&gt;&amp;gt;&amp;gt;I was wondering how you and other users handle the GPL license&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;The FNET stack is LGPL.&lt;/P&gt;&lt;P&gt;&amp;gt;It means, that ONLY changes/fixes in the FNET stack source code should be shared with community, what is pretty fair.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes that is fair. RTEMS is the same but does not use or accept LGPL code. The demands on the user is too much.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;You should&amp;nbsp;NOT open your proprietary code and you may use LGPL with any other license code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As long as you provide access to the closed source object modules so an end users can use a new version of FNET, link it to the object modules and create a new version of the software. Being able to&amp;nbsp;practically do this is not important.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;(If you still need a special exception clause, it can be added).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have found in RTEMS this is the best solution. We use GCC's libgcc license. It does not make sense to rebuild software for an embedded system this way and shared libraries (or DLL) type technology is not used how-ever the users of the code still need to provide the ability to relink the application no matter how difficult.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;One additional bonus: LGPL is compatible with GPL, so you can use FNET in GPL projects too (LGPL automatically &amp;gt;converted to GPL). Many people do not know about this LGPL feature ,that is why FNET is dual licensed. So you can &amp;gt;choose what license to choose in your project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The libgcc license is the same. We all want users to contribute patches and new features back to the project.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Nov 2010 05:02:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Ethernet-With-ColdFire-V2/m-p/154026#M4269</guid>
      <dc:creator>ChrisJohns</dc:creator>
      <dc:date>2010-11-05T05:02:23Z</dc:date>
    </item>
  </channel>
</rss>