<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB_DM_PDOWN  AND USB_DP_PDOWN in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-DM-PDOWN-AND-USB-DP-PDOWN/m-p/152738#M4106</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Jaime&lt;BR /&gt;&lt;BR /&gt;The D+/D- pull downs are required in USB-OTG / HOST modes (the outputs are used to control pull-downs in the range 14.25k and 24.8k, which should be either active or high impedance depending on the mode).&lt;BR /&gt;&lt;BR /&gt;&lt;B&gt;If you are using only device mode you don't need them and it is probably best to remove the resistors to the CS outputs to ensure that there is no disturbance.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;Generally these signals are static and so could probably be realized with normal ports.&lt;BR /&gt;&lt;BR /&gt;However I don't have concrete experience with OTG mode so there may be an exception somewhere. Possibly some one else could confirm or explain consequences.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 14 Feb 2009 04:47:07 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2009-02-14T04:47:07Z</dc:date>
    <item>
      <title>USB_DM_PDOWN  AND USB_DP_PDOWN</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-DM-PDOWN-AND-USB-DP-PDOWN/m-p/152737#M4105</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am using MCF52259 with USB interface, but I am also using 3 SPI interfaces.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My problem is I cant find any information about USB_DM_PDOWN&amp;nbsp; AND USB_DP_PDOWN&amp;nbsp; pins (in order to see if I can manage their function with other pins or not use them at all). &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the EV Board they use these pins for USB configuration but I need to use them for the Chip Select function.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;What can I do?&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Feb 2009 01:08:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-DM-PDOWN-AND-USB-DP-PDOWN/m-p/152737#M4105</guid>
      <dc:creator>JaimeR</dc:creator>
      <dc:date>2009-02-14T01:08:09Z</dc:date>
    </item>
    <item>
      <title>Re: USB_DM_PDOWN  AND USB_DP_PDOWN</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-DM-PDOWN-AND-USB-DP-PDOWN/m-p/152738#M4106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Jaime&lt;BR /&gt;&lt;BR /&gt;The D+/D- pull downs are required in USB-OTG / HOST modes (the outputs are used to control pull-downs in the range 14.25k and 24.8k, which should be either active or high impedance depending on the mode).&lt;BR /&gt;&lt;BR /&gt;&lt;B&gt;If you are using only device mode you don't need them and it is probably best to remove the resistors to the CS outputs to ensure that there is no disturbance.&lt;/B&gt;&lt;BR /&gt;&lt;BR /&gt;Generally these signals are static and so could probably be realized with normal ports.&lt;BR /&gt;&lt;BR /&gt;However I don't have concrete experience with OTG mode so there may be an exception somewhere. Possibly some one else could confirm or explain consequences.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Feb 2009 04:47:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/USB-DM-PDOWN-AND-USB-DP-PDOWN/m-p/152738#M4106</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-02-14T04:47:07Z</dc:date>
    </item>
  </channel>
</rss>