<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: MCF5485evb evaluation board; Linux kernel 2.6.10 BSP; Trouble with rootfs in flash</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152723#M4099</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;Well, that stopped the error messages associate with the flash but I still get a kernel panic because it can't mount rootfs:&lt;BR /&gt;&lt;BR /&gt;============================================================================&lt;BR /&gt;Linux version 2.6.10 (jkimble@sc020702-udp067736uds.cs.myharris.net) (gcc versio&lt;BR /&gt;n 3.4.0) #8 Fri May 2 08:35:13 EDT 2008&lt;BR /&gt;starting up linux rev 0.2: startmem 0xc02b8000, size 61MB&lt;BR /&gt;Built 1 zonelists&lt;BR /&gt;Kernel command line: mac0=00:00:54:85:00:01 root=/dev/mtdblock2 rootfstype=jffs2&lt;BR /&gt;&amp;nbsp;noinitrd ip=none mtdparts=phys_mapped_flash:256k(Colilo),2816(kernel),13312k(us&lt;BR /&gt;er)&lt;BR /&gt;PID hash table entries: 512 (order: 9, 8192 bytes)&lt;BR /&gt;RTC driver is not initialized yet, returning 1970.&lt;BR /&gt;Console: colour dummy device 80x25&lt;BR /&gt;Dentry cache hash table entries: 16384 (order: 3, 65536 bytes)&lt;BR /&gt;Inode-cache hash table entries: 8192 (order: 2, 32768 bytes)&lt;BR /&gt;Memory: 62240k/65536k available (2088k kernel code, 1016k data, 96k init)&lt;BR /&gt;Mount-cache hash table entries: 1024 (order: 0, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;Linux/m68k PCI BIOS32 revision 0.05&lt;BR /&gt;ColdFire PCI Host Bridge (Rev. 0) detected&lt;BR /&gt;PCI: Probing PCI hardware&lt;BR /&gt;ColdFire internal SEC driver version 0.11&lt;BR /&gt;jiffies: -29911&lt;BR /&gt;time: -29911&lt;BR /&gt;SEC_INIT_TIMEOUT: 100&lt;BR /&gt;SEC_SMCR_RESET: 16777216MCF547x/8x SEC device driver installed&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;NET: Registered protocol family 23&lt;BR /&gt;Initialize Multi-channel DMA API Alpha v0.3 (2004-04-26)&lt;BR /&gt;JFFS2 version 2.2. (C) 2001-2003 Red Hat, Inc.&lt;BR /&gt;Initializing Cryptographic API&lt;BR /&gt;rtc: RV5C387 RTC driver successfully loaded&lt;BR /&gt;ColdFire watchdog driver is loaded.&lt;BR /&gt;MCF547x/8x DSPI device driver installed&lt;BR /&gt;Coldfire DSPI driver is loaded&lt;BR /&gt;ColdFire internal UART serial driver version 1.00&lt;BR /&gt;ttyS0 at 0xe0008600 (irq = 99) is a builtin ColdFire UART&lt;BR /&gt;ttyS1 at 0xe0008700 (irq = 98) is a builtin ColdFire UART&lt;BR /&gt;ttyS2 at 0xe0008800 (irq = 97) is a builtin ColdFire UART&lt;BR /&gt;ttyS3 at 0xe0008900 (irq = 96) is a builtin ColdFire UART&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler anticipatory registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered&lt;BR /&gt;RAMDISK driver initialized: 16 RAM disks of 8192K size 1024 blocksize&lt;BR /&gt;loop: loaded (max 8 devices)&lt;BR /&gt;ColdFire internal FEC driver version 0.11&lt;BR /&gt;elevator: using anticipatory as default io scheduler&lt;BR /&gt;Unlock all sector for Intel on Fire Engine...&lt;BR /&gt;physmap flash device: 1000000 at f0000000&lt;BR /&gt;phys_mapped_flash: Found 1 x16 devices at 0x0 in 16-bit bank&lt;BR /&gt;&amp;nbsp;Intel/Sharp Extended Query Table at 0x0031&lt;BR /&gt;Using buffer write method&lt;BR /&gt;cfi_cmdset_0001: Erase suspend on write enabled&lt;BR /&gt;mtd: partition size too small (b00)&lt;BR /&gt;RedBoot partition parsing not available&lt;BR /&gt;Using physmap partition definition&lt;BR /&gt;Creating 2 MTD partitions on "phys_mapped_flash":&lt;BR /&gt;0x00000000-0x00040000 : "Colilo (256K)"&lt;BR /&gt;0x00040000-0x00200000 : "user (other Flash memory) 2Mb-256K"&lt;BR /&gt;mice: PS/2 mouse device common for all mice&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;i2c-algo-mcf.o: I2C ColdFire algorithm module is loaded.&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;IP: routing cache hash table of 1024 buckets, 8Kbytes&lt;BR /&gt;TCP: Hash tables configured (established 8192 bind 16384)&lt;BR /&gt;Initializing IPsec netlink socket&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;NET: Registered protocol family 15&lt;BR /&gt;IrCOMM protocol (Dag Brattli)&lt;BR /&gt;Root-NFS: No NFS server available, giving up.&lt;BR /&gt;VFS: Unable to mount root fs via NFS, trying floppy.&lt;BR /&gt;Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)&lt;BR /&gt;=========================================================================&lt;BR /&gt;&lt;BR /&gt;My command line is:&lt;BR /&gt;"mac0=00:00:54:85:00:01 root=/dev/mtdblock2 rootfstype=jffs2 noinitrd ip=none mtdparts=phys_mapped_flash:256k(Colilo),2816(kernel),13312k(user)"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 May 2008 19:56:24 GMT</pubDate>
    <dc:creator>jkimble</dc:creator>
    <dc:date>2008-05-02T19:56:24Z</dc:date>
    <item>
      <title>MCF5485evb evaluation board; Linux kernel 2.6.10 BSP; Trouble with rootfs in flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152720#M4096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;&lt;SPAN&gt;I've followed the "Users Guide" document to the letter in building and burning the kernel and the rootfs to flash. I can boot to NFS with no problem. The flash file system appears to be initialized correctly but when I go to auto boot from flash and load the rootfs from flash I get the following errors:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;=====================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;IrCOMM protocol (Dag Brattli)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000000: 0x1f8b in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;stead&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000004: 0xe10b in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;stead&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000008: 0x0003 in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;stead&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0000000c: 0x6c69 in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;stead&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x000e0024: 0x08ff in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;stead&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Further such events for this erase block will not be printed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Old JFFS2 bitmask found at 0x000e00e8&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You cannot use older JFFS2 filesystems with newer kernels&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Old JFFS2 bitmask found at 0x000fc464&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You cannot use older JFFS2 filesystems with newer kernels&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00100000: 0x3e1b in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;stead&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00120024: 0xceca in&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;stead&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Further such events for this erase block will not be printed&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Cowardly refusing to erase blocks on filesystem with no valid JFFS2 nodes&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;empty_blocks 4, bad_blocks 0, c-&amp;gt;nr_blocks 14&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;VFS: Cannot open root device "mtdblock1" or unknown-block(31,1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please append a correct "root=" boot option&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(31,1)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;=========================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What am I doing wrong??&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 May 2008 01:43:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152720#M4096</guid>
      <dc:creator>jkimble</dc:creator>
      <dc:date>2008-05-02T01:43:45Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5485evb evaluation board; Linux kernel 2.6.10 BSP; Trouble with rootfs in flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152721#M4097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;What does your kernel command line look like?&amp;nbsp;&amp;nbsp; Are you&lt;BR /&gt;sure it shouldn't say root=/dev/mtdblock2 instead of&lt;BR /&gt;root=/dev/mtdblock1?&lt;BR /&gt;&lt;BR /&gt;--Matt&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 May 2008 03:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152721#M4097</guid>
      <dc:creator>mwaddel</dc:creator>
      <dc:date>2008-05-02T03:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5485evb evaluation board; Linux kernel 2.6.10 BSP; Trouble with rootfs in flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152722#M4098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;I'll give it a try. Thanks!&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 May 2008 10:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152722#M4098</guid>
      <dc:creator>jkimble</dc:creator>
      <dc:date>2008-05-02T10:22:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5485evb evaluation board; Linux kernel 2.6.10 BSP; Trouble with rootfs in flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152723#M4099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;Well, that stopped the error messages associate with the flash but I still get a kernel panic because it can't mount rootfs:&lt;BR /&gt;&lt;BR /&gt;============================================================================&lt;BR /&gt;Linux version 2.6.10 (jkimble@sc020702-udp067736uds.cs.myharris.net) (gcc versio&lt;BR /&gt;n 3.4.0) #8 Fri May 2 08:35:13 EDT 2008&lt;BR /&gt;starting up linux rev 0.2: startmem 0xc02b8000, size 61MB&lt;BR /&gt;Built 1 zonelists&lt;BR /&gt;Kernel command line: mac0=00:00:54:85:00:01 root=/dev/mtdblock2 rootfstype=jffs2&lt;BR /&gt;&amp;nbsp;noinitrd ip=none mtdparts=phys_mapped_flash:256k(Colilo),2816(kernel),13312k(us&lt;BR /&gt;er)&lt;BR /&gt;PID hash table entries: 512 (order: 9, 8192 bytes)&lt;BR /&gt;RTC driver is not initialized yet, returning 1970.&lt;BR /&gt;Console: colour dummy device 80x25&lt;BR /&gt;Dentry cache hash table entries: 16384 (order: 3, 65536 bytes)&lt;BR /&gt;Inode-cache hash table entries: 8192 (order: 2, 32768 bytes)&lt;BR /&gt;Memory: 62240k/65536k available (2088k kernel code, 1016k data, 96k init)&lt;BR /&gt;Mount-cache hash table entries: 1024 (order: 0, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;Linux/m68k PCI BIOS32 revision 0.05&lt;BR /&gt;ColdFire PCI Host Bridge (Rev. 0) detected&lt;BR /&gt;PCI: Probing PCI hardware&lt;BR /&gt;ColdFire internal SEC driver version 0.11&lt;BR /&gt;jiffies: -29911&lt;BR /&gt;time: -29911&lt;BR /&gt;SEC_INIT_TIMEOUT: 100&lt;BR /&gt;SEC_SMCR_RESET: 16777216MCF547x/8x SEC device driver installed&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;NET: Registered protocol family 23&lt;BR /&gt;Initialize Multi-channel DMA API Alpha v0.3 (2004-04-26)&lt;BR /&gt;JFFS2 version 2.2. (C) 2001-2003 Red Hat, Inc.&lt;BR /&gt;Initializing Cryptographic API&lt;BR /&gt;rtc: RV5C387 RTC driver successfully loaded&lt;BR /&gt;ColdFire watchdog driver is loaded.&lt;BR /&gt;MCF547x/8x DSPI device driver installed&lt;BR /&gt;Coldfire DSPI driver is loaded&lt;BR /&gt;ColdFire internal UART serial driver version 1.00&lt;BR /&gt;ttyS0 at 0xe0008600 (irq = 99) is a builtin ColdFire UART&lt;BR /&gt;ttyS1 at 0xe0008700 (irq = 98) is a builtin ColdFire UART&lt;BR /&gt;ttyS2 at 0xe0008800 (irq = 97) is a builtin ColdFire UART&lt;BR /&gt;ttyS3 at 0xe0008900 (irq = 96) is a builtin ColdFire UART&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler anticipatory registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered&lt;BR /&gt;RAMDISK driver initialized: 16 RAM disks of 8192K size 1024 blocksize&lt;BR /&gt;loop: loaded (max 8 devices)&lt;BR /&gt;ColdFire internal FEC driver version 0.11&lt;BR /&gt;elevator: using anticipatory as default io scheduler&lt;BR /&gt;Unlock all sector for Intel on Fire Engine...&lt;BR /&gt;physmap flash device: 1000000 at f0000000&lt;BR /&gt;phys_mapped_flash: Found 1 x16 devices at 0x0 in 16-bit bank&lt;BR /&gt;&amp;nbsp;Intel/Sharp Extended Query Table at 0x0031&lt;BR /&gt;Using buffer write method&lt;BR /&gt;cfi_cmdset_0001: Erase suspend on write enabled&lt;BR /&gt;mtd: partition size too small (b00)&lt;BR /&gt;RedBoot partition parsing not available&lt;BR /&gt;Using physmap partition definition&lt;BR /&gt;Creating 2 MTD partitions on "phys_mapped_flash":&lt;BR /&gt;0x00000000-0x00040000 : "Colilo (256K)"&lt;BR /&gt;0x00040000-0x00200000 : "user (other Flash memory) 2Mb-256K"&lt;BR /&gt;mice: PS/2 mouse device common for all mice&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;i2c-algo-mcf.o: I2C ColdFire algorithm module is loaded.&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;IP: routing cache hash table of 1024 buckets, 8Kbytes&lt;BR /&gt;TCP: Hash tables configured (established 8192 bind 16384)&lt;BR /&gt;Initializing IPsec netlink socket&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;NET: Registered protocol family 15&lt;BR /&gt;IrCOMM protocol (Dag Brattli)&lt;BR /&gt;Root-NFS: No NFS server available, giving up.&lt;BR /&gt;VFS: Unable to mount root fs via NFS, trying floppy.&lt;BR /&gt;Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)&lt;BR /&gt;=========================================================================&lt;BR /&gt;&lt;BR /&gt;My command line is:&lt;BR /&gt;"mac0=00:00:54:85:00:01 root=/dev/mtdblock2 rootfstype=jffs2 noinitrd ip=none mtdparts=phys_mapped_flash:256k(Colilo),2816(kernel),13312k(user)"&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 May 2008 19:56:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152723#M4099</guid>
      <dc:creator>jkimble</dc:creator>
      <dc:date>2008-05-02T19:56:24Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5485evb evaluation board; Linux kernel 2.6.10 BSP; Trouble with rootfs in flash</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152724#M4100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BR /&gt;Disregard last message. On my command line I had:&lt;BR /&gt;&lt;BR /&gt;set cl mac0=00:00:54:85:00:01 root=/dev/mtdblock2 rootfstype=jffs2 noinitrd ip=none mtdparts=phys_mapped_flash:256k(Colilo),2816(kernel),13312k(user)&lt;BR /&gt;&lt;BR /&gt;Rather than:&lt;BR /&gt;&lt;BR /&gt;set cl mac0=00:00:54:85:00:01 root=/dev/mtdblock2 rootfstype=jffs2 noinitrd ip=none mtdparts=phys_mapped_flash:256k(Colilo),2816k(kernel),13312k(user)&lt;BR /&gt;&lt;BR /&gt;2816 bytes is a little cramped for the kernel apparently....&lt;BR /&gt;&lt;BR /&gt;Thanks for your help.&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 May 2008 20:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5485evb-evaluation-board-Linux-kernel-2-6-10-BSP-Trouble-with/m-p/152724#M4100</guid>
      <dc:creator>jkimble</dc:creator>
      <dc:date>2008-05-02T20:06:31Z</dc:date>
    </item>
  </channel>
</rss>