<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 CW 7.2 /MQX Programmer 128K Limit Problems</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CW-7-2-MQX-Programmer-128K-Limit-Problems/m-p/152609#M4085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been through some of the tutorials for MQX using the M52233DEMO board.&amp;nbsp; All went well until I tried to do anything with RTCS other than the telnet example.&amp;nbsp; After compiling the examples, and trying to program them into flash, I get a message that the programmer is limited to 128K.&amp;nbsp; I also tried a new project with MQX+RTCS stationery, and it is also too big to program and debug.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is MQX and RTCS really this big, or are there some configuration options I can use to reduce this?&amp;nbsp; I'm working my way through all of the documentaion I can find, but it is an enormous task due to the sheer volume!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had originally had the CW Special edition on my PC.&amp;nbsp; I tried to uninstall this and install the EVAL version, but I am wondering if I didn't really install the Eval version.&amp;nbsp; When I look in the license file, I see lots of "stuff" in the "special" portion of the license file, but there is nothing in the "eval" section of the license file.&amp;nbsp; Would it make sense for the license file to be like this if I correctly installed the eval version?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does the Eval version of 7.2 have limits on the program size for programming and debug?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there some procedure I need to follow to install the eval version once the special version has been installed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any help with this!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Oct 2010 06:10:05 GMT</pubDate>
    <dc:creator>bobsawyer</dc:creator>
    <dc:date>2010-10-04T06:10:05Z</dc:date>
    <item>
      <title>CW 7.2 /MQX Programmer 128K Limit Problems</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CW-7-2-MQX-Programmer-128K-Limit-Problems/m-p/152609#M4085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been through some of the tutorials for MQX using the M52233DEMO board.&amp;nbsp; All went well until I tried to do anything with RTCS other than the telnet example.&amp;nbsp; After compiling the examples, and trying to program them into flash, I get a message that the programmer is limited to 128K.&amp;nbsp; I also tried a new project with MQX+RTCS stationery, and it is also too big to program and debug.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is MQX and RTCS really this big, or are there some configuration options I can use to reduce this?&amp;nbsp; I'm working my way through all of the documentaion I can find, but it is an enormous task due to the sheer volume!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had originally had the CW Special edition on my PC.&amp;nbsp; I tried to uninstall this and install the EVAL version, but I am wondering if I didn't really install the Eval version.&amp;nbsp; When I look in the license file, I see lots of "stuff" in the "special" portion of the license file, but there is nothing in the "eval" section of the license file.&amp;nbsp; Would it make sense for the license file to be like this if I correctly installed the eval version?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does the Eval version of 7.2 have limits on the program size for programming and debug?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there some procedure I need to follow to install the eval version once the special version has been installed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any help with this!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Oct 2010 06:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CW-7-2-MQX-Programmer-128K-Limit-Problems/m-p/152609#M4085</guid>
      <dc:creator>bobsawyer</dc:creator>
      <dc:date>2010-10-04T06:10:05Z</dc:date>
    </item>
    <item>
      <title>Re: CW 7.2 /MQX Programmer 128K Limit Problems</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CW-7-2-MQX-Programmer-128K-Limit-Problems/m-p/152610#M4086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The evaluation version of CodeWarrior has no limits, but that capability expires in 30 days. Either the evaluation install failed, or the clock ran out on you. Is the e-mail in your registration info valid? I can send you a temporary eval license to help track down the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Oct 2010 19:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/CW-7-2-MQX-Programmer-128K-Limit-Problems/m-p/152610#M4086</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2010-10-04T19:25:01Z</dc:date>
    </item>
  </channel>
</rss>