<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Reset Vector for MCF5445x in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-Vector-for-MCF5445x/m-p/151515#M3961</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I don't think you can.&amp;nbsp; You either boot off a flexbus device or using the Serial Boot Flash (SBF) over SPI.&lt;BR /&gt;&lt;BR /&gt;The two signals that control booting are BOOTMOD[1:0] (section 10.2.1 in the RM).&amp;nbsp; Your options are:&lt;BR /&gt;&lt;UL&gt;&lt;LI&gt;Boot from Flexbus with defaults&lt;/LI&gt;&lt;LI&gt;Boot from Flexbus and override defaults via data bus&lt;/LI&gt;&lt;LI&gt;Boot from Flexbus and override defaults via the serial boot facility&lt;/LI&gt;&lt;LI&gt;Reserved (just for those wondering about the last bit combination)&lt;BR /&gt;&lt;/LI&gt;&lt;/UL&gt;You can't go directly to SDRAM.&amp;nbsp; Also you'd need to setup the SDRAM controller before you could execute code from it.&lt;BR /&gt;&lt;BR /&gt;--Kurt&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Feb 2009 05:34:13 GMT</pubDate>
    <dc:creator>kmahan</dc:creator>
    <dc:date>2009-02-11T05:34:13Z</dc:date>
    <item>
      <title>Reset Vector for MCF5445x</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-Vector-for-MCF5445x/m-p/151514#M3960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am writing a boot loader for an MCF5445x based target.&amp;nbsp; I am wondering if it is possible to issue a soft reset but then have the reset vector route execution to the kernel I have just loaded into RAM (i.e. base address at 0x4002000) rather than do its usual load from ROM (0x00000000) or via SPI.&amp;nbsp; I've been reading the MCF54455RM spec doc and my first impression is that it is not easily done, but perhaps I missed something.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2009 05:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-Vector-for-MCF5445x/m-p/151514#M3960</guid>
      <dc:creator>Thad</dc:creator>
      <dc:date>2009-02-11T05:25:16Z</dc:date>
    </item>
    <item>
      <title>Re: Reset Vector for MCF5445x</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-Vector-for-MCF5445x/m-p/151515#M3961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I don't think you can.&amp;nbsp; You either boot off a flexbus device or using the Serial Boot Flash (SBF) over SPI.&lt;BR /&gt;&lt;BR /&gt;The two signals that control booting are BOOTMOD[1:0] (section 10.2.1 in the RM).&amp;nbsp; Your options are:&lt;BR /&gt;&lt;UL&gt;&lt;LI&gt;Boot from Flexbus with defaults&lt;/LI&gt;&lt;LI&gt;Boot from Flexbus and override defaults via data bus&lt;/LI&gt;&lt;LI&gt;Boot from Flexbus and override defaults via the serial boot facility&lt;/LI&gt;&lt;LI&gt;Reserved (just for those wondering about the last bit combination)&lt;BR /&gt;&lt;/LI&gt;&lt;/UL&gt;You can't go directly to SDRAM.&amp;nbsp; Also you'd need to setup the SDRAM controller before you could execute code from it.&lt;BR /&gt;&lt;BR /&gt;--Kurt&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2009 05:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-Vector-for-MCF5445x/m-p/151515#M3961</guid>
      <dc:creator>kmahan</dc:creator>
      <dc:date>2009-02-11T05:34:13Z</dc:date>
    </item>
    <item>
      <title>Re: Reset Vector for MCF5445x</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-Vector-for-MCF5445x/m-p/151516#M3962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I thought as much.&amp;nbsp; I was hoping for a shortcut, but it looks like I'll just have to set the board state manually before jumping to the kernel entry point.&amp;nbsp; Thanks.&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2009 07:22:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Reset-Vector-for-MCF5445x/m-p/151516#M3962</guid>
      <dc:creator>Thad</dc:creator>
      <dc:date>2009-02-11T07:22:31Z</dc:date>
    </item>
  </channel>
</rss>