<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: 52259 wont boot without bdm attached?</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-wont-boot-without-bdm-attached/m-p/150525#M3834</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It could be the same problem as this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/65237#65237" title="https://community.freescale.com/message/65237#65237"&gt;https://community.freescale.com/message/65237#65237&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 24 Sep 2010 02:40:51 GMT</pubDate>
    <dc:creator>scifi</dc:creator>
    <dc:date>2010-09-24T02:40:51Z</dc:date>
    <item>
      <title>52259 wont boot without bdm attached?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-wont-boot-without-bdm-attached/m-p/150524#M3833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ive got a 52259 on a custom board that boots and runs fine from codewarrior with the bdm attached. However, when I remove the bdm and reset the board, it doesnt run. Im using a 48mhz crystal and it should work with clkmod0 and 1 pulled up to vcc. However, have tried all configurations of clkmod0 and clkmod1 with no luck. When I try the same code on the tower board, it works find and boots up with or without the bdm attached. I have the same 4 pins pulled upon my bdm connector as on the tower board. Im using the same crystal as on the tower board. I dont get it. Im sure its something obvious, but I cant find it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any help!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--Byra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Sep 2010 00:58:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-wont-boot-without-bdm-attached/m-p/150524#M3833</guid>
      <dc:creator>Byra</dc:creator>
      <dc:date>2010-09-24T00:58:00Z</dc:date>
    </item>
    <item>
      <title>Re: 52259 wont boot without bdm attached?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-wont-boot-without-bdm-attached/m-p/150525#M3834</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It could be the same problem as this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/65237#65237" title="https://community.freescale.com/message/65237#65237"&gt;https://community.freescale.com/message/65237#65237&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Sep 2010 02:40:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/52259-wont-boot-without-bdm-attached/m-p/150525#M3834</guid>
      <dc:creator>scifi</dc:creator>
      <dc:date>2010-09-24T02:40:51Z</dc:date>
    </item>
  </channel>
</rss>