<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCF5328 PWM GPIO bits in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5328-PWM-GPIO-bits/m-p/149330#M3732</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm confused by the MCF5328 family&amp;nbsp;documentation and header files regarding the PWM1/3/5/7 pins used as GPIO.&amp;nbsp; The MCF5329 reference manual (rev 3) shows only bits 2,3,4 and 5 being used&amp;nbsp;in the PODR_PWM, PDDR_PWM and PPDSDR_PWM registers, which does match the PWM&amp;nbsp;"bits" 1/3/5/7 (which are shown as GPIO signals PWM1/3/5/7 in table 2-1).&amp;nbsp;&amp;nbsp;For the PPDSDR_PWM register it specifically states that these are the controls for signals PWM2/3/4/5 - which does not match the actual PWM numbers.&amp;nbsp; Looking in the header files from Freescale - it also uses the 2/3/4/5 bit numbers for these registers - not matching the PWM1/3/5/7 numbers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anybody tell me the correct meanings of the bits in the PODR_PWM, PDDR_PWM and PPDSDR_PWM registers for the MCF5328?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paul Withers&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jul 2011 02:40:21 GMT</pubDate>
    <dc:creator>powie_freescale</dc:creator>
    <dc:date>2011-07-14T02:40:21Z</dc:date>
    <item>
      <title>MCF5328 PWM GPIO bits</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5328-PWM-GPIO-bits/m-p/149330#M3732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm confused by the MCF5328 family&amp;nbsp;documentation and header files regarding the PWM1/3/5/7 pins used as GPIO.&amp;nbsp; The MCF5329 reference manual (rev 3) shows only bits 2,3,4 and 5 being used&amp;nbsp;in the PODR_PWM, PDDR_PWM and PPDSDR_PWM registers, which does match the PWM&amp;nbsp;"bits" 1/3/5/7 (which are shown as GPIO signals PWM1/3/5/7 in table 2-1).&amp;nbsp;&amp;nbsp;For the PPDSDR_PWM register it specifically states that these are the controls for signals PWM2/3/4/5 - which does not match the actual PWM numbers.&amp;nbsp; Looking in the header files from Freescale - it also uses the 2/3/4/5 bit numbers for these registers - not matching the PWM1/3/5/7 numbers.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can anybody tell me the correct meanings of the bits in the PODR_PWM, PDDR_PWM and PPDSDR_PWM registers for the MCF5328?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Paul Withers&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2011 02:40:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5328-PWM-GPIO-bits/m-p/149330#M3732</guid>
      <dc:creator>powie_freescale</dc:creator>
      <dc:date>2011-07-14T02:40:21Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5328 PWM GPIO bits</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5328-PWM-GPIO-bits/m-p/149331#M3733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That looks like a cut-and-paste bug when those manuals were being assembled.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Searching shows those register and bit names only exist in the MCF5329 and MCF5373 manuals, so it doesn't immediately look like a chapter got pasted from an MCF52xx chip as I've seen before.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"bits 2,3,4 and 5 being used&amp;nbsp;in the PODR_PWM, PDDR_PWM and PPDSDR_PWM﻿" have been named as per the bits in that register, which is consistent for that chapter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PWM signals are named for their function.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think the "proper fix" would be to change only the second column in "Table 2-1. MCF5327/8/9 Signal Information and Muxing﻿" and&amp;nbsp; "Table 13-1. MCF5327/8/9 Signal Information and Muxing﻿" to something like:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="2"&gt;Signal Name&amp;nbsp;&amp;nbsp; GPIO&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="2"&gt;--------------------&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="2"&gt;PWM7&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PPWM5&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="2"&gt;PWM5&lt;FONT face="courier new,courier" size="2"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PPWM4&lt;/FONT&gt;﻿&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="2"&gt;PWM3&lt;FONT face="courier new,courier" size="2"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PPWM3&lt;/FONT&gt;﻿&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="2"&gt;PWM1&lt;FONT face="courier new,courier" size="2"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PPWM&lt;/FONT&gt;2&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please write some code totest this out and then report back.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2011 08:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5328-PWM-GPIO-bits/m-p/149331#M3733</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2011-07-14T08:16:00Z</dc:date>
    </item>
  </channel>
</rss>