<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: COLDFIRE UARTS Carrier Detect</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/COLDFIRE-UARTS-Carrier-Detect/m-p/147223#M3398</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi&lt;BR /&gt;&lt;BR /&gt;Some of the UARTs support RTS/CTS lines which have capabilities of automatically controlling flow control:&lt;BR /&gt;&lt;A href="http://www.utasker.com/forum/index.php?topic=105.msg424#msg424" rel="nofollow" target="_blank"&gt;http://www.utasker.com/forum/index.php?topic=105.msg424#msg424&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;The CTS interrupt capability allows interrupt driven flow control too.&lt;BR /&gt;&lt;BR /&gt;Since CD input is generally more of an informative nature rather than than controlling data flow (with some reaction constraints) it doesn't usually merit a dedicated modem control signal at the UART.&lt;BR /&gt;&lt;BR /&gt;The same function can be achieved by any free Edge Port line. When there are no edge ports free further interrupt capability is possible by using timers in edge-capture more and even the interrupt driven trigger functionality of the ADC inputs. More generally polling any free GPIO is often adequate as well.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Jan 2009 04:21:17 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2009-01-29T04:21:17Z</dc:date>
    <item>
      <title>COLDFIRE UARTS Carrier Detect</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/COLDFIRE-UARTS-Carrier-Detect/m-p/147222#M3397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Is there any way to implement carrier detect on the RS232 ports ?&lt;/DIV&gt;&lt;DIV&gt;I see only RTS/CTS.&lt;/DIV&gt;&lt;DIV&gt;Is there software available to implement using a gpio ?&lt;/DIV&gt;&lt;DIV&gt;Thanks in advance !&lt;/DIV&gt;&lt;DIV&gt;John&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2009 02:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/COLDFIRE-UARTS-Carrier-Detect/m-p/147222#M3397</guid>
      <dc:creator>queequeg</dc:creator>
      <dc:date>2009-01-29T02:05:58Z</dc:date>
    </item>
    <item>
      <title>Re: COLDFIRE UARTS Carrier Detect</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/COLDFIRE-UARTS-Carrier-Detect/m-p/147223#M3398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi&lt;BR /&gt;&lt;BR /&gt;Some of the UARTs support RTS/CTS lines which have capabilities of automatically controlling flow control:&lt;BR /&gt;&lt;A href="http://www.utasker.com/forum/index.php?topic=105.msg424#msg424" rel="nofollow" target="_blank"&gt;http://www.utasker.com/forum/index.php?topic=105.msg424#msg424&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;The CTS interrupt capability allows interrupt driven flow control too.&lt;BR /&gt;&lt;BR /&gt;Since CD input is generally more of an informative nature rather than than controlling data flow (with some reaction constraints) it doesn't usually merit a dedicated modem control signal at the UART.&lt;BR /&gt;&lt;BR /&gt;The same function can be achieved by any free Edge Port line. When there are no edge ports free further interrupt capability is possible by using timers in edge-capture more and even the interrupt driven trigger functionality of the ADC inputs. More generally polling any free GPIO is often adequate as well.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2009 04:21:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/COLDFIRE-UARTS-Carrier-Detect/m-p/147223#M3398</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2009-01-29T04:21:17Z</dc:date>
    </item>
  </channel>
</rss>