<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KSZ8041 PHY Chip for the MCF52259 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146467#M3270</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what do you mean with:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;"The only problem i had (lost link sometimes) was the capacitors on quartz too low (18pF increased to 33pF)."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;did u use an independent crystal for the CI? whats frequency? 25MHz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 23 Jan 2010 04:56:37 GMT</pubDate>
    <dc:creator>Flaviohpo</dc:creator>
    <dc:date>2010-01-23T04:56:37Z</dc:date>
    <item>
      <title>KSZ8041 PHY Chip for the MCF52259</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146464#M3267</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp; I have on order MCF52259 processors and also ordered KSZ8041 PHY as in the demo kit.&amp;nbsp; The demo kit has the KSZ8041NL , but I can only get the KSZ8041TLI part. The only difference I can see is that the TLI part also does SMII interface, package type, and about £1 more expensive. I have never used a PHY chip before, but can anyone tell me if there would be a problem using this one?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Neil&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jan 2009 00:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146464#M3267</guid>
      <dc:creator>ND</dc:creator>
      <dc:date>2009-01-27T00:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: KSZ8041 PHY Chip for the MCF52259</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146465#M3268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I have the same question, but I also would like to know some alternatives to the KSZ8041NL that is not QFN package. Thanks.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jan 2010 21:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146465#M3268</guid>
      <dc:creator>Flaviohpo</dc:creator>
      <dc:date>2010-01-21T21:05:37Z</dc:date>
    </item>
    <item>
      <title>Re: KSZ8041 PHY Chip for the MCF52259</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146466#M3269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used a KSZ8041TL connected to a MCF52259 because TQFP package is easier to solder.&lt;/P&gt;&lt;P&gt;It runs with the same software the DEMO board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The only problem i had (lost link sometimes) was the capacitors on quartz too low (18pF increased to 33pF).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No other problems.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Henri&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2010 03:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146466#M3269</guid>
      <dc:creator>HLaidet</dc:creator>
      <dc:date>2010-01-22T03:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: KSZ8041 PHY Chip for the MCF52259</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146467#M3270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;what do you mean with:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;"The only problem i had (lost link sometimes) was the capacitors on quartz too low (18pF increased to 33pF)."&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;did u use an independent crystal for the CI? whats frequency? 25MHz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Jan 2010 04:56:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146467#M3270</guid>
      <dc:creator>Flaviohpo</dc:creator>
      <dc:date>2010-01-23T04:56:37Z</dc:date>
    </item>
    <item>
      <title>Re: KSZ8041 PHY Chip for the MCF52259</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146468#M3271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i use the basic schematic with a crystal 25MHz(Fundamental)+1M resistor and two 18pF capacitors ( like the schematic of M52259DEMO board ).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;the quartz is: CITIZEN HCM49 25.000MABJ-UT&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;because it is the first time i use a PHY, then i did a test endurance.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;that's when i found errors ethernet.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;by putting traps, i have found losses of LINK (status register, bit LINK STATUS).&lt;/P&gt;&lt;P&gt;to get everything correct, i had to increase the 18pF capacitors on quartz.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;now the test is done without errors (several hours).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Henri&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jan 2010 20:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/KSZ8041-PHY-Chip-for-the-MCF52259/m-p/146468#M3271</guid>
      <dc:creator>HLaidet</dc:creator>
      <dc:date>2010-01-25T20:49:07Z</dc:date>
    </item>
  </channel>
</rss>