<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: ADC Power control - M5223X / M5213</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ADC-Power-control-M5223X-M5213/m-p/146408#M3260</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Mark,&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;The MCF5213 family&amp;nbsp;does have a relaxation (dumb name) OSC on-chip. Better put, the MCF5213 has an on-chip OSC that can run at 8MHz and be used as an input to the PLL. This I’ve done in the past so it works fine.&lt;/P&gt;&lt;P&gt;The MCF5222x (K2U) also has this (or at least the documentation does). Haven’t tested ever.&lt;/P&gt;&lt;P&gt;The MCF5223x (K2E) does not have relaxation OSC.&lt;/P&gt;&lt;P&gt;I’m sure the reference to SIM_PCE in Section 28.5.8.1 should be changed to reference the PPMR (Peripheral Power Management) setting for ADC.&lt;/P&gt;&lt;P&gt;Regards, David&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Apr 2008 23:29:53 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2008-04-17T23:29:53Z</dc:date>
    <item>
      <title>ADC Power control - M5223X / M5213</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ADC-Power-control-M5223X-M5213/m-p/146407#M3259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi All&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a few questions about the ADC in these devices in relation to its power modes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to the users' manual there are 5 different modes.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;These operate partly by using the relaxation oscillator [OCO] (needs to be 8MHz). In addition there is a note about the ADC's clock being disabled if ADC is not equal to '1' in the SIM_PCE register.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However it seems as though there is no SIM_PCE register in these devices (SIM module).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Also, apart from in the ADC chapter, there is no reference to a releaxation oscillator in the devices or how it could be configured.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In order to complete a driver interface to this module I would like to find out whether these power modes are possible or whether the description in the users' manual is possibly incorrect.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mark Butcher&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.uTasker.com" rel="nofollow" target="_blank"&gt;http://www.uTasker.com&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Apr 2008 10:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ADC-Power-control-M5223X-M5213/m-p/146407#M3259</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2008-04-13T10:13:36Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Power control - M5223X / M5213</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ADC-Power-control-M5223X-M5213/m-p/146408#M3260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi Mark,&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;The MCF5213 family&amp;nbsp;does have a relaxation (dumb name) OSC on-chip. Better put, the MCF5213 has an on-chip OSC that can run at 8MHz and be used as an input to the PLL. This I’ve done in the past so it works fine.&lt;/P&gt;&lt;P&gt;The MCF5222x (K2U) also has this (or at least the documentation does). Haven’t tested ever.&lt;/P&gt;&lt;P&gt;The MCF5223x (K2E) does not have relaxation OSC.&lt;/P&gt;&lt;P&gt;I’m sure the reference to SIM_PCE in Section 28.5.8.1 should be changed to reference the PPMR (Peripheral Power Management) setting for ADC.&lt;/P&gt;&lt;P&gt;Regards, David&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2008 23:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ADC-Power-control-M5223X-M5213/m-p/146408#M3260</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2008-04-17T23:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Power control - M5223X / M5213</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ADC-Power-control-M5223X-M5213/m-p/146409#M3261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi David&lt;BR /&gt;&lt;BR /&gt;Thanks. This corresponds with latest information so all seems clear now.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Apr 2008 01:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/ADC-Power-control-M5223X-M5213/m-p/146409#M3261</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2008-04-18T01:08:27Z</dc:date>
    </item>
  </channel>
</rss>