<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: MCF52233 bootloader with TFTP and DHCP client</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145372#M3080</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Peter&lt;BR /&gt;&lt;BR /&gt;I am sure that the NicheLite stack (as other free or open source ones) includes the protocols needed so it would be possible to patch up something after adding the necessary in circuit FLASH routines (IAP).&lt;BR /&gt;&lt;BR /&gt;You can also look at the uTasker solution which is designed for the M5223X (free for non-commercial work). It is a 2k boot loader (one FLASH sector in the M5223X) and it allows complete software updates via Internet (I say Internet rather than LAN because it has secure upload capabilities based on HTTP POST methods and doesn't need a server as TFTP does).&lt;BR /&gt;It may be that this doesn't suit but you could look at it to be sure (it is documented here):&lt;BR /&gt;&lt;A href="http://www.utasker.com/docs/uTasker/uTaskerBootLoader.PDF" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/uTasker/uTaskerBootLoader.PDF&lt;/A&gt;&lt;BR /&gt;&lt;A href="http://www.utasker.com/docs/uTasker/BM-Booloader_for_M5223X.PDF" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/uTasker/BM-Booloader_for_M5223X.PDF&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;You will see that it requires application support (to allow the transfers using TCP based methods) before the application, OS and stack are replaced by the loader) and so needs enough space to store the new program alongside the old one. [The file system supports also saving in cheap external SPI based memory for such jobs which is an interesting approach when FLASH is restricted].&lt;BR /&gt;&lt;BR /&gt;The uTasker bootloader doesn't have a configuration (at present) for a TFTP based transfer but the components are available if you would like to "plug them together"...&lt;BR /&gt;The disadvantage of having TFTP [IP, ARP, UDP] and DHCP [plus IAP] in the boot loader is that it will probably require about 16k of FLASH on the M5223X - see code size comparisons here:&lt;BR /&gt;&lt;A href="http://www.utasker.com/docs/M5223X/uTaskerV1.2-Tutorial-M5223X.PDF" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/M5223X/uTaskerV1.2-Tutorial-M5223X.PDF&lt;/A&gt; (page 15)&lt;BR /&gt;&lt;BR /&gt;A further approach is to include the OS and TCP/IP stack in the bootloader [disadvantage is that these elements can not be updated via LAN - only the application can be or parts of the others 'patched'], then the size of the boot loader is not an issue. The application parts make use of the same resources (eg. OS, Stack, File system etc.) after it has been loaded. The uTasker has what we call MULTISTART support - it enables an application (or additional applications) to be uploaded to the board and the system reconfigures itself to schedule the new software parts. In other words it can function as an application specific boot loader using what ever methods are required.&lt;BR /&gt;&lt;BR /&gt;PS: Have you tried stripping down the dBug code (it is available as source) to see how small it can be made?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;&lt;IMG src="http://www.uTasker.com/uTaskerLogoSS.jpg" /&gt;&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 18 Feb 2007 03:46:57 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2007-02-18T03:46:57Z</dc:date>
    <item>
      <title>MCF52233 bootloader with TFTP and DHCP client</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145371#M3079</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;Hi&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;I need to download and/or reload the firmware for my MCF52233 device via the Ethernet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;I have an application running on the NicheLite stack. I am only using the UDP interface to send data logs from my embedded device to a server application.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;Right know I am using the dBUG from Freescale but it is too large, I am planning on using the MCF52230 with only 128Kb on the final product.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;Therefore I need a small bootloader with TFTP and DHCP client to&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;Obtain an IP adr from the DHCP server at power up first time&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;Check the current SW version on the TFTP server and replace the SW if needed.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;&amp;nbsp;&lt;SPAN&gt;Any help?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;Regards&lt;/SPAN&gt; &lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;Peter Kirketerp&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;Develco A/S&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style=": ; color: #000000; font-size: 3; font-family: 'Times New Roman';"&gt;&lt;SPAN&gt;Denmark&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Feb 2007 21:57:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145371#M3079</guid>
      <dc:creator>PeterKirketerp</dc:creator>
      <dc:date>2007-02-17T21:57:38Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52233 bootloader with TFTP and DHCP client</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145372#M3080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Peter&lt;BR /&gt;&lt;BR /&gt;I am sure that the NicheLite stack (as other free or open source ones) includes the protocols needed so it would be possible to patch up something after adding the necessary in circuit FLASH routines (IAP).&lt;BR /&gt;&lt;BR /&gt;You can also look at the uTasker solution which is designed for the M5223X (free for non-commercial work). It is a 2k boot loader (one FLASH sector in the M5223X) and it allows complete software updates via Internet (I say Internet rather than LAN because it has secure upload capabilities based on HTTP POST methods and doesn't need a server as TFTP does).&lt;BR /&gt;It may be that this doesn't suit but you could look at it to be sure (it is documented here):&lt;BR /&gt;&lt;A href="http://www.utasker.com/docs/uTasker/uTaskerBootLoader.PDF" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/uTasker/uTaskerBootLoader.PDF&lt;/A&gt;&lt;BR /&gt;&lt;A href="http://www.utasker.com/docs/uTasker/BM-Booloader_for_M5223X.PDF" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/uTasker/BM-Booloader_for_M5223X.PDF&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;You will see that it requires application support (to allow the transfers using TCP based methods) before the application, OS and stack are replaced by the loader) and so needs enough space to store the new program alongside the old one. [The file system supports also saving in cheap external SPI based memory for such jobs which is an interesting approach when FLASH is restricted].&lt;BR /&gt;&lt;BR /&gt;The uTasker bootloader doesn't have a configuration (at present) for a TFTP based transfer but the components are available if you would like to "plug them together"...&lt;BR /&gt;The disadvantage of having TFTP [IP, ARP, UDP] and DHCP [plus IAP] in the boot loader is that it will probably require about 16k of FLASH on the M5223X - see code size comparisons here:&lt;BR /&gt;&lt;A href="http://www.utasker.com/docs/M5223X/uTaskerV1.2-Tutorial-M5223X.PDF" rel="nofollow" target="_blank"&gt;http://www.utasker.com/docs/M5223X/uTaskerV1.2-Tutorial-M5223X.PDF&lt;/A&gt; (page 15)&lt;BR /&gt;&lt;BR /&gt;A further approach is to include the OS and TCP/IP stack in the bootloader [disadvantage is that these elements can not be updated via LAN - only the application can be or parts of the others 'patched'], then the size of the boot loader is not an issue. The application parts make use of the same resources (eg. OS, Stack, File system etc.) after it has been loaded. The uTasker has what we call MULTISTART support - it enables an application (or additional applications) to be uploaded to the board and the system reconfigures itself to schedule the new software parts. In other words it can function as an application specific boot loader using what ever methods are required.&lt;BR /&gt;&lt;BR /&gt;PS: Have you tried stripping down the dBug code (it is available as source) to see how small it can be made?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;&lt;IMG src="http://www.uTasker.com/uTaskerLogoSS.jpg" /&gt;&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Feb 2007 03:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145372#M3080</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2007-02-18T03:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52233 bootloader with TFTP and DHCP client</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145373#M3081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Peter&lt;BR /&gt;&lt;BR /&gt;Could you detail how you envisabe the checking of the software on the TFTP server?&lt;BR /&gt;&lt;BR /&gt;Your board will be operating as a client and has the ability to perform a read or a write but not request information about the files there. Do you envisage reading a standard named file and comparing its content? If the content doesn't match that loaded on the board then deleting the boards code and reading the file again?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;&lt;IMG src="http://www.uTasker.com/uTaskerLogoSS.jpg" /&gt;&lt;/A&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Feb 2007 04:20:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145373#M3081</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2007-02-19T04:20:55Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52233 bootloader with TFTP and DHCP client</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145374#M3082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;Hi Mark&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;The TFTP client retrieves a specified configuration file name from the server. It is the content of the file we interpret.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;We have down size the dBUG to 25Kb but that is without DHCP client, normally the DHCP client is 8Kb.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;First I was thinking of using the NicheLite stack as the bootloader and then have the application running from a user define adr. But I have problems splitting up the stack and the application I 2 separated *.s19 or *.bin files. I was only using the dBUG because of the problems splitting up the stack and the application.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT color="#000000" face="Times New Roman" size="3"&gt;I can see that the uTasker has a&lt;/FONT&gt; &lt;A target="_blank"&gt;&lt;/A&gt;&lt;A target="_blank"&gt;&lt;SPAN&gt;&lt;FONT color="#000000" face="Times New Roman" size="3"&gt;MULTISTART functionality&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;for replacing only the application code it sounds like what I am looking for!&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;I am very interesting in getting the source code for the uTasker to test the MULTISTART functionality with my application, please tell me how I can get the source code?&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;B&gt;&lt;SPAN&gt;Med venlig hilsen / Best regards&lt;/SPAN&gt;&lt;/B&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;&lt;B&gt;&lt;SPAN&gt;Peter Kirketerp&lt;/SPAN&gt;&lt;/B&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Project manager&lt;/SPAN&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;&lt;FONT face="Times New Roman" size="3"&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Direct: +45 87 400 311&lt;/SPAN&gt;&lt;/FONT&gt;&lt;SPAN&gt;&lt;FONT color="#000000" face="Times New Roman" size="3"&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;FONT color="#000000"&gt;Email:&lt;/FONT&gt;&lt;U&gt;&lt;FONT color="#000000"&gt;&lt;/FONT&gt;&lt;SPAN&gt;pkh@develco.dk&lt;/SPAN&gt;&lt;/U&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;B&gt;&lt;SPAN&gt;DEVELC&lt;/SPAN&gt;&lt;/B&gt;&lt;B&gt;&lt;SPAN&gt;O&lt;/SPAN&gt;&lt;/B&gt;&lt;B&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/B&gt;&lt;B&gt;&lt;SPAN&gt;&lt;FONT color="#000000" face="Times New Roman" size="3"&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/B&gt;&lt;B&gt;&lt;SPAN&gt;A/S&lt;/SPAN&gt;&lt;/B&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;&lt;FONT face="Times New Roman" size="3"&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Olof Palmes Allé 40&lt;/SPAN&gt;&lt;/FONT&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;&lt;FONT face="Times New Roman" size="3"&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;SPAN&gt;DK-8200 Aarhus N&lt;/SPAN&gt;&lt;/FONT&gt;&lt;SPAN&gt;&lt;FONT color="#000000" face="Times New Roman" size="3"&gt;&lt;BR /&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;FONT color="#000000"&gt;Pho&lt;/FONT&gt;&lt;FONT color="#000000"&gt;: +45 87 400 300&lt;BR /&gt;Fax: +45 87 400 333&lt;BR /&gt;web: &lt;A href="http://www.develco.dk/" rel="nofollow" target="_blank"&gt;www.develco.dk&lt;/A&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Feb 2007 16:43:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145374#M3082</guid>
      <dc:creator>PeterKirketerp</dc:creator>
      <dc:date>2007-02-19T16:43:20Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52233 bootloader with TFTP and DHCP client</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145375#M3083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Peter&lt;BR /&gt;&lt;BR /&gt;The uTasker is free for non-commercial use - see the application form on the web site (which I have sent to you by email).&lt;BR /&gt;Commercial evaluation is free for 30 day including full email support.&lt;BR /&gt;If a project becomes commercial, a royalty free project license costs $485 including an additional 3 months personal email support.&lt;BR /&gt;&lt;BR /&gt;I think that in your case the MULTISTART support will be a very powerful method to achieve what you require.&lt;BR /&gt;If you would like to strip down to a minimum boot loader here are the code sizes to be reconned with using the uTasker elements:&lt;BR /&gt;- DHCP 4.5k (this does full support including randomising and lease periods control to up to 100 years so could probably be reduced quite a lot if critical)&lt;BR /&gt;- TFTP client/server 2.4k (the PUT method could probally be removed to make it a bit smaller)&lt;BR /&gt;- File system 1.5k&lt;BR /&gt;- Ethernet 0.7k&lt;BR /&gt;- Hardware driver incl. interrupst etc. (this is not so clear but maybe 1k..2k ?)&lt;BR /&gt;- ARP - 2.9k&lt;BR /&gt;- IP - 1.4k&lt;BR /&gt;- UDP - 1.4k&lt;BR /&gt;- OS support in the boot phase (makes it easier but could be stripped) 1.3k plus drivers for internal timers and messaging (if needed) around 2k.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Mark&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Feb 2007 19:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145375#M3083</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2007-02-19T19:53:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52233 bootloader with TFTP and DHCP client</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145376#M3084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;Hi Mark&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;Thanks for the uTasker it is GREATE, especially the Visual Studion simulator.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;I am now up a running with the bootloader and the stack you send me!!!, It was very easy (good documentation and a nice tutorial).&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;I have been working with the TCP/IP stack from InterNiche for some months, but in the future I will recommend the uTasker. One of the greats benefit is the simulator and the documentation.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;&lt;FONT face="Times New Roman"&gt;Keep on the good work Mark&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;Best regards&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;&lt;FONT color="#000000"&gt;&lt;FONT face="Times New Roman"&gt;&lt;SPAN&gt;Peter Kirketerp&lt;/SPAN&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT color="#000000" face="Times New Roman" size="3"&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT color="#000000" face="Times New Roman" size="3"&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;FONT color="#000000" face="Times New Roman" size="3"&gt;&lt;/FONT&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2007 06:39:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52233-bootloader-with-TFTP-and-DHCP-client/m-p/145376#M3084</guid>
      <dc:creator>PeterKirketerp</dc:creator>
      <dc:date>2007-02-22T06:39:06Z</dc:date>
    </item>
  </channel>
</rss>