<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Flash programming with coldfire</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-with-coldfire/m-p/144998#M3027</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The boot flash is located at FF800000, but for my user code I load at FFE00000. The code space is located at E00000... for the eval boards from Freescale.&lt;BR /&gt;&lt;BR /&gt;Code Flasher allows you to select the 5485evb(boot), which defaults to FF800000 or the code space default is E0000000.&lt;BR /&gt;&lt;BR /&gt;I suggest you try both FF800000 or FFE00000. Also look at your boot rom hw cfg pins.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 11 Feb 2007 16:26:02 GMT</pubDate>
    <dc:creator>Marreshe</dc:creator>
    <dc:date>2007-02-11T16:26:02Z</dc:date>
    <item>
      <title>Flash programming with coldfire</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-with-coldfire/m-p/144997#M3026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I am using MCF5485 with coldfire development kit to build an application.&lt;/DIV&gt;&lt;DIV&gt;My program is downloaded to RAM by default when I use BDM and is working fine.&lt;/DIV&gt;&lt;DIV&gt;I wish to download it to flash using the flash programmer tool given with the freescale codewarrior IDE.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;1. I built the application giving the target name as "M5485 ROM". A memory file called "M5484EVB_ROM.elf.xMAP" is created. It shows that my code starts at FE001BF8 which is a boot flash location. Should'nt this&amp;nbsp;show one of the code flash locations?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;2. I&amp;nbsp;am using flash programmer to write the code to the flash. I selected the Flash Memory Base Address as 0x40000000 as shown by my memory configuration file for the code flash's&amp;nbsp;base address.When I try to erase a sector of flash memory, the status shown is "Erase succeeded", but the blank check returns an error: Blank Check failed and the details button says "no error". I proceeded to program /verify and tried to program, which says 0 bytes programmed.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Am I missing something to setup for writing to flash?&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Feb 2007 12:31:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-with-coldfire/m-p/144997#M3026</guid>
      <dc:creator>Poornima</dc:creator>
      <dc:date>2007-02-11T12:31:33Z</dc:date>
    </item>
    <item>
      <title>Re: Flash programming with coldfire</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-with-coldfire/m-p/144998#M3027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The boot flash is located at FF800000, but for my user code I load at FFE00000. The code space is located at E00000... for the eval boards from Freescale.&lt;BR /&gt;&lt;BR /&gt;Code Flasher allows you to select the 5485evb(boot), which defaults to FF800000 or the code space default is E0000000.&lt;BR /&gt;&lt;BR /&gt;I suggest you try both FF800000 or FFE00000. Also look at your boot rom hw cfg pins.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Feb 2007 16:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-with-coldfire/m-p/144998#M3027</guid>
      <dc:creator>Marreshe</dc:creator>
      <dc:date>2007-02-11T16:26:02Z</dc:date>
    </item>
  </channel>
</rss>