<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: MCF52235: EzPort write enable</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52235-EzPort-write-enable/m-p/144908#M3019</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;I'll try to upload the waveforms again...&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Sep 2007 01:55:33 GMT</pubDate>
    <dc:creator>Petter</dc:creator>
    <dc:date>2007-09-12T01:55:33Z</dc:date>
    <item>
      <title>MCF52235: EzPort write enable</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52235-EzPort-write-enable/m-p/144907#M3018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;PRE&gt;I can read FLASH data through the EzPort just fine. However, if I try
to set the write enable bit by issuing a WREN(0x6) command, the status
register read back using RDSR(0x5) does not return anything but zero.
As you see from the enclosed analyzer waveforms I send 0x06, 0x05, and
0x00 (EZBYTE1,2, and 3) but the output is zero.

I've also tried to do a RDSR in a loop, but I still only get zero as
output. I have no problem of issuing a READ(0x3) to read data from the
FLASH. I'm using the M52235EVB board. Any ideas or pointers to
documentation/erratas?


&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 08:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52235-EzPort-write-enable/m-p/144907#M3018</guid>
      <dc:creator>Petter</dc:creator>
      <dc:date>2020-10-29T08:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52235: EzPort write enable</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52235-EzPort-write-enable/m-p/144908#M3019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;I'll try to upload the waveforms again...&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2007 01:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52235-EzPort-write-enable/m-p/144908#M3019</guid>
      <dc:creator>Petter</dc:creator>
      <dc:date>2007-09-12T01:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: MCF52235: EzPort write enable</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52235-EzPort-write-enable/m-p/144909#M3020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;The reason was that I did not release RCON* after I asserted it initially. In this mode I could read the FLASH just fine, but not do any writes to the control register. I can now both read and write to the FLASH from the EzPort.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 16 Sep 2007 22:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF52235-EzPort-write-enable/m-p/144909#M3020</guid>
      <dc:creator>Petter</dc:creator>
      <dc:date>2007-09-16T22:16:46Z</dc:date>
    </item>
  </channel>
</rss>