<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flash programming automation for Coldfire M52233 with USB-TAP? in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-automation-for-Coldfire-M52233-with-USB-TAP/m-p/144298#M2878</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;how can I automate the programming of the built in flash of the Coldfire M52233? I would like to use the USB TAP hardware for ISP in the production line. The programming files were made with the CodeWarrior Development Studio. I don't care about which software language and method is used. As long as I get this task controlled with LabView or C++.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Your help is much appreciated because I have not found any hint in the documentation / help files / forums / Google.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks a lot!&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Sep 2007 15:45:22 GMT</pubDate>
    <dc:creator>nasowasauch</dc:creator>
    <dc:date>2007-09-04T15:45:22Z</dc:date>
    <item>
      <title>Flash programming automation for Coldfire M52233 with USB-TAP?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-automation-for-Coldfire-M52233-with-USB-TAP/m-p/144298#M2878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;how can I automate the programming of the built in flash of the Coldfire M52233? I would like to use the USB TAP hardware for ISP in the production line. The programming files were made with the CodeWarrior Development Studio. I don't care about which software language and method is used. As long as I get this task controlled with LabView or C++.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Your help is much appreciated because I have not found any hint in the documentation / help files / forums / Google.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks a lot!&lt;/SPAN&gt;&lt;BR /&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Sep 2007 15:45:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-automation-for-Coldfire-M52233-with-USB-TAP/m-p/144298#M2878</guid>
      <dc:creator>nasowasauch</dc:creator>
      <dc:date>2007-09-04T15:45:22Z</dc:date>
    </item>
    <item>
      <title>Re: Flash programming automation for Coldfire M52233 with USB-TAP?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-automation-for-Coldfire-M52233-with-USB-TAP/m-p/144299#M2879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;What kind of&amp;nbsp; USB JTAG programmer do you have? What kind of input files does it accept? SVF? Do you have other devices in your JTAG chain?&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Sep 2007 17:48:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-automation-for-Coldfire-M52233-with-USB-TAP/m-p/144299#M2879</guid>
      <dc:creator>Petter</dc:creator>
      <dc:date>2007-09-07T17:48:12Z</dc:date>
    </item>
    <item>
      <title>Re: Flash programming automation for Coldfire M52233 with USB-TAP?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-automation-for-Coldfire-M52233-with-USB-TAP/m-p/144300#M2880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I'm using the freescale Codewarrior USB TAP BDM device. There are no other devices in the JTAG chain.&lt;BR /&gt;&lt;BR /&gt;BUT this is not the point. I need to program the M52233 incircuit for serial production. How can I achieve that? There are two possibilities:&lt;BR /&gt;1. I use the USB TAP with some kind of remote software or&lt;BR /&gt;2. I use a third party equipment to do that. Do you have some recomendations?&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2007 14:40:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-automation-for-Coldfire-M52233-with-USB-TAP/m-p/144300#M2880</guid>
      <dc:creator>nasowasauch</dc:creator>
      <dc:date>2007-09-10T14:40:05Z</dc:date>
    </item>
    <item>
      <title>Re: Flash programming automation for Coldfire M52233 with USB-TAP?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-automation-for-Coldfire-M52233-with-USB-TAP/m-p/144301#M2881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;I'm using the freescale Codewarrior USB TAP BDM device. There are no other devices in the JTAG chain.&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;PRE&gt;I'm assuming this is the P&amp;amp;E Microcomputer Systems Inc. USB Multilink.&lt;/PRE&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;1. I use the USB TAP with some kind of remote software or&lt;DIV&gt;&lt;/DIV&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;I don't think P&amp;amp;E has published the programming interface for this programmer. I think batch programming is available only for the more expensive models like the Cyclone MAX.&lt;BLOCKQUOTE&gt;&lt;HR /&gt;2. I use a third party equipment to do that. Do you have some recomendations?&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;I'm currently developing my own solution. It's using the EzPort. But it requires that the EzPort is available as a connector. I want to use JTAG for testing the board so I was hoping that there was a way to toggle the EzPort pins into the core from JTAG. But I can't seem to find any documentation on how to do that. I can of course connect a JTAG buffer or some other low cost part to the EzPort pins, but this will add cost (if you have spare/share pins on a JTAG device already in your design you can of course use that)&lt;BR /&gt;&lt;BR /&gt;If somebody has any information on how to program the FLASH or control the EzPort from JTAG I would be very happy.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 08:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Flash-programming-automation-for-Coldfire-M52233-with-USB-TAP/m-p/144301#M2881</guid>
      <dc:creator>Petter</dc:creator>
      <dc:date>2020-10-29T08:45:19Z</dc:date>
    </item>
  </channel>
</rss>