<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: M5213EVB connection problem over QSPI</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5213EVB-connection-problem-over-QSPI/m-p/144270#M2867</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Feb 2007 19:15:27 GMT</pubDate>
    <dc:creator>fiskom</dc:creator>
    <dc:date>2007-02-02T19:15:27Z</dc:date>
    <item>
      <title>M5213EVB connection problem over QSPI</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5213EVB-connection-problem-over-QSPI/m-p/144269#M2866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hello&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've got the M5213EVB and I try to connect it over QSPI with an EEPROM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I checked all pins of the EEPROM with an oscilloscope, and everything is how I imagined.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But the SlaveOutput.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So can someone take a look at my code (only the QSPI code with an simple routine to write and read data over QSPI).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The important parameters of the EEPROM are listed at the top of the .c-file&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks in advance for help,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2007 18:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5213EVB-connection-problem-over-QSPI/m-p/144269#M2866</guid>
      <dc:creator>fiskom</dc:creator>
      <dc:date>2007-02-02T18:33:48Z</dc:date>
    </item>
    <item>
      <title>Re: M5213EVB connection problem over QSPI</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5213EVB-connection-problem-over-QSPI/m-p/144270#M2867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2007 19:15:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5213EVB-connection-problem-over-QSPI/m-p/144270#M2867</guid>
      <dc:creator>fiskom</dc:creator>
      <dc:date>2007-02-02T19:15:27Z</dc:date>
    </item>
    <item>
      <title>Re: M5213EVB connection problem over QSPI</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5213EVB-connection-problem-over-QSPI/m-p/144271#M2868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I assume that the QSPI interface of the MCF5213 is identical to the one of the 5235 (and the other coldfires) ...&lt;BR /&gt;I've had a short look into your sourcecode and noticed one possible problem.&lt;BR /&gt;On line 125 you set up QAR to access the command RAM and write 1 :smileyalert: word into it. Then you write 3 :smileyalert: words into the transmit RAM.&lt;BR /&gt;This will at best transmit only the first word to over QSPI to your EEPROM.&lt;BR /&gt;&lt;BR /&gt;HTH&lt;BR /&gt;Stamatis&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Feb 2007 22:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M5213EVB-connection-problem-over-QSPI/m-p/144271#M2868</guid>
      <dc:creator>stzari</dc:creator>
      <dc:date>2007-02-02T22:13:08Z</dc:date>
    </item>
  </channel>
</rss>