<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using the 547X as a PCI device - not controller in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-the-547X-as-a-PCI-device-not-controller/m-p/144194#M2857</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Has anyone ever done this before?&amp;nbsp; That is has anyone ever used the 5475's PCI controller to create 5475 based PCI card?&lt;BR /&gt;&lt;BR /&gt;The MBAR1 window being soo large (1 GB) does seem to be a limiting factor, but perhaps this would work in&amp;nbsp; a 64-bit system?&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jun 2007 23:07:01 GMT</pubDate>
    <dc:creator>C_G_B_Spender</dc:creator>
    <dc:date>2007-06-19T23:07:01Z</dc:date>
    <item>
      <title>Using the 547X as a PCI device - not controller</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-the-547X-as-a-PCI-device-not-controller/m-p/144193#M2856</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I have a functional 5474 design, running an RTOS,&amp;nbsp;that communicates with a host computer using LAN, USB, or Serial.&amp;nbsp; I have been asked convert this board into a&amp;nbsp;conventional 32-bit, 33Mhz, PCI plug-in card.&amp;nbsp; Because I knew I might be asked to do this, I used a multiplexed add/data bus and kept the PCI pins open.&amp;nbsp; The card will NOT be the host or system controller.&amp;nbsp; Initially, it will reside in a&amp;nbsp;Windows box followed by support for&amp;nbsp;Linux.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I am looking for guidance, warnings,&amp;nbsp;drivers/code... basically help of any kind connecting the 5474 to the PCI bus and communicating with the system host.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I envision a simple protocol for communicating with the&amp;nbsp;system controller.&amp;nbsp;&amp;nbsp;For example, the controller sends data (a few kbytes max, normally &amp;lt; 128 bytes) across the PCI bus which gets stuffed into the cards memory/fifo/? and then interrupts the Coldfire somehow to process the data.&amp;nbsp; The Coldfire reads the data, does something,&amp;nbsp;and replies by sending&amp;nbsp;some data (normally &amp;lt; 128 bytes, could be 1Mbyte) across the PCI bus using a similar "write and interrupt" mechanism.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any help would be greatly appreciated.&amp;nbsp; My PCI knowledge is pretty basic.&amp;nbsp; I know the host discovers the PCI devices, devices requests memory/io space, the host tells the device where to go (in memory that is &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt;), and then the device is considered&amp;nbsp;"configured".&amp;nbsp; I have used the AMCC 5933 PCI MatchMaker in a previous 68k design so I familiar with the fifo/doorbell mechanism for a PCI device to communicate with a PCI host/master.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Feb 2007 22:32:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-the-547X-as-a-PCI-device-not-controller/m-p/144193#M2856</guid>
      <dc:creator>droidian</dc:creator>
      <dc:date>2007-02-01T22:32:52Z</dc:date>
    </item>
    <item>
      <title>Re: Using the 547X as a PCI device - not controller</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-the-547X-as-a-PCI-device-not-controller/m-p/144194#M2857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Has anyone ever done this before?&amp;nbsp; That is has anyone ever used the 5475's PCI controller to create 5475 based PCI card?&lt;BR /&gt;&lt;BR /&gt;The MBAR1 window being soo large (1 GB) does seem to be a limiting factor, but perhaps this would work in&amp;nbsp; a 64-bit system?&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jun 2007 23:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Using-the-547X-as-a-PCI-device-not-controller/m-p/144194#M2857</guid>
      <dc:creator>C_G_B_Spender</dc:creator>
      <dc:date>2007-06-19T23:07:01Z</dc:date>
    </item>
  </channel>
</rss>