<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: MCF5329EVB - Chip select signals and memory mapping problems</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329EVB-Chip-select-signals-and-memory-mapping-problems/m-p/142673#M2593</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Thanks for the reply Paolo.&lt;BR /&gt;I have already read the MCF5329 Reference Manual and the MCF5329 Hardware Specification and&lt;BR /&gt;I have set the flex-bus for accessing Compact Flash in this way:&lt;BR /&gt;&lt;BR /&gt;CSAR1 = 0x02000000;&lt;BR /&gt;CSCR1 = 0x002A3780; //as MCF5329 Hardware Specification&lt;BR /&gt;CSMR1 = 0x01FF0001; // Compact Flash with 32MB of memory&lt;BR /&gt;&lt;BR /&gt;I have try to write from the 0x02000000 address but I can't.&lt;BR /&gt;Have I to set something else?&lt;BR /&gt;Thank you very much,&lt;BR /&gt;&lt;BR /&gt;mastro&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jan 2007 18:57:27 GMT</pubDate>
    <dc:creator>mastro</dc:creator>
    <dc:date>2007-01-15T18:57:27Z</dc:date>
    <item>
      <title>MCF5329EVB - Chip select signals and memory mapping problems</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329EVB-Chip-select-signals-and-memory-mapping-problems/m-p/142671#M2591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the Coldfire MCF5329 evaluation board and I have to access with the Compact Flash.Which is the initial address that I have to set for read and write to?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The Compact Flash is mapped with the chip select 1 signal, but how can I set it?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;How is organized the memory?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank in advance!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;mastro&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jan 2007 00:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329EVB-Chip-select-signals-and-memory-mapping-problems/m-p/142671#M2591</guid>
      <dc:creator>mastro</dc:creator>
      <dc:date>2007-01-13T00:33:18Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5329EVB - Chip select signals and memory mapping problems</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329EVB-Chip-select-signals-and-memory-mapping-problems/m-p/142672#M2592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Depends on how your LCF is organized (how software fits on hardware)&lt;BR /&gt;And finally Chips Selects base address configuration is important.&lt;BR /&gt;You have to read more about ColdFire or at least entire Chip Select memory chapter&lt;BR /&gt;&lt;BR /&gt;Good luck&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Jan 2007 09:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329EVB-Chip-select-signals-and-memory-mapping-problems/m-p/142672#M2592</guid>
      <dc:creator>PaoloRenzo</dc:creator>
      <dc:date>2007-01-13T09:22:14Z</dc:date>
    </item>
    <item>
      <title>Re: MCF5329EVB - Chip select signals and memory mapping problems</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329EVB-Chip-select-signals-and-memory-mapping-problems/m-p/142673#M2593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;Thanks for the reply Paolo.&lt;BR /&gt;I have already read the MCF5329 Reference Manual and the MCF5329 Hardware Specification and&lt;BR /&gt;I have set the flex-bus for accessing Compact Flash in this way:&lt;BR /&gt;&lt;BR /&gt;CSAR1 = 0x02000000;&lt;BR /&gt;CSCR1 = 0x002A3780; //as MCF5329 Hardware Specification&lt;BR /&gt;CSMR1 = 0x01FF0001; // Compact Flash with 32MB of memory&lt;BR /&gt;&lt;BR /&gt;I have try to write from the 0x02000000 address but I can't.&lt;BR /&gt;Have I to set something else?&lt;BR /&gt;Thank you very much,&lt;BR /&gt;&lt;BR /&gt;mastro&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2007 18:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MCF5329EVB-Chip-select-signals-and-memory-mapping-problems/m-p/142673#M2593</guid>
      <dc:creator>mastro</dc:creator>
      <dc:date>2007-01-15T18:57:27Z</dc:date>
    </item>
  </channel>
</rss>