<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Linux booting halts 2 (a bit more)</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142094#M2519</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks guys,&lt;BR /&gt;&lt;BR /&gt;This was just the info I needed. &lt;BR /&gt;I've started working on coldfire-linux almost 2 months now, and&lt;BR /&gt;this trick helped a great deal. &lt;BR /&gt;&lt;BR /&gt;I don't have the final answer to the "kernel panic", but I got it running with a workaround: I exported the original directory in which the root-file system is generated by LTIB (/my-ltib-root-dir/rootfs) directly, in stead of using the link in /tftpboot.&lt;BR /&gt;&lt;BR /&gt;I'm new to linux but for your information, this is how it worked:&lt;BR /&gt;I used the /etc/exports - file and added:&lt;BR /&gt;/path-to-my-ltib-root-dir/rootfs 192.168.1.202(rw,async,no_root_squash) &lt;BR /&gt;&lt;BR /&gt;in which "192.168.1.202" is the IP-address of my target board&lt;BR /&gt;&lt;BR /&gt;Remarks:&lt;BR /&gt;* In the setup for the command-line (colilo&amp;gt;set cl mac0= ... etc etc) refer directly to: &lt;BR /&gt;nfsroot=my-host-IP-address:/path-to-my-ltib-root-dir/rootfs&lt;BR /&gt;&lt;BR /&gt;* When I do the start-up sequence I have to switch serial communication to 115200 baud-rate, after the linux kernel has started.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Jul 2006 16:45:59 GMT</pubDate>
    <dc:creator>dyon</dc:creator>
    <dc:date>2006-07-17T16:45:59Z</dc:date>
    <item>
      <title>Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142085#M2510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;hi to all!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So, i have a 547x/548x lite evaluation board with MCF5484 processor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i build a linux image with LTIB and succesfully downloaded and executed colilo.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i have also downloaded my linux kernel image called "vmlinux.bin". Following the freescale's linux target image user's guide (specific for MCF54x5 and MCF54x4) after the download, it says to type "config save" and "g 2000" commands...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the commands output is shown below:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;set cl mac0=00:04:9f:b5:69:3a noinitrd root=/dev/nfs rw nfsroot=192.168.1.39:/tftpboot/ltib ip= 192.168.1.40:192.168.1.39:192.168.1.1:255.255.255.0:C&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;oldFire:eth0&lt;/SPAN&gt;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif"&gt;&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;&lt;/A&gt;&lt;SPAN&gt;ff mtdparts=phys_mapped_flash:256k(Colilo),2816k(User)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Command line:'mac0=00:04:9f:b5:69:3a noinitrd root=/dev/nfs rw nfsroot=192.168.1.39:/tftpboot/ltib ip= 192.168.1.40:192.168.1.39:192.168.1.1:255.255.255.0:C&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;oldFire:eth0&lt;/SPAN&gt;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif"&gt;&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;&lt;/A&gt;&lt;SPAN&gt;ff mtdparts=phys_mapped_flash:256k(Colilo),2816k(User)'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;set kfl 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;set mac 00:04:9f:b5:69:3a&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MAC address:'00:04:9f:b5:69:3a'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;set ip 192.168.1.40&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;IP address:'192.168.1.40'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;set server 192.168.1.39&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TFTP Server: '192.168.1.39'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;set netmask 255.255.255.0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Netmask: '255.255.255.0'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;set gw 192.168.1.1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Gateway IP address:'192.168.1.1'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;set image vmlinux.bin&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Image: 'vmlinux.bin'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;tftp 0x1000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TFTP download:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Download address:1000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Using FEC:0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Board MAC: '00:04:9f:b5:69:3a'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Board IP: '192.168.1.40'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Board netmask:'255.255.255.0'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Board gateway:'192.168.1.1'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;TFTP server:'192.168.1.39'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Image:'vmlinux.bin'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Initializing TCP/IP stack...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Receiving file 'vmlinux.bin' from '192.168.1.39'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;-&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Image size = 2699264 bytes&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;# so the download succeed succesfully!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;# but now:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;config save&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Code Manufactor detected = F000 (S/B 0x89)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Code Device detected = F000 (S/B 0x8803)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Boot Device detected = 88C5 (S/B 0x88C3)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Burning 848 bytes to flash 0xf0020000 from 0x1febc60&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Starting flash sector: 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Erase 1 128K sectors, starting 1, address f0020000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Retry = 600000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Problems with sector erasing!...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Programing...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Retry = 1024&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Problems with data writing!...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;data:436F in flash: F002 addr:20000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Problems with data writing!...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Retry = 1024&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Problems with data writing!...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;data:4C69 in flash: F002 addr:20002&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Problems with data writing!...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Retry = 1024&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Problems with data writing!...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;data:4C6F in flash: F002 addr:20004&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.....&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Problems with data writing!...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;data:BFC4 in flash: F002 addr:2034E&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Problems with data writing!...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;848 bytes written&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;# i tried to run the image instead&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colilo&amp;gt;g 2000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Linux version 2.6.10 (gianluca@gianluca) (gcc version 3.4.0) #1 Fri Jun 30 15:30:47 CEST 2006&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;starting up linux rev 0.2: startmem 0xc0296000, size 61MB&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Built 1 zonelists&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Kernel command line: mac0=00:04:9f:b5:69:3a noinitrd root=/dev/nfs rw nfsroot=192.168.1.39:/tftpboot/ltib ip=192.168.1.40:192.168.1.39:192.168.1.1:255.255.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;255.0:ColdFire:eth0&lt;/SPAN&gt;&lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif"&gt;&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;&lt;/A&gt;&lt;SPAN&gt;ff mtdparts=phys_mapped_flash:256k(Colilo),2816k(User)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PID hash table entries: 512 (order: 9, 8192 bytes)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;RTC driver is not initialized yet, returning 1970.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Console: colour dummy device 80x25&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Dentry cache hash table entries: 16384 (order: 3, 65536 bytes)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Inode-cache hash table entries: 8192 (order: 2, 32768 bytes)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Memory: 62376k/65536k available (1936k kernel code, 1032k data, 96k init)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mount-cache hash table entries: 1024 (order: 0, 8192 bytes)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NET: Registered protocol family 16&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Linux/m68k PCI BIOS32 revision 0.05&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ColdFire PCI Host Bridge (Rev. 0) detected&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PCI: Probing PCI hardware&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;ColdFire internal SEC driver version 0.11&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;# and here the booting halts&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could anyone help me?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks, Gianluca Salvador&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jul 2006 15:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142085#M2510</guid>
      <dc:creator>Gian</dc:creator>
      <dc:date>2006-07-05T15:11:18Z</dc:date>
    </item>
    <item>
      <title>Linux booting halts 2 (a bit more)</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142086#M2511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi to all!&lt;BR /&gt;Thanks to Coray for the suggestion and for his linux.bin image:&lt;BR /&gt;I tried it and works for itself, but now i have problems with my server PC, not with linux image. Infact as shown in the output below, target linux cannot mount /tftpboot/ltib because the server returned error (-13 it says). &lt;BR /&gt;The nfs server was configurated and restarted as sad in the user's guide.&lt;BR /&gt;I looked in my /dev directory but i didn't find any nfs device, so i thought that it could be the problem. Isn't it? &lt;BR /&gt;If so, how could i solve it?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;As you request me by mail i show you also the colilo "?" output&lt;BR /&gt;now it works correctly and my beginning problem was a bit stupid: i didn't know that colilo works by default at 19200 baud rate, while my coldfire and minicom was setted for 115200! &lt;BR /&gt;So I seen garbage when i tried to run colilo!!!&lt;BR /&gt;&lt;BR /&gt;Another thing: where can i found documentation that explain the rules for set colilo and colilo kernel command line? &lt;BR /&gt;&lt;BR /&gt;Thanks and regards,&lt;BR /&gt;Gianluca Salvador&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;colilo&amp;gt;?&lt;BR /&gt;Coldfire Linux Loader&lt;BR /&gt; Platform: -- Colilo M547X - M548X Bootloader --&lt;BR /&gt; -- 2005 Freescale/2004 Motorola(c) --&lt;BR /&gt;Commands available:&lt;BR /&gt; b - boot default image&lt;BR /&gt; m [addr] - memory dump at addr&lt;BR /&gt; g [xfer_addr] - go to xfer_addr&lt;BR /&gt; l [down_addr] [port] - load image from port&lt;BR /&gt; f [down_addr] [size] [val] - fill memory with value&lt;BR /&gt; pl [addr] [val] - set the 32 bit value at address&lt;BR /&gt; ps [addr] [val] - set the 16 bit value at address&lt;BR /&gt; pc [addr] [val] - set the 8 bit value at address&lt;BR /&gt; rl [addr] - read a 32 bit value at address&lt;BR /&gt; rs [addr] - read a 16 bit value at address&lt;BR /&gt; rc [addr] - read a 8 bit value at address&lt;BR /&gt; c [source_addr] [dest_addr] [size] - copy memory&lt;BR /&gt; d [source_addr] [dest_addr] [size] - decompress image&lt;BR /&gt; x [down_addr] [dest_addr] [xfer_addr] [port] - cmds l, d, g&lt;BR /&gt; z [source_addr] [dest_addr] [xfer_addr] - cmds d, g&lt;BR /&gt;TCP/IP commands:&lt;BR /&gt; set mac [MAC address] - set board MAC address&lt;BR /&gt; set ip [IP address] - set board IP address&lt;BR /&gt; set gw [IP address] - set board gateway address&lt;BR /&gt; set netmask [IP address] - set board netmask&lt;BR /&gt; set server [IP address] - set address of TFTP server for TFTP download&lt;BR /&gt; set image [Image name] - set name of image for downloading&lt;BR /&gt; set fec [fec number] - select FEC to use&lt;BR /&gt; set cl [command_line] - set kernel command line&lt;BR /&gt; set kfl [0/1] - set to 1 if kernel image is in flash, 0 - otherwise&lt;BR /&gt; tftp [down_addr] - download image from TFTP server&lt;BR /&gt; bootp - request bootp information&lt;BR /&gt; Where:&lt;BR /&gt; flash_addr - address in flash to start burning from&lt;BR /&gt; xfer_addr: hex address to start running at&lt;BR /&gt; down_addr: hex address of downloaded image&lt;BR /&gt; dest_addr: hex address of image destination&lt;BR /&gt; source_addr: hex address of compressed image&lt;BR /&gt; size: size of compressed image&lt;BR /&gt; port: 0 = /dev/ttyS0, 1 = /dev/ttyS1&lt;BR /&gt; IP address: IP address in format xxx.xxx.xxx.xxx&lt;BR /&gt; MAC address: MAC address in format xx:xx:xx:xx:xx:xx&lt;BR /&gt; Image name: string, filename&lt;BR /&gt; fec number: 0 or 1&lt;BR /&gt; Default values for paramaters:&lt;BR /&gt; down_addr: 1000&lt;BR /&gt; source_addr: 7fc10000&lt;BR /&gt; dest_addr: 1000&lt;BR /&gt; xfer_addr: 2000&lt;BR /&gt; flash_addr: 0&lt;BR /&gt; size: 130000&lt;BR /&gt; downloadPort: 1&lt;BR /&gt; kernel command line: root=/dev/ram&lt;BR /&gt; kernel image in flash: no&lt;BR /&gt; start booting automaticaly: no&lt;BR /&gt; Current TCP/IP configuration:&lt;BR /&gt; Board MAC: 00:04:9f:b5:69:3a&lt;BR /&gt; Board IP: 192.168.1.40&lt;BR /&gt; Netmask: 255.255.255.0&lt;BR /&gt; Board gateway: 192.168.10.1&lt;BR /&gt; TFTP server: 192.168.1.39&lt;BR /&gt; Image name: linux.bin&lt;BR /&gt;colilo&amp;gt;&lt;BR /&gt;&lt;BR /&gt;colilo&amp;gt;g 2000&lt;BR /&gt;Linux version 2.6.10 (coray@fastball) (gcc version 3.4.0) #3 Thu Jul 6 16:48:26 CDT 2006&lt;BR /&gt;starting up linux rev 0.2: startmem 0xc0270000, size 61MB&lt;BR /&gt;Built 1 zonelists&lt;BR /&gt;Kernel command line: mac0=00:04:9f:b5:69:3a noinitrd root=/dev/nfs rw nfsroot=192.168.1.39:/tftpboot/ltib ip=192.168.1.40:192.168.1.39:192.168.1.1:255.255.255.0:ColdFire:eth0&lt;IMG alt=":smileysurprised:" class="emoticon emoticon-smileysurprised" id="smileysurprised" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-surprised.gif" title="Smiley Surprised" /&gt;f&lt;BR /&gt;f&lt;BR /&gt;PID hash table entries: 512 (order: 9, 8192 bytes)&lt;BR /&gt;RTC driver is not initialized yet, returning 1970.&lt;BR /&gt;Console: colour dummy device 80x25&lt;BR /&gt;Dentry cache hash table entries: 16384 (order: 3, 65536 bytes)&lt;BR /&gt;Inode-cache hash table entries: 8192 (order: 2, 32768 bytes)&lt;BR /&gt;Memory: 62528k/65536k available (1800k kernel code, 1016k data, 96k init)&lt;BR /&gt;Mount-cache hash table entries: 1024 (order: 0, 8192 bytes)&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;Linux/m68k PCI BIOS32 revision 0.05&lt;BR /&gt;ColdFire PCI Host Bridge (Rev. 0) detected&lt;BR /&gt;PCI: Probing PCI hardware&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;Initialize Multi-channel DMA API Alpha v0.3 (2004-04-26)&lt;BR /&gt;Initializing Cryptographic API&lt;BR /&gt;rtc: RV5C387 RTC driver successfully loaded&lt;BR /&gt;MCF547x/8x DSPI device driver installed&lt;BR /&gt;Coldfire DSPI driver is loaded&lt;BR /&gt;ISA-Philips-Basic-CAN memory mapped CAN Driver 3.1_ColdFire_FlexCAN (c) Jul 6 2006 16:22:57&lt;BR /&gt;ColdFire internal UART serial driver version 1.00&lt;BR /&gt;ttyS0 at 0xe0008600 (irq = 99) is a builtin ColdFire UART&lt;BR /&gt;ttyS1 at 0xe0008700 (irq = 98) is a builtin ColdFire UART&lt;BR /&gt;ttyS2 at 0xe0008800 (irq = 97) is a builtin ColdFire UART&lt;BR /&gt;ttyS3 at 0xe0008900 (irq = 96) is a builtin ColdFire UART&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler anticipatory registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered&lt;BR /&gt;RAMDISK driver initialized: 16 RAM disks of 8192K size 1024 blocksize&lt;BR /&gt;ColdFire internal FEC driver version 0.11&lt;BR /&gt;Loaded prism54 driver, version 1.2&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;i2c-algo-mcf.o: I2C ColdFire algorithm module is loaded.&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;IP: routing cache hash table of 1024 buckets, 8Kbytes&lt;BR /&gt;TCP: Hash tables configured (established 8192 bind 16384)&lt;BR /&gt;Initializing IPsec netlink socket&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;NET: Registered protocol family 15&lt;BR /&gt;IP-Config: Complete:&lt;BR /&gt; device=eth0, addr=192.168.1.40, mask=255.255.255.0, gw=192.168.1.1,&lt;BR /&gt; host=ColdFire, domain=, nis-domain=(none),&lt;BR /&gt; bootserver=192.168.1.39, rootserver=192.168.1.39, rootpath=&lt;BR /&gt;Looking up port of RPC 100003/2 on 192.168.1.39&lt;BR /&gt;Looking up port of RPC 100005/1 on 192.168.1.39&lt;BR /&gt;Root-NFS: Server returned error -13 while mounting /tftpboot/ltib&lt;BR /&gt;VFS: Unable to mount root fs via NFS, trying floppy.&lt;BR /&gt;VFS: Cannot open root device "nfs" or unknown-block(2,0)&lt;BR /&gt;Please append a correct "root=" boot option&lt;BR /&gt;Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2006 16:51:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142086#M2511</guid>
      <dc:creator>Gian</dc:creator>
      <dc:date>2006-07-07T16:51:51Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142087#M2512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello all&lt;BR /&gt;&lt;BR /&gt;Someone looks have send to Gian good answer for this trouble, is it possible to have here this answer? I have exactly the same problem&lt;BR /&gt;Linux boot and stop after display:&lt;BR /&gt;&lt;BR /&gt;Coldfire internal SEC driver version 0.11&lt;BR /&gt;&lt;BR /&gt;Please help&lt;BR /&gt;&lt;BR /&gt;Thanks a lot&lt;BR /&gt;&lt;BR /&gt;Olivier&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2006 00:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142087#M2512</guid>
      <dc:creator>OL</dc:creator>
      <dc:date>2006-07-12T00:23:54Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142088#M2513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Olivier!&lt;BR /&gt;&lt;BR /&gt;This is a kernel configuration issue. You need to disable:&lt;BR /&gt;&lt;BR /&gt;Device Drivers ---&amp;gt;&lt;BR /&gt;Misc drivers ---&amp;gt;&lt;BR /&gt;[*] Security &lt;BR /&gt;&lt;BR /&gt;Device Drivers ---&amp;gt;&lt;BR /&gt;Memory Technology Drivers ---&amp;gt;&lt;BR /&gt;[*} MTD support&lt;BR /&gt;&lt;BR /&gt;After that it will work!&lt;BR /&gt;Regards,&lt;BR /&gt;Gian&lt;P&gt;Message Edited by Gian on &lt;SPAN class="date_text"&gt;2006-07-12&lt;/SPAN&gt; &lt;SPAN class="time_text"&gt;01:53 AM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2006 13:52:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142088#M2513</guid>
      <dc:creator>Gian</dc:creator>
      <dc:date>2006-07-12T13:52:55Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142089#M2514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks a lot Gian for your help&lt;BR /&gt;&lt;BR /&gt;I try it tonight!&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Olivier&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Jul 2006 14:33:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142089#M2514</guid>
      <dc:creator>OL</dc:creator>
      <dc:date>2006-07-12T14:33:45Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142090#M2515</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Really thanks, now it work until kernel panic because it can't connect NFS server as you notice!&lt;BR /&gt;&lt;BR /&gt;I'm going to try solve this, perhaps have the solution?!!!&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;Olivier&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2006 03:09:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142090#M2515</guid>
      <dc:creator>OL</dc:creator>
      <dc:date>2006-07-13T03:09:38Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142091#M2516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Unfortunately yesterday i tried to put colilo in boot-flash (and so erasing DBUG) to avoid the kernel image's download and the net-parameters settings every time. The colilo image work from RAM, but NOT from FLASH!!!!!&lt;BR /&gt;So now i must restore the DBUG monitor through BDM interface...&lt;BR /&gt;At now i didn't resolve the nfs problem yet, so the first do it, could help the other, ok?&lt;BR /&gt;Bye,&lt;BR /&gt;Gianluca&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jul 2006 14:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142091#M2516</guid>
      <dc:creator>Gian</dc:creator>
      <dc:date>2006-07-13T14:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142092#M2517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello&lt;BR /&gt;&lt;BR /&gt;There is a specific colilo for flash, and it is wrote it is possible to have dbug and colilo on the flash.&lt;BR /&gt;&lt;BR /&gt;For NFS, of course if I find something I put some information here, probably this is a mistake on NFS server config.&lt;BR /&gt;&lt;BR /&gt;Olivier&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2006 03:53:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142092#M2517</guid>
      <dc:creator>OL</dc:creator>
      <dc:date>2006-07-14T03:53:01Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142093#M2518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello&lt;BR /&gt;&lt;BR /&gt;Some news, NFS not work but messages change!&lt;BR /&gt;&lt;BR /&gt;Perhap do you not have "portmap" service running?&lt;BR /&gt;&lt;BR /&gt;I have notice a strange problem configuration I have put something like this for IP address that can access to my NFS server: 192.168.1.*&lt;BR /&gt;and it looks not work I have replace it by: 192.168.1.0/255.255.255.0&lt;BR /&gt;This was need for me for test NFS server from my computer&lt;BR /&gt;&lt;BR /&gt;as root I have done this sort of test:&lt;BR /&gt;mount 192.168.1.39:/tftpboot/ltib /mnt/ltib&lt;BR /&gt;&lt;BR /&gt;You should be able to mount it, for me it work&lt;BR /&gt;&lt;BR /&gt;Now I have probably to look in NFS right, I not understand how the coldfire card is identify.&lt;BR /&gt;&lt;BR /&gt;Olivier&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 15 Jul 2006 14:10:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142093#M2518</guid>
      <dc:creator>OL</dc:creator>
      <dc:date>2006-07-15T14:10:06Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts 2 (a bit more)</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142094#M2519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks guys,&lt;BR /&gt;&lt;BR /&gt;This was just the info I needed. &lt;BR /&gt;I've started working on coldfire-linux almost 2 months now, and&lt;BR /&gt;this trick helped a great deal. &lt;BR /&gt;&lt;BR /&gt;I don't have the final answer to the "kernel panic", but I got it running with a workaround: I exported the original directory in which the root-file system is generated by LTIB (/my-ltib-root-dir/rootfs) directly, in stead of using the link in /tftpboot.&lt;BR /&gt;&lt;BR /&gt;I'm new to linux but for your information, this is how it worked:&lt;BR /&gt;I used the /etc/exports - file and added:&lt;BR /&gt;/path-to-my-ltib-root-dir/rootfs 192.168.1.202(rw,async,no_root_squash) &lt;BR /&gt;&lt;BR /&gt;in which "192.168.1.202" is the IP-address of my target board&lt;BR /&gt;&lt;BR /&gt;Remarks:&lt;BR /&gt;* In the setup for the command-line (colilo&amp;gt;set cl mac0= ... etc etc) refer directly to: &lt;BR /&gt;nfsroot=my-host-IP-address:/path-to-my-ltib-root-dir/rootfs&lt;BR /&gt;&lt;BR /&gt;* When I do the start-up sequence I have to switch serial communication to 115200 baud-rate, after the linux kernel has started.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jul 2006 16:45:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142094#M2519</guid>
      <dc:creator>dyon</dc:creator>
      <dc:date>2006-07-17T16:45:59Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142095#M2520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi OL!&lt;BR /&gt;Some news: now my nfs seems work a little bit...&lt;BR /&gt;I have updated my nfs-utils, changed the /tftpboot permissions in 775 and now during the kernel execution, it said&lt;BR /&gt;&lt;BR /&gt;[...]&lt;BR /&gt;IP-Config: Complete:&lt;BR /&gt; device=eth0, addr=192.168.1.40, mask=255.255.255.0, gw=192.168.1.1,&lt;BR /&gt; host=ColdFire, domain=, nis-domain=(none),&lt;BR /&gt; bootserver=192.168.1.39, rootserver=192.168.1.39, rootpath=&lt;BR /&gt;Looking up port of RPC 100003/2 on 192.168.1.39&lt;BR /&gt;Looking up port of RPC 100005/1 on 192.168.1.39&lt;BR /&gt;VFS: Mounted root (nfs filesystem).&lt;BR /&gt;Setting the hostname to freescale&lt;BR /&gt;Mounting filesystems&lt;BR /&gt;mount: Mounting usbfs on /proc/bus/usb failed: No such file or directory&lt;BR /&gt;Starting syslogd and klogd&lt;BR /&gt;Setting up networking on loopback device:&lt;BR /&gt;Setting up networking on eth0:&lt;BR /&gt;Adding static route for default gateway to 192.168.0.1:&lt;BR /&gt;RPC: sendmsg returned error 101&lt;BR /&gt;nfs: RPC call returned error 101&lt;BR /&gt;RPC: sendmsg returned error 101&lt;BR /&gt; &lt;BR /&gt;and here stops.&lt;BR /&gt;&lt;BR /&gt;So i don't know if there is an nfs problem still, but i didn't understand why it has tried to setup eth0 an other time. Perhaps, the gw is wrong... and maybe this could be the origin of the 101 error problem...&lt;BR /&gt;If you have any suggestion...&lt;BR /&gt;Regards, &lt;BR /&gt;Gianluca Salvador&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jul 2006 17:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142095#M2520</guid>
      <dc:creator>Gian</dc:creator>
      <dc:date>2006-07-18T17:08:44Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142096#M2521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi to all!&lt;BR /&gt;I have linux prompt on ColdFire!!!!!!!&lt;BR /&gt;I solved the nfs problem and also the last problem. That was a eth0 setup issue: In fact i rebuild the linux kernel image checking the dhcp flag for the ethernet configuration. Now i have -sh-2.05b# and theworld is beautifull :smileywink: almost untill the next problem ;-P&lt;BR /&gt;Regards,&lt;BR /&gt;Gian&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2006 20:13:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142096#M2521</guid>
      <dc:creator>Gian</dc:creator>
      <dc:date>2006-07-19T20:13:05Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting halts</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142097#M2522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Yes happy to you&lt;BR /&gt;&lt;BR /&gt;I haven't still totaly solve my problems, but I have a problem issue in my Linux Box I have probably to reinstall it!&lt;BR /&gt;&lt;BR /&gt;Good work&lt;BR /&gt;&lt;BR /&gt;Olivier&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2006 20:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Linux-booting-halts/m-p/142097#M2522</guid>
      <dc:creator>OL</dc:creator>
      <dc:date>2006-07-19T20:38:15Z</dc:date>
    </item>
  </channel>
</rss>