<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MAC address matching with M5223X in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140625#M2338</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I spoke this the experts this morning and it was explained to me that the pause frames are just special forms of the mulitcast.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The ColdFire_lite stack does not use the Group Hash table so any address with the odd first oclet is ignored. This configuration is in the ifec.c driver.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Jun 2006 00:42:18 GMT</pubDate>
    <dc:creator>DrSeuss</dc:creator>
    <dc:date>2006-06-28T00:42:18Z</dc:date>
    <item>
      <title>MAC address matching with M5223X</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140621#M2334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;SPAN&gt;Hi All&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I was playing around with the M52235EVB today.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I set several MAC addresses and checked that ARP, ping &amp;nbsp;and an embedded web server were working correctly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;These are the addresses which I used:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;00-00-00-00-00-00&lt;BR /&gt;00-00-00-00-00-11&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;00-00-00-00-11-22&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;00-00-11-22-33-44&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;00-11-22-33-44-55&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;11-22-33-44-55-66&lt;BR /&gt;&lt;/SPAN&gt; &lt;SPAN&gt;66-55-44-33-22-11&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In each case ARP works fine. The device responds to the broadcast with its MAC address (as shown in the list) and the PC then displays the IP/MAC combination in its ARP table (I delete the ARP table in the PC with arp -d between tests)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In each case pings and the web browser operate correctly with the exception of the MAC address 11-22-33-44-55-66. No frames are received with the MAC destination, only broadcasts.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can any one reproduce this or explain why the one address (or some sort of combinations) would not work?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Many thanks for ideas.&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Mark Butcher&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.mjbc.ch%2F" rel="nofollow" target="_blank"&gt;www.mjbc.ch&lt;/A&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;P&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jun 2006 06:37:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140621#M2334</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2006-06-22T06:37:26Z</dc:date>
    </item>
    <item>
      <title>Re: MAC address matching with M5223X</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140622#M2335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;This is a multicast address, and the syptoms are consistent with this.&lt;BR /&gt;The address really should not be used. To be safe, always make the first octet a zero (never odd!)&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2006 06:28:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140622#M2335</guid>
      <dc:creator>DrSeuss</dc:creator>
      <dc:date>2006-06-26T06:28:55Z</dc:date>
    </item>
    <item>
      <title>Re: MAC address matching with M5223X</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140623#M2336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Doc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But has this to do with the operation of the MAC compare unit, even when all unicast and multcast features are disabled in the EMAC? I was expecting it to simply do a compare of the 48 bit MAC and either match it with the value programmed or reject it. This must mean that it is more than just a 48 bit comparator working there...(?).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;BR /&gt;&lt;A href="http://www.mjbc.ch/"&gt;www.mjbc.ch&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2006 07:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140623#M2336</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2006-06-26T07:10:07Z</dc:date>
    </item>
    <item>
      <title>Re: MAC address matching with M5223X</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140624#M2337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;I misspoke in that I was thinking of pause frames&amp;nbsp; &lt;FONT face="TimesNewRoman"&gt;(01:80:C2:00:00:01).&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;Perhaps, this is an error that has been worked around for a long time. It is possible that the FEC trashes ANY frame with an odd first oclet.&lt;/P&gt;&lt;P&gt;I am referring to sec 18.4.8 in the specification. Per flow chart it appears that ANY odd first oclet is assumed to be a pause frame. There is more going one than a simple compare.&lt;/P&gt;&lt;P&gt;Can you run your test again to determine if all odd first oclets are trashed?&lt;/P&gt;&lt;P&gt;What about the pause frame above?&lt;B&gt;&lt;FONT face="Helvetica-Bold" size="4"&gt;&lt;/FONT&gt;&lt;/B&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2006 07:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140624#M2337</guid>
      <dc:creator>DrSeuss</dc:creator>
      <dc:date>2006-06-27T07:31:22Z</dc:date>
    </item>
    <item>
      <title>Re: MAC address matching with M5223X</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140625#M2338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I spoke this the experts this morning and it was explained to me that the pause frames are just special forms of the mulitcast.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The ColdFire_lite stack does not use the Group Hash table so any address with the odd first oclet is ignored. This configuration is in the ifec.c driver.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2006 00:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/MAC-address-matching-with-M5223X/m-p/140625#M2338</guid>
      <dc:creator>DrSeuss</dc:creator>
      <dc:date>2006-06-28T00:42:18Z</dc:date>
    </item>
  </channel>
</rss>