<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: Problem to build a new uclinux image for M5208EVB</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-to-build-a-new-uclinux-image-for-M5208EVB/m-p/125153#M227</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Alban,&lt;BR /&gt;No, I think there was a misunderstood here. I have two types of problems, the first one is that I wrote in this thread, it occurs when I try to create a new image, setting in the configuration for example: nfsmount and jffs2. When I try this the image is not even created.&lt;BR /&gt;In the other thread I have another problem. There I can build a new image (I take all configuration from a default image and just add one more feature into it, for example: jffs), I use de ‘make’ command and the image is created successfully. In that case the error occurs when I download my new image to my M5208evb and reset the kit, just in that moment I have the problem.&lt;BR /&gt;As you can notice I’m not a native English speaker, so maybe I didn’t make myself clear. Hope I was clear this time.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Mar 2007 01:56:55 GMT</pubDate>
    <dc:creator>Roger</dc:creator>
    <dc:date>2007-03-07T01:56:55Z</dc:date>
    <item>
      <title>Problem to build a new uclinux image for M5208EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-to-build-a-new-uclinux-image-for-M5208EVB/m-p/125151#M225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I am having some problems to build a new uclinux image using 'make menuconfig'. I have linux Ubuntu 6.06 in my host, and my target is a M5208EVB, and I'm using 'uClinux-dist-20060803.tar' and 'm68k-uclinux-tools-20060615.sh' that I download from the uclunix.org.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem doesn't happen all the times, but in some cases when I try to add a new feature to the image like: nfsmount or jffs2 for example, I have this problem. When I do the 'make' commannd (try to compile the image) it occurs a erro end the compile process stops. This is the error message:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;"ucfront-gcc m68k-elf-gcc -m5307 -DCONFIG_COLDFIRE -Os -g -fomit-frame-pointer -pipe -fno-common -fno-builtin -Wall -DEMBED -msep-data -Dlinux -D__linux__ -Dunix -D__uClinux__ -DHAVE_NFS -c -o nfsmount.o nfsmount.c&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;nfsmount.c:35:23: error: gnu/types.h: Arquivo ou diretÃ³rio inexistente&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In file included from nfsmount.c:46:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;sundries.h:54: warning: type qualifiers ignored on function return type&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In file included from /uClinux-dist/uClibc/include/linux/nfs_mount.h:11,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;from nfs_mount3.h:15,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;from nfsmount.c:51:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:26: error: redeclaration of enumerator "IPPROTO_IP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:32: error: previous definition of "IPPROTO_IP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:27: error: redeclaration of enumerator "IPPROTO_ICMP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:36: error: previous definition of "IPPROTO_ICMP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:28: error: redeclaration of enumerator "IPPROTO_IGMP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:38: error: previous definition of "IPPROTO_IGMP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:29: error: redeclaration of enumerator "IPPROTO_IPIP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:40: error: previous definition of "IPPROTO_IPIP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:30: error: redeclaration of enumerator "IPPROTO_TCP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:42: error: previous definition of "IPPROTO_TCP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:31: error: redeclaration of enumerator "IPPROTO_EGP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:44: error: previous definition of "IPPROTO_EGP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:32: error: redeclaration of enumerator "IPPROTO_PUP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:46: error: previous definition of "IPPROTO_PUP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:33: error: redeclaration of enumerator "IPPROTO_UDP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:48: error: previous definition of "IPPROTO_UDP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:34: error: redeclaration of enumerator "IPPROTO_IDP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:50: error: previous definition of "IPPROTO_IDP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:36: error: redeclaration of enumerator "IPPROTO_RSVP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:60: error: previous definition of "IPPROTO_RSVP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:37: error: redeclaration of enumerator "IPPROTO_GRE"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:62: error: previous definition of "IPPROTO_GRE" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:39: error: redeclaration of enumerator "IPPROTO_IPV6"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:54: error: previous definition of "IPPROTO_IPV6" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:41: error: redeclaration of enumerator "IPPROTO_ESP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:64: error: previous definition of "IPPROTO_ESP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:42: error: redeclaration of enumerator "IPPROTO_AH"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:66: error: previous definition of "IPPROTO_AH" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:43: error: redeclaration of enumerator "IPPROTO_PIM"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:78: error: previous definition of "IPPROTO_PIM" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:45: error: redeclaration of enumerator "IPPROTO_COMP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:80: error: previous definition of "IPPROTO_COMP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:46: error: redeclaration of enumerator "IPPROTO_SCTP"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:82: error: previous definition of "IPPROTO_SCTP" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:48: error: redeclaration of enumerator "IPPROTO_RAW"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:84: error: previous definition of "IPPROTO_RAW" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:50: error: redeclaration of enumerator "IPPROTO_MAX"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/netinet/in.h:87: error: previous definition of "IPPROTO_MAX" was here&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:54: error: redefinition of "struct in_addr"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:113: error: redefinition of "struct ip_mreq"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:119: error: redefinition of "struct ip_mreqn"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:170: error: redefinition of "struct in_pktinfo"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/uClinux-dist/uClibc/include/linux/in.h:178: error: redefinition of "struct sockaddr_in"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;nfsmount.c: In function 'nfsmount'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;nfsmount.c:237: error: 'NFS_VERSION' undeclared (first use in this function)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;nfsmount.c:237: error: (Each undeclared identifier is reported only once&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;nfsmount.c:237: error: for each function it appears in.)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;nfsmount.c:445: warning: implicit declaration of function "time"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;nfsmount.c:118: warning: unused variable "hp"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make[3]: ** [nfsmount.o] Erro 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make[3]: Saindo do diretório `/uClinux-dist/user/mount'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make[2]: ** [mount] Erro 2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make[2]: Saindo do diretório `/uClinux-dist/user'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make[1]: ** [all] Erro 2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make[1]: Saindo do diretório `/uClinux-dist/user'&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;make: ** [subdirs] Erro 1"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anyone know what is happing? Why does this error?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;hope someone can help me.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2007 05:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-to-build-a-new-uclinux-image-for-M5208EVB/m-p/125151#M225</guid>
      <dc:creator>Roger</dc:creator>
      <dc:date>2007-03-06T05:50:29Z</dc:date>
    </item>
    <item>
      <title>Re: Problem to build a new uclinux image for M5208EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-to-build-a-new-uclinux-image-for-M5208EVB/m-p/125152#M226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hello,&lt;/DIV&gt;&lt;DIV&gt;You created&amp;nbsp;a new thread saying you created the image successfully.&lt;/DIV&gt;&lt;DIV&gt;Therefore should we understand that this thread is closed and doesn't need assistance ?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Regards,&lt;/DIV&gt;&lt;DIV&gt;Alban.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2007 06:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-to-build-a-new-uclinux-image-for-M5208EVB/m-p/125152#M226</guid>
      <dc:creator>Alban</dc:creator>
      <dc:date>2007-03-06T06:08:07Z</dc:date>
    </item>
    <item>
      <title>Re: Problem to build a new uclinux image for M5208EVB</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-to-build-a-new-uclinux-image-for-M5208EVB/m-p/125153#M227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Alban,&lt;BR /&gt;No, I think there was a misunderstood here. I have two types of problems, the first one is that I wrote in this thread, it occurs when I try to create a new image, setting in the configuration for example: nfsmount and jffs2. When I try this the image is not even created.&lt;BR /&gt;In the other thread I have another problem. There I can build a new image (I take all configuration from a default image and just add one more feature into it, for example: jffs), I use de ‘make’ command and the image is created successfully. In that case the error occurs when I download my new image to my M5208evb and reset the kit, just in that moment I have the problem.&lt;BR /&gt;As you can notice I’m not a native English speaker, so maybe I didn’t make myself clear. Hope I was clear this time.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Mar 2007 01:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Problem-to-build-a-new-uclinux-image-for-M5208EVB/m-p/125153#M227</guid>
      <dc:creator>Roger</dc:creator>
      <dc:date>2007-03-07T01:56:55Z</dc:date>
    </item>
  </channel>
</rss>