<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re-compile gives different size in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Re-compile-gives-different-size/m-p/125121#M223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I've the following "simple" problem: compiling the MSL_RuntimeCF.mcp project gives *.a files of different sizes (and contents) when compiled on two different machines. Obviously both PC have CodeWarrior 5.2.1174 and I've not changed anything in the project settings. Anybody has an idea why the libraries are different?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Ronald&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Jul 2006 22:47:58 GMT</pubDate>
    <dc:creator>tfd</dc:creator>
    <dc:date>2006-07-27T22:47:58Z</dc:date>
    <item>
      <title>Re-compile gives different size</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Re-compile-gives-different-size/m-p/125121#M223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I've the following "simple" problem: compiling the MSL_RuntimeCF.mcp project gives *.a files of different sizes (and contents) when compiled on two different machines. Obviously both PC have CodeWarrior 5.2.1174 and I've not changed anything in the project settings. Anybody has an idea why the libraries are different?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Ronald&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2006 22:47:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Re-compile-gives-different-size/m-p/125121#M223</guid>
      <dc:creator>tfd</dc:creator>
      <dc:date>2006-07-27T22:47:58Z</dc:date>
    </item>
    <item>
      <title>Re: Re-compile gives different size</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Re-compile-gives-different-size/m-p/125122#M224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Do you look at the file size?&lt;BR /&gt;The elf files contain dates and most probably the cause for your differences, absolute paths (and maybe other things), so just checking the file size does not show much.&lt;BR /&gt;I would actually take the two *.a files, add them to a CW project, disassemble (context menu in the project) them and then compare the listing files.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Aug 2006 01:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Re-compile-gives-different-size/m-p/125122#M224</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2006-08-03T01:43:34Z</dc:date>
    </item>
  </channel>
</rss>