<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: linux startup problem on 548x (custom board)</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/linux-startup-problem-on-548x-custom-board/m-p/139497#M2176</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Sridhar,&lt;BR /&gt;&lt;BR /&gt;I'm not an expert on porting linux. But one common mistake is in the SDRAM init when moving from a Freescale board to a custom board. Sometimes it seems like the SDRAM is working, but when you enable cache and MMU you'll sometimes see problems arise. Try doing some DMA memory tests with a simple bootloader program or a codewarrior application to make sure your SDRAM init is robust.&lt;BR /&gt;&lt;BR /&gt;-JWW&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 24 Dec 2006 15:05:54 GMT</pubDate>
    <dc:creator>JWW</dc:creator>
    <dc:date>2006-12-24T15:05:54Z</dc:date>
    <item>
      <title>linux startup problem on 548x (custom board)</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/linux-startup-problem-on-548x-custom-board/m-p/139496#M2175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I&amp;nbsp;have got linux-2.6.10 up &amp;amp; running on fire engine eval board (MCF5485) using the LTIB and BSP package provided by freescale . However when I run the same on a custom board , I get a trap at the point where it jumps to _running_high code after initializing the MMU in head.S . Any suggestions on where the problem could be ?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;The only difference between the two setups is that in the latter , I use a BDM to single step and see where the problem is. I use colilo as the bootloader and I am able to the UART0 prints from colilo on my custom board, so I assume there is no problem there. The only change that I had to do in colilo is to change the RAM initilialization and change the clock frequency from 100mhz to 80mhz.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Also is there some tips/documentation available for changes needed to get linux up on a custom board running MCF54xx?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks in advance,&lt;/DIV&gt;&lt;DIV&gt;Sridhar&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2006 00:20:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/linux-startup-problem-on-548x-custom-board/m-p/139496#M2175</guid>
      <dc:creator>SridharS</dc:creator>
      <dc:date>2006-12-11T00:20:30Z</dc:date>
    </item>
    <item>
      <title>Re: linux startup problem on 548x (custom board)</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/linux-startup-problem-on-548x-custom-board/m-p/139497#M2176</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Sridhar,&lt;BR /&gt;&lt;BR /&gt;I'm not an expert on porting linux. But one common mistake is in the SDRAM init when moving from a Freescale board to a custom board. Sometimes it seems like the SDRAM is working, but when you enable cache and MMU you'll sometimes see problems arise. Try doing some DMA memory tests with a simple bootloader program or a codewarrior application to make sure your SDRAM init is robust.&lt;BR /&gt;&lt;BR /&gt;-JWW&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Dec 2006 15:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/linux-startup-problem-on-548x-custom-board/m-p/139497#M2176</guid>
      <dc:creator>JWW</dc:creator>
      <dc:date>2006-12-24T15:05:54Z</dc:date>
    </item>
  </channel>
</rss>