<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and Processors中的主题 Re: About MPC8248 USB hardware interrupt</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MPC8248-USB-hardware-interrupt/m-p/139032#M2124</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Andrew&lt;BR /&gt;&lt;BR /&gt;I think you may have posted your question in the wrong place.&lt;BR /&gt;&lt;BR /&gt;This is a discussion forum about the ColdFire microprocessor range. Your question relates to a PowerPC processor, so you may not find anyone here that can help you.&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Dec 2006 18:27:51 GMT</pubDate>
    <dc:creator>SimonMarsden_de</dc:creator>
    <dc:date>2006-12-05T18:27:51Z</dc:date>
    <item>
      <title>About MPC8248 USB hardware interrupt</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MPC8248-USB-hardware-interrupt/m-p/139031#M2123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;We use the MPC8248 usb controller as a usb host. But I don't know what are the pre-conditions for the usb hardware interrupt to occur.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Firstly,I clear the SIPNR_L[USB] and set the the SIMR_L[USB].And I set he MSR[EE].&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Secondly,I set some needed bits(for example,IDLE,RESET,SOF,TXB,TXE1)in USBMR.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Althrough at this time, I haven't registered the ISR with the interruper vector(0b00_1011).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;When the borad brings up,and the above conditions are also meet, I think that,if a usb flash disk is inserted to the board, the system should set the SIPNR_L[USB] automatically. Am I true?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If I'm wrong,the software should do something else to let the system set the SIPNR_L[USB].Could you tell me ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Dec 2006 18:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MPC8248-USB-hardware-interrupt/m-p/139031#M2123</guid>
      <dc:creator>AndrewChou</dc:creator>
      <dc:date>2006-12-05T18:09:05Z</dc:date>
    </item>
    <item>
      <title>Re: About MPC8248 USB hardware interrupt</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MPC8248-USB-hardware-interrupt/m-p/139032#M2124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi Andrew&lt;BR /&gt;&lt;BR /&gt;I think you may have posted your question in the wrong place.&lt;BR /&gt;&lt;BR /&gt;This is a discussion forum about the ColdFire microprocessor range. Your question relates to a PowerPC processor, so you may not find anyone here that can help you.&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Dec 2006 18:27:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/About-MPC8248-USB-hardware-interrupt/m-p/139032#M2124</guid>
      <dc:creator>SimonMarsden_de</dc:creator>
      <dc:date>2006-12-05T18:27:51Z</dc:date>
    </item>
  </channel>
</rss>