<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic A question about using non-multiplexed mode for the Flexbus in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/A-question-about-using-non-multiplexed-mode-for-the-Flexbus/m-p/137525#M1968</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I have a question about any limitations there might be in using non-multiplexed mode versus multiplexed mode for the Coldfire Flexbus.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;We are in the design phase of a new circuit board that uses an MCF5485 CPU. We won't be using the PCI bus so would like to use non-multiplexed mode to eliminate the need for an address latch. The issue is, there are sections of the MCF5485 reference manual (Rev. 4) that seem to suggest that non-multiplexed mode is more limited in terms of the number of address and data lines that can be used at any one time. For instance,&amp;nbsp;in the section on Bus Cycle Multiplexing in chapter 17, all of the figures that illustrate basic&amp;nbsp;read and write cycles always show a net total of 32 address and data lines when non-multiplexed mode is used, ie, 16 Address with 16 data lines, or 24 address and 8 data lines. There is also a line in the description of Figure 17-16&amp;nbsp;that says "&lt;SPAN style="font-family: TimesNewRoman;"&gt;Notice that when the device port size is 32 bits, the only mode the bus supports is multiplexing address and data lines."&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Am I misunderstanding something, or is the Flexbus really more limited in non-multplexed mode?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks!&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by JeffC on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2007-06-20&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;06:16 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Jun 2007 00:15:20 GMT</pubDate>
    <dc:creator>JeffC</dc:creator>
    <dc:date>2007-06-21T00:15:20Z</dc:date>
    <item>
      <title>A question about using non-multiplexed mode for the Flexbus</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/A-question-about-using-non-multiplexed-mode-for-the-Flexbus/m-p/137525#M1968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;I have a question about any limitations there might be in using non-multiplexed mode versus multiplexed mode for the Coldfire Flexbus.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;We are in the design phase of a new circuit board that uses an MCF5485 CPU. We won't be using the PCI bus so would like to use non-multiplexed mode to eliminate the need for an address latch. The issue is, there are sections of the MCF5485 reference manual (Rev. 4) that seem to suggest that non-multiplexed mode is more limited in terms of the number of address and data lines that can be used at any one time. For instance,&amp;nbsp;in the section on Bus Cycle Multiplexing in chapter 17, all of the figures that illustrate basic&amp;nbsp;read and write cycles always show a net total of 32 address and data lines when non-multiplexed mode is used, ie, 16 Address with 16 data lines, or 24 address and 8 data lines. There is also a line in the description of Figure 17-16&amp;nbsp;that says "&lt;SPAN style="font-family: TimesNewRoman;"&gt;Notice that when the device port size is 32 bits, the only mode the bus supports is multiplexing address and data lines."&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Am I misunderstanding something, or is the Flexbus really more limited in non-multplexed mode?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks!&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Message Edited by JeffC on &lt;/SPAN&gt;&lt;SPAN class="date_text"&gt;2007-06-20&lt;/SPAN&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;06:16 PM&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jun 2007 00:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/A-question-about-using-non-multiplexed-mode-for-the-Flexbus/m-p/137525#M1968</guid>
      <dc:creator>JeffC</dc:creator>
      <dc:date>2007-06-21T00:15:20Z</dc:date>
    </item>
    <item>
      <title>Re: A question about using non-multiplexed mode for the Flexbus</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/A-question-about-using-non-multiplexed-mode-for-the-Flexbus/m-p/137526#M1969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;MCF548X Flexbus supports operation with the following:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;1.Non-multiplexed 32-bit address and 32-bit data (32-bit address muxed over&lt;BR /&gt;&amp;nbsp;&amp;nbsp; PCI bus–PCI not usable)&lt;BR /&gt;&amp;nbsp;2.Multiplexed 32-bit address and 32-bit data (PCI usable)&lt;BR /&gt;&amp;nbsp;3.Multiplexed 32-bit address and 16-bit data&lt;BR /&gt;&amp;nbsp;4.Multiplexed 32-bit address and 8-bit data&lt;/DIV&gt;&lt;DIV&gt;as it is described in section 1.4 of the MCF548X Reference Manual.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;During reset, the FlexBus can be configured to operate in a non-multiplexed 32-bit address with 32-bit data mode. In this mode, the 32-bit FlexBus AD[31:0] is used for the data bus, and the PCI bus PCIAD[31:0] is used as the address bus.&lt;BR /&gt;Section 2.2.6 Reset Configuration Pins of the Reference Manual describes that.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If the FlexBus is configured to operate in a multiplexed mode during reset, then the full 32-bit address will always be driven on the first clock of a bus cycle on AD lines.&lt;BR /&gt;Some AD lines will be used later during the data phase for data.&lt;BR /&gt;Which AD lines is determined by the port size programmed in corresponding chip select configuration register CSCRn.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jun 2007 18:56:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/A-question-about-using-non-multiplexed-mode-for-the-Flexbus/m-p/137526#M1969</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2007-06-22T18:56:11Z</dc:date>
    </item>
    <item>
      <title>Re: A question about using non-multiplexed mode for the Flexbus</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/A-question-about-using-non-multiplexed-mode-for-the-Flexbus/m-p/137527#M1970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using MCF5485.i want to activate DE1 so,i should activate PCIAD2 as 1 and BG4 as 1.I make BG4 as 1.But dunno how to activate AD2.Will anyone please help me how to activate only that AD2(G26) to activate my external device????&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by Manju on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-03-13&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;12:19 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2009 13:49:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/A-question-about-using-non-multiplexed-mode-for-the-Flexbus/m-p/137527#M1970</guid>
      <dc:creator>Manju</dc:creator>
      <dc:date>2009-03-13T13:49:07Z</dc:date>
    </item>
  </channel>
</rss>