<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Help QADC from coldfire 5282 in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Help-QADC-from-coldfire-5282/m-p/137198#M1908</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;Lucho wrote:&lt;BR /&gt;I'm tring to use the module QADC from the coldfire 5282. I have problems with the registers of this QADC, I configure it for AN0 and I send the answer to the port TC and I don't have eny answer. If someone have an exemple of this please send it to me.&lt;BR /&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;Hi:&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Maybe you are using interrupts and using a stationary code from Codewarrior.&lt;BR /&gt;&lt;BR /&gt;By default, vector table is not included in RAM target, only in ROM targets, so if you are using debug green arrow, is not enough.&lt;BR /&gt;&lt;BR /&gt;In order to allow interrupts you have to burn FLASH memory to include the vector table (vector.s). After that you can debug the code, but, as I said, only in ROM targets.&lt;BR /&gt;&lt;BR /&gt;Only guessing your problem &lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;BR /&gt;&lt;BR /&gt;Good luck!&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Dec 2006 05:28:40 GMT</pubDate>
    <dc:creator>PaoloRenzo</dc:creator>
    <dc:date>2006-12-20T05:28:40Z</dc:date>
    <item>
      <title>Help QADC from coldfire 5282</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Help-QADC-from-coldfire-5282/m-p/137197#M1907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I'm tring to use the module QADC from the coldfire 5282. I have problems with the registers of this QADC, I configure it for AN0 and I send the answer to the port TC and I don't have eny answer. If someone have an exemple of this please send it to me.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Nov 2006 10:19:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Help-QADC-from-coldfire-5282/m-p/137197#M1907</guid>
      <dc:creator>Lucho</dc:creator>
      <dc:date>2006-11-20T10:19:34Z</dc:date>
    </item>
    <item>
      <title>Re: Help QADC from coldfire 5282</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Help-QADC-from-coldfire-5282/m-p/137198#M1908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;Lucho wrote:&lt;BR /&gt;I'm tring to use the module QADC from the coldfire 5282. I have problems with the registers of this QADC, I configure it for AN0 and I send the answer to the port TC and I don't have eny answer. If someone have an exemple of this please send it to me.&lt;BR /&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;BR /&gt;Hi:&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Maybe you are using interrupts and using a stationary code from Codewarrior.&lt;BR /&gt;&lt;BR /&gt;By default, vector table is not included in RAM target, only in ROM targets, so if you are using debug green arrow, is not enough.&lt;BR /&gt;&lt;BR /&gt;In order to allow interrupts you have to burn FLASH memory to include the vector table (vector.s). After that you can debug the code, but, as I said, only in ROM targets.&lt;BR /&gt;&lt;BR /&gt;Only guessing your problem &lt;IMG alt=":smileywink:" class="emoticon emoticon-smileywink" id="smileywink" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-wink.gif" title="Smiley Wink" /&gt;&lt;BR /&gt;&lt;BR /&gt;Good luck!&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Dec 2006 05:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/Help-QADC-from-coldfire-5282/m-p/137198#M1908</guid>
      <dc:creator>PaoloRenzo</dc:creator>
      <dc:date>2006-12-20T05:28:40Z</dc:date>
    </item>
  </channel>
</rss>