<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 5V tolerant I/O on MCF5223x ? in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5V-tolerant-I-O-on-MCF5223x/m-p/135121#M1558</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;While not strictly 5v tolerant - 5V signals can be connected as long as there is a series resistor to limit the current flow into the pin. The pin will clamp the input to 3.6V, as long as the resistor limits the input current (&amp;lt;2mA) 5V signals can connect to the 3.3v pins.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Nov 2006 23:49:55 GMT</pubDate>
    <dc:creator>DrSeuss</dc:creator>
    <dc:date>2006-11-09T23:49:55Z</dc:date>
    <item>
      <title>5V tolerant I/O on MCF5223x ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5V-tolerant-I-O-on-MCF5223x/m-p/135119#M1556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;&lt;STRONG&gt;Is the general purpose i/o on mcf5223x microcontrollers 5V tolerant?&lt;/STRONG&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Also, where can I find this and other electrical specs for this processor family?&amp;nbsp; I have looked in the Reference Manual and many other available documents but can't find electrical specs anywhere.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2006 06:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5V-tolerant-I-O-on-MCF5223x/m-p/135119#M1556</guid>
      <dc:creator>lambtron</dc:creator>
      <dc:date>2006-11-02T06:21:43Z</dc:date>
    </item>
    <item>
      <title>Re: 5V tolerant I/O on MCF5223x ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5V-tolerant-I-O-on-MCF5223x/m-p/135120#M1557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Unfortunately, MCF5223x are not 5V I/O tolerant see:&lt;BR /&gt;&lt;A href="http://www.freescale.com/files/32bit/doc/data_sheet/MCF52235DS.pdf" target="test_blank"&gt;http://www.freescale.com/files/32bit/doc/data_sheet/MCF52235DS.pdf&lt;/A&gt;&lt;BR /&gt;chapter 2.3 table 22&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Emmanuel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2006 16:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5V-tolerant-I-O-on-MCF5223x/m-p/135120#M1557</guid>
      <dc:creator>Nouchi</dc:creator>
      <dc:date>2006-11-02T16:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: 5V tolerant I/O on MCF5223x ?</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5V-tolerant-I-O-on-MCF5223x/m-p/135121#M1558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;While not strictly 5v tolerant - 5V signals can be connected as long as there is a series resistor to limit the current flow into the pin. The pin will clamp the input to 3.6V, as long as the resistor limits the input current (&amp;lt;2mA) 5V signals can connect to the 3.3v pins.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Nov 2006 23:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/5V-tolerant-I-O-on-MCF5223x/m-p/135121#M1558</guid>
      <dc:creator>DrSeuss</dc:creator>
      <dc:date>2006-11-09T23:49:55Z</dc:date>
    </item>
  </channel>
</rss>