<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>ColdFire/68K Microcontrollers and ProcessorsのトピックRe: using an 8-bit LCD with the MCF52230</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/using-an-8-bit-LCD-with-the-MCF52230/m-p/134885#M1513</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi BadDad&lt;BR /&gt;&lt;BR /&gt;Take a look at the uTasker project.&lt;BR /&gt;It includes LCD support, including an LCD simulator.&lt;BR /&gt;See &lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;regards&lt;BR /&gt;&lt;BR /&gt;Mark Butcher&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 26 May 2007 15:50:57 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2007-05-26T15:50:57Z</dc:date>
    <item>
      <title>using an 8-bit LCD with the MCF52230</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/using-an-8-bit-LCD-with-the-MCF52230/m-p/134884#M1512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Has anyone succefully used&amp;nbsp;an 8-bit LCD with the MCF52230?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;If so, do you have any tips, tricks or code examples you would be willing to share?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Best Regards,&lt;/DIV&gt;&lt;DIV&gt;BadDad&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 May 2007 23:10:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/using-an-8-bit-LCD-with-the-MCF52230/m-p/134884#M1512</guid>
      <dc:creator>baddad</dc:creator>
      <dc:date>2007-05-25T23:10:57Z</dc:date>
    </item>
    <item>
      <title>Re: using an 8-bit LCD with the MCF52230</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/using-an-8-bit-LCD-with-the-MCF52230/m-p/134885#M1513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hi BadDad&lt;BR /&gt;&lt;BR /&gt;Take a look at the uTasker project.&lt;BR /&gt;It includes LCD support, including an LCD simulator.&lt;BR /&gt;See &lt;A href="http://www.uTasker.com" rel="nofollow" target="_blank"&gt;www.uTasker.com&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;regards&lt;BR /&gt;&lt;BR /&gt;Mark Butcher&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 May 2007 15:50:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/using-an-8-bit-LCD-with-the-MCF52230/m-p/134885#M1513</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2007-05-26T15:50:57Z</dc:date>
    </item>
    <item>
      <title>Re: using an 8-bit LCD with the MCF52230</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/using-an-8-bit-LCD-with-the-MCF52230/m-p/134886#M1514</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Note that there is an online demo of LCD control at&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://84.253.57.46:8081/0" rel="nofollow" target="_blank"&gt;LCD control&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;It can be seen by web cam at &lt;A href="http://84.253.57.46:8080/" rel="nofollow" target="_blank"&gt;WEB CAM&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;At the control link there is also a stand-alone LCD (and key board) simulator which can be downloaded (called VIPpanel). This is not M52230 specific but does enable control of a web-based LCD as well as practical testing of all LCD functionality - full documentation is included in the simulator.&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 May 2007 16:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/using-an-8-bit-LCD-with-the-MCF52230/m-p/134886#M1514</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2007-05-26T16:07:15Z</dc:date>
    </item>
  </channel>
</rss>