<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: M52235 and External Memory in ColdFire/68K Microcontrollers and Processors</title>
    <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235-and-External-Memory/m-p/134516#M1471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi BenjaminRoy,&lt;/P&gt;&lt;P&gt;The MCF5223x family of ColdFire microcontrollers does not support external memory for flash, sram and/or dram.&lt;/P&gt;&lt;P&gt;If memory is accessible via SPI or I2C then we have then ability to do so but we do have to start the boot process from internal flash first.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards, DavidS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 May 2006 09:39:20 GMT</pubDate>
    <dc:creator>DavidS</dc:creator>
    <dc:date>2006-05-04T09:39:20Z</dc:date>
    <item>
      <title>M52235 and External Memory</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235-and-External-Memory/m-p/134515#M1470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;Is the M52235 capable of accessing external memory? MMC and SD cards interface through SPI (as far as I know), and is there any way of using the M52235's QSPI to connect, and access one of those, or any external memory IC's?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks, Benjamin Roy&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2006 07:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235-and-External-Memory/m-p/134515#M1470</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2006-05-04T07:34:55Z</dc:date>
    </item>
    <item>
      <title>Re: M52235 and External Memory</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235-and-External-Memory/m-p/134516#M1471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi BenjaminRoy,&lt;/P&gt;&lt;P&gt;The MCF5223x family of ColdFire microcontrollers does not support external memory for flash, sram and/or dram.&lt;/P&gt;&lt;P&gt;If memory is accessible via SPI or I2C then we have then ability to do so but we do have to start the boot process from internal flash first.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards, DavidS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2006 09:39:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235-and-External-Memory/m-p/134516#M1471</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2006-05-04T09:39:20Z</dc:date>
    </item>
    <item>
      <title>Re: M52235 and External Memory</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235-and-External-Memory/m-p/134517#M1472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Say I wanted to host a large page on the M52235. It would be well over the size of the coldfire's memory. Could the M52235 boot off it's internal flash/sram and then load the page off the SD Card?&lt;BR /&gt;&lt;BR /&gt;Is there any schematics or special hardware needed for the QSPI interface to the memory card? The memory cards' pinouts that I think are SPI are here:&lt;BR /&gt;&lt;BR /&gt;&lt;A href="http://pinouts.ru/data/memorysrick_pinout.shtml" target="test_blank"&gt;http://pinouts.ru/data/memorysrick_pinout.shtml&lt;/A&gt;&lt;BR /&gt;&lt;A href="http://pinouts.ru/data/sdcard_pinout.shtml" target="test_blank"&gt;http://pinouts.ru/data/sdcard_pinout.shtml&lt;/A&gt;&lt;BR /&gt;&lt;A href="http://pinouts.ru/data/mmcard_pinout.shtml" target="test_blank"&gt;http://pinouts.ru/data/mmcard_pinout.shtml&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;By there way, is there a way that a hard drive could be interfaced to the M52235?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2006 21:30:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235-and-External-Memory/m-p/134517#M1472</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2006-05-04T21:30:12Z</dc:date>
    </item>
    <item>
      <title>Re: M52235 and External Memory</title>
      <link>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235-and-External-Memory/m-p/134518#M1473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi BenjaminRoy,&lt;/P&gt;&lt;P&gt;SST and Spansion have external flash memories that have a SPI interface.&lt;/P&gt;&lt;P&gt;You could bit bang a protocol on GPIO for the memory sticks you've sent links to but that bandwidth would be far less than using the intergrates SPI bus.&lt;/P&gt;&lt;P&gt;I do not have an example SPI to Flash schematic.&lt;/P&gt;&lt;P&gt;Regards, DavidS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 May 2006 02:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/ColdFire-68K-Microcontrollers/M52235-and-External-Memory/m-p/134518#M1473</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2006-05-06T02:21:19Z</dc:date>
    </item>
  </channel>
</rss>